License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
This notice may not be removed or altered from any source distribution.
/***************************************************************************/
#ifndef _OTA_BROADCAST_BOOTLOADER_CLIENT_H_
#define _OTA_BROADCAST_BOOTLOADER_CLIENT_H_
#include "ota-broadcast-bootloader/ota-broadcast-bootloader-protocol.h"
#include "ota-broadcast-bootloader/ota-broadcast-bootloader-types.h"
EmberAfOtaBootloaderStatus emberAfPluginOtaBootloaderClientAbortImageDownload(uint8_t imageTag,
uint8_t applicationErrorStatus);
//------------------------------------------------------------------------------
// Callbacks
bool emberAfPluginOtaBootloaderClientNewIncomingImageCallback(EmberNodeId serverId,
EmberNodeId *alternateServerId,
uint8_t imageTag);
void emberAfPluginOtaBootloaderClientIncomingImageSegmentCallback(EmberNodeId serverId,
uint32_t startIndex,
uint32_t endIndex,
uint8_t imageTag,
uint8_t *imageSegment);
void emberAfPluginOtaBootloaderClientImageDownloadCompleteCallback(EmberAfOtaBootloaderStatus status,
uint8_t imageTag,
uint32_t imageSize);
void emberAfPluginOtaBootloaderClientIncomingRequestStatusCallback(EmberNodeId serverId,
uint8_t applicationServerStatus,
uint8_t *applicationStatus);
bool emberAfPluginOtaBootloaderClientIncomingRequestBootloadCallback(EmberNodeId serverId,
uint8_t imageTag,
uint32_t bootloadDelayMs,
uint8_t *applicationStatus);
#endif // _OTA_BROADCAST_BOOTLOADER_CLIENT_H_
Callbacks#
A callback invoked when the OTA Bootloader Client starts receiving a new image. The application can choose to start receiving the image or it can ignore it. If the application chooses to receive the image, other images sent out by other servers are ignored until the client completes this download.
A callback invoked when an image segment, that is part of an image that the application elected to download, was received on the OTA Bootloader Client.
A callback invoked on an OTA Bootloader Client to indicate that an image downlaod is completed.
A callback invoked on the OTA Bootloader Client to indicate that an OTA Bootloader Server has requested the status of the client device.
A callback invoked by the OTA Bootloader Client plugin to indicate that an OTA Bootloader Server has requested to perform a bootload operation at a certain point in time in the future.
Functions#
Abort an ongoing image download process.
Callbacks Documentation#
emberAfPluginOtaBootloaderClientNewIncomingImageCallback#
bool emberAfPluginOtaBootloaderClientNewIncomingImageCallback (EmberNodeId serverId, EmberNodeId * alternateServerId, uint8_t imageTag)
A callback invoked when the OTA Bootloader Client starts receiving a new image. The application can choose to start receiving the image or it can ignore it. If the application chooses to receive the image, other images sent out by other servers are ignored until the client completes this download.
[in] | serverId | The node ID of the server that initiated the new image distribution process. |
[out] | alternateServerId | This node ID can be set by the application to include a well-known alternate server. If this is set to a valid address, the client allows segments also from this alternate server. If this is set to EMBER_BROADCAST_ADDRESS, the client accepts segments with the same image tag from any server. |
[in] | imageTag | A 1-byte tag that identifies the incoming image. |
Returns
Return true to accept the image or false to ignore it.
94
of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/ota-broadcast-bootloader/ota-broadcast-bootloader-client/ota-broadcast-bootloader-client.h
emberAfPluginOtaBootloaderClientIncomingImageSegmentCallback#
void emberAfPluginOtaBootloaderClientIncomingImageSegmentCallback (EmberNodeId serverId, uint32_t startIndex, uint32_t endIndex, uint8_t imageTag, uint8_t * imageSegment)
A callback invoked when an image segment, that is part of an image that the application elected to download, was received on the OTA Bootloader Client.
[in] | serverId | The node ID of the server that initiated the image distribution process. |
[in] | startIndex | The index of the first byte of the passed segment. |
[in] | endIndex | The index of the last byte of the passed segment. |
[in] | imageTag | A 1-byte tag of the image the passed segment belongs to. |
[in] | imageSegment | An array containing the image segment. |
114
of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/ota-broadcast-bootloader/ota-broadcast-bootloader-client/ota-broadcast-bootloader-client.h
emberAfPluginOtaBootloaderClientImageDownloadCompleteCallback#
void emberAfPluginOtaBootloaderClientImageDownloadCompleteCallback (EmberAfOtaBootloaderStatus status, uint8_t imageTag, uint32_t imageSize)
A callback invoked on an OTA Bootloader Client to indicate that an image downlaod is completed.
[in] | status | An EmberAfOtaBootloaderStatus value of:
|
[in] | imageTag | A 1-byte tag of the image this callback refers to. |
[in] | imageSize | The total size of the downloaded image in bytes. This parameter is meaningful only in case the status parameter is set to EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS. |
143
of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/ota-broadcast-bootloader/ota-broadcast-bootloader-client/ota-broadcast-bootloader-client.h
emberAfPluginOtaBootloaderClientIncomingRequestStatusCallback#
void emberAfPluginOtaBootloaderClientIncomingRequestStatusCallback (EmberNodeId serverId, uint8_t applicationServerStatus, uint8_t * applicationStatus)
A callback invoked on the OTA Bootloader Client to indicate that an OTA Bootloader Server has requested the status of the client device.
[in] | serverId | The ID of the server the request came from. |
[in] | applicationServerStatus | The server application status, which was set by emberAfPluginBootloaderServerInitiateRequestTargetsStatus() |
[out] | applicationStatus | A 1-byte status set by the client application that is reported to the server. |
158
of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/ota-broadcast-bootloader/ota-broadcast-bootloader-client/ota-broadcast-bootloader-client.h
emberAfPluginOtaBootloaderClientIncomingRequestBootloadCallback#
bool emberAfPluginOtaBootloaderClientIncomingRequestBootloadCallback (EmberNodeId serverId, uint8_t imageTag, uint32_t bootloadDelayMs, uint8_t * applicationStatus)
A callback invoked by the OTA Bootloader Client plugin to indicate that an OTA Bootloader Server has requested to perform a bootload operation at a certain point in time in the future.
[in] | serverId | The ID of the server the request came from. |
[in] | imageTag | A 1-byte tag of the image this callback refers to. |
[in] | bootloadDelayMs | The delay in milliseconds after which the client has been requested to perform a bootload operation. |
[out] | applicationStatus | A 1-byte status set by the client application that is reported to the server. |
Returns
Return true if the application accepted the request of bootloading the specified image at the requested time, false otherwise.
179
of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/ota-broadcast-bootloader/ota-broadcast-bootloader-client/ota-broadcast-bootloader-client.h
Function Documentation#
emberAfPluginOtaBootloaderClientAbortImageDownload#
EmberAfOtaBootloaderStatus emberAfPluginOtaBootloaderClientAbortImageDownload (uint8_t imageTag, uint8_t applicationErrorStatus)
Abort an ongoing image download process.
[in] | imageTag | A 1-byte tag that identifies the image the client should no longer download. |
[in] | applicationErrorStatus | A 1-byte error code reported to the server. |
Returns
An EmberAfOtaBootloaderStatus value of:
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS If the ongoing image download process was successfully aborted.
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_INVALID_CALL If the client was not currently involved in an image download process or it was currently downloading an image with a different tag.
62
of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/ota-broadcast-bootloader/ota-broadcast-bootloader-client/ota-broadcast-bootloader-client.h