/***************************************************************************/
#ifndef RADIO_STREAM_H
#define RADIO_STREAM_H

EmberStatus emberStartTxStream(EmberTxStreamParameters parameters, uint16_t channel);

EmberStatus emberStopTxStream(void);

 #endif

Functions#

emberStartTxStream(EmberTxStreamParameters parameters, uint16_t channel)

Start a continuous TX stream to test RF.

Stop an RF stream in progress.

Function Documentation#

emberStartTxStream#

EmberStatus emberStartTxStream (EmberTxStreamParameters parameters, uint16_t channel)

Start a continuous TX stream to test RF.

Parameters
TypeDirectionArgument NameDescription
EmberTxStreamParameters[in]parameters

Stream mode. See EmberTxStreamParameters.

uint16_t[in]channel

RF channel.

Returns

  • EMBER_INVALID_CALL if the stack can not process the request EMBER_BAD_ARGUMENT if the parameters are wrong EMBER_SUCCESS if the stream can be started


emberStopTxStream#

EmberStatus emberStopTxStream (void )

Stop an RF stream in progress.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • EMBER_INVALID_CALL if no stream is in progress EMBER_SUCCESS otherwise