License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
This notice may not be removed or altered from any source distribution.
/***************************************************************************/
#ifndef _OTA_BROADCAST_BOOTLOADER_SERVER_H_
#define _OTA_BROADCAST_BOOTLOADER_SERVER_H_
#include "ota-broadcast-bootloader/ota-broadcast-bootloader-protocol.h"
#include "ota-broadcast-bootloader/ota-broadcast-bootloader-types.h"
#define EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_STACK_ERRORS 8
#define EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_UNICAST_ERRORS 4
#define EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_RESPONSE_TIMEOUT_MS 250
#define EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_BROADCAST_ROUNDS 5
//------------------------------------------------------------------------------
// APIs
EmberAfOtaBootloaderStatus emberAfPluginOtaBootloaderServerInitiateImageDistribution(uint32_t imageSize,
uint8_t imageTag,
EmberNodeId *targetList,
uint16_t targetListLength);
EmberAfOtaBootloaderStatus emberAfPluginBootloaderServerInitiateRequestTargetsStatus(EmberNodeId *targetList,
uint16_t targetListLength,
uint8_t applicationServerStatus);
EmberAfOtaBootloaderStatus emberAfPluginBootloaderServerInitiateRequestTargetsBootload(uint32_t bootloadDelayMs,
uint8_t imageTag,
EmberNodeId *targetList,
uint16_t targetListLength);
EmberAfOtaBootloaderTargetStatus emberAfPluginBootloaderServerGetTargetStatus(EmberNodeId targetId,
uint8_t *applicationTargetStatus);
EmberAfOtaBootloaderStatus emberAfPluginOtaBootloaderServerAbortCurrentProcess(void);
//------------------------------------------------------------------------------
// Callbacks
bool emberAfPluginOtaBootloaderServerGetImageSegmentCallback(uint32_t startIndex,
uint32_t endIndex,
uint8_t imageTag,
uint8_t *imageSegment);
void emberAfPluginOtaBootloaderServerImageDistributionCompleteCallback(EmberAfOtaBootloaderStatus status);
void emberAfPluginBootloaderServerRequestTargetsStatusCompleteCallback(EmberAfOtaBootloaderStatus status);
void emberAfPluginBootloaderServerRequestTargetsBootloadCompleteCallback(EmberAfOtaBootloaderStatus status);
#endif // _OTA_BROADCAST_BOOTLOADER_SERVER_H_
Callbacks#
A callback invoked on the OTA Bootloader Server during an image distribution process to retrieve a contiguous segment of the image being distributed.
A callback invoked on the OTA Bootloader Server when the image distribution process is terminated. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API to retrieve the status reported by each target device.
A callback invoked on the OTA Bootloader Server when bootload request process has completed. Within this callback, the application should use the emberAfPluginBootloaderServerGetTargetStatus() API to retrieve the status and application status reported by each target.
A callback invoked on the OTA Bootloader Server when a bootload request process has completed. Within this callback, the application should use the emberAfPluginBootloaderServerGetTargetStatus() API to retrieve the status and the application status reported by each target.
Macros#
The number of consecutive stack message submission errors or stack-related errors, such as CSMA failures, after which the plugin gives up.
The number of consecutive unicast attempts after which a target is declared unreachable. Legal values for this are in the [0,7] range.
The time in milliseconds after which the server gives up waiting for a response from a client.
The maximum number of image broadcast rounds the server performs before declaring an image distribution process failed.
Functions#
Initiate the image distribution process. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API at any time during the image distribution process to check the status of each target.
Initiate the process to request the status of a set of target devices. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API at any time during the target status request process to check the status of each target.
Start the process where a server requests a set of target devices to initiate the bootload of a received image at some point in the future. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API at any time during the bootload request process to check the status of each target.
Retrieve the locally stored status of an individual target in the distribution list. The locally stored status can be updated by calling emberAfPluginBootloaderServerInitiateRequestTargetsStatus().
Abort the ongoing process (image distribution, status request or bootload request). Note that aborting a bootload request process likely results in some targets performing the bootload while some others do not.
Callbacks Documentation#
emberAfPluginOtaBootloaderServerGetImageSegmentCallback#
bool emberAfPluginOtaBootloaderServerGetImageSegmentCallback (uint32_t startIndex, uint32_t endIndex, uint8_t imageTag, uint8_t * imageSegment)
A callback invoked on the OTA Bootloader Server during an image distribution process to retrieve a contiguous segment of the image being distributed.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | startIndex | The index of the first byte the application should copy into the passed array. |
| uint32_t | [in] | endIndex | The index of the last byte the application should copy into the passed array. |
| uint8_t | [in] | imageTag | A 1-byte tag of the image for which a segment is being requested. |
| uint8_t * | [out] | imageSegment | An array of (endIndex - startIndex + 1) length to which the application should copy the requested image segment. |
Returns
A boolean indicating whether the application successfully copied the requested bytes into the passed array. If the application returns false, the OTA Server plugin aborts the ongoing distribution process.
emberAfPluginOtaBootloaderServerImageDistributionCompleteCallback#
void emberAfPluginOtaBootloaderServerImageDistributionCompleteCallback (EmberAfOtaBootloaderStatus status)
A callback invoked on the OTA Bootloader Server when the image distribution process is terminated. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API to retrieve the status reported by each target device.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberAfOtaBootloaderStatus | [in] | status | An EmberAfOtaBootloaderStatus value of:
|
emberAfPluginBootloaderServerRequestTargetsStatusCompleteCallback#
void emberAfPluginBootloaderServerRequestTargetsStatusCompleteCallback (EmberAfOtaBootloaderStatus status)
A callback invoked on the OTA Bootloader Server when bootload request process has completed. Within this callback, the application should use the emberAfPluginBootloaderServerGetTargetStatus() API to retrieve the status and application status reported by each target.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberAfOtaBootloaderStatus | [in] | status | An EmberAfOtaBootloaderStatus value of:
|
emberAfPluginBootloaderServerRequestTargetsBootloadCompleteCallback#
void emberAfPluginBootloaderServerRequestTargetsBootloadCompleteCallback (EmberAfOtaBootloaderStatus status)
A callback invoked on the OTA Bootloader Server when a bootload request process has completed. Within this callback, the application should use the emberAfPluginBootloaderServerGetTargetStatus() API to retrieve the status and the application status reported by each target.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberAfOtaBootloaderStatus | [in] | status | An EmberAfOtaBootloaderStatus value of:
|
Function Documentation#
emberAfPluginOtaBootloaderServerInitiateImageDistribution#
EmberAfOtaBootloaderStatus emberAfPluginOtaBootloaderServerInitiateImageDistribution (uint32_t imageSize, uint8_t imageTag, EmberNodeId * targetList, uint16_t targetListLength)
Initiate the image distribution process. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API at any time during the image distribution process to check the status of each target.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | imageSize | The image size in bytes to be distributed. |
| uint8_t | [in] | imageTag | A 1-byte tag that will be embedded in the server-to-client over-the-air messages. The application can use the image tag for versioning purposes and/or for distinguishing between different image types. |
| EmberNodeId * | [out] | targetList | An array of EmberNodeId indicating the node IDs of the target devices. |
| uint16_t | [in] | targetListLength | The length of the passed |
Returns
An EmberAfOtaBootloaderStatus value of:
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS if the image distribution is successfully initiated. If this is the case, the emberAfPluginOtaBootloaderServerImageDistributionCompleteCallback() callback is invoked when the distribution process terminates.
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_INVALID_CALL if some of the passed parameters are invalid.
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_BUSY if the server is already performing another image distribution or some other over-the-air process.
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_NO_BUFFERS if the server can't allocate memory from the heap to store the passed target list. (See Memory Buffer for details).
emberAfPluginBootloaderServerInitiateRequestTargetsStatus#
EmberAfOtaBootloaderStatus emberAfPluginBootloaderServerInitiateRequestTargetsStatus (EmberNodeId * targetList, uint16_t targetListLength, uint8_t applicationServerStatus)
Initiate the process to request the status of a set of target devices. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API at any time during the target status request process to check the status of each target.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId * | [in] | targetList | An array of EmberNodeId indicating the node IDs of the target devices that are queried for their status. |
| uint16_t | [in] | targetListLength | The length of the passed |
| uint8_t | [in] | applicationServerStatus | The application can set a status here which will be sent to the clients in emberAfPluginOtaBootloaderClientIncomingRequestStatusCallback() |
Returns
An EmberAfOtaBootloaderStatus value of:
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS if the plugin successfully initiated the process of requesting the status of a set of targets. If this is the case, the corresponding callback emberAfPluginBootloaderServerRequestTargetsStatusCompleteCallback() is invoked when the request process to all targets completes.
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_INVALID_CALL if some of the passed parameters are invalid.
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_BUSY if the server is currently involved in another over-the-air process.
emberAfPluginBootloaderServerInitiateRequestTargetsBootload#
EmberAfOtaBootloaderStatus emberAfPluginBootloaderServerInitiateRequestTargetsBootload (uint32_t bootloadDelayMs, uint8_t imageTag, EmberNodeId * targetList, uint16_t targetListLength)
Start the process where a server requests a set of target devices to initiate the bootload of a received image at some point in the future. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API at any time during the bootload request process to check the status of each target.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | bootloadDelayMs | The delay in milliseconds after which all the targets should perform an image bootload. |
| uint8_t | [in] | imageTag | A 1-byte tag that identifies the image to be bootloaded at the target devices. |
| EmberNodeId * | [in] | targetList | An array of EmberNodeId indicating the node IDs of the target devices that is requested to bootload an image. |
| uint16_t | [in] | targetListLength | The length of the passed |
Returns
An EmberAfOtaBootloaderStatus value of:
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS if the plugin successfully initiated the process of requesting a set of targets to initiate a bootload. If this is the case, the corresponding callback emberAfPluginBootloaderServerRequestTargetsBootloadCompleteCallback() shall be invoked when the request process to all targets has completed.
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_INVALID_CALL if some of the passed parameters are invalid.
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_BUSY if the server is currently involved in another over-the-air process.
emberAfPluginBootloaderServerGetTargetStatus#
EmberAfOtaBootloaderTargetStatus emberAfPluginBootloaderServerGetTargetStatus (EmberNodeId targetId, uint8_t * applicationTargetStatus)
Retrieve the locally stored status of an individual target in the distribution list. The locally stored status can be updated by calling emberAfPluginBootloaderServerInitiateRequestTargetsStatus().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | [in] | targetId | The node ID of the target device whose status is being requested. |
| uint8_t * | [out] | applicationTargetStatus | The application status reported by the client side application. This parameter is valid only for certain return status codes (see return status documentation). |
Returns
An EmberAfOtaBootloaderTargetStatus value of:
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_INVALID if the passed node ID does not appear in the current server target list of the current ongoing process or if there is no current ongoing process.
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_UNREACHABLE if the target has not responded to any of the server's unicast messages.
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_DISTRIBUTION_COMPLETED if the server is currently performing an image distribution process and the target confirmed that it received the full image.
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_DISTRIBUTION_ONGOING if the server is currently performing an image distribution process and the target has partially received the image and distribution is continuing.
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_DISTRIBUTION_REFUSED if the target has refused the current image.
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_DISTRIBUTION_FAILED if the server is currently performing an image distribution process and the target reported that an error was encountered.
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_DISTRIBUTION_ABORTED if the server is currently performing an image distribution process and the target decided to abort the image download process. In this case, the client also reports an application status. Therefore, the applicationTargetStatus parameter is valid.
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_STATUS_REQUEST_COMPLETED if the server is currently performing a target status request process and the target has responded to the server's inquiry. In this case, the client also reports an application status. Therefore, the applicationTargetStatus parameter is valid.
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_STATUS_REQUEST_ONGOING if the server is currently performing a target status request process and the target is not yet queried by the server.
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_BOOTLOAD_REQUEST_ACCEPTED if the server is currently performing a bootload request process and the target has accepted to perform the requested image bootload.
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_BOOTLOAD_REQUEST_REFUSED if the server is currently performing a bootload request process and the target has refused to perform the requested image bootload.
EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_BOOTLOAD_REQUEST_ONGOING if the server is currently performing a bootload request process and the target is not yet reached by the server.
emberAfPluginOtaBootloaderServerAbortCurrentProcess#
EmberAfOtaBootloaderStatus emberAfPluginOtaBootloaderServerAbortCurrentProcess (void )
Abort the ongoing process (image distribution, status request or bootload request). Note that aborting a bootload request process likely results in some targets performing the bootload while some others do not.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
An EmberAfOtaBootloaderStatus value of:
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS if the current ongoing process was successfully aborted.
EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_INVALID_CALL if the server is not currently involved in any process.