Silicon Labs
connect-stack/4.0.0/connect-stack-api/group-parent-support
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
Results 1-5 of 5 for connect-stack/4.0.0/connect-stack-api/group-parent-support in 0.26 seconds
Advertiser | Bluetooth Stack API Reference | Bluetooth LE | v8.0.0 | Silicon Labs
https://docs.silabs.com/.../sl-bt-adverti...
Community Support Github ... // Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... 3: Advertise on CH37 and CH38 4: Advertise on CH39 5: Advertise on CH37 and CH39
BGAPI | BGAPI headers | Bluetooth LE | v5.0 | Silicon Labs
https://docs.silabs.com/....
Training ... // Bluetooth LE//Version 5.0 //API Reference //BGAPI Headers ... Locate the row in the message group according to the message ID which is the Byte 4 of the message header.
TX Power Limitations for Regulatory Compliance (ETSI, FCC) | System & Performance | Bluetooth LE | v3.1 | Silicon Labs
https://docs.silabs.com/.../tx-power-limitations-for-regulatory-compliance-etsi-...
Community Support Github ... Because Bluetooth stack follows strict regulations, the maximum output power is 10 dBm ... This stack limitation (10 dBm EIRP) is valid for all PHYs and devices.
Adaptive Frequency Hopping | System & Performance | Bluetooth LE | v5.0 | Silicon Labs
https://docs.silabs.com/.../adaptive-frequency-hopp...
Community Support Github ... Channel map update procedure is part of the Bluetooth 4.0 specification. ... one connection is active, the Bluetooth stack runs a periodic background task that ...
AN1328: Enabling a Radio Co-Processor using the Bluetooth HCI Function
https://www.silabs.com/.../an1328-enabling-rcp-using-bt-hci....
KEY POINTS ... The application communicates with the Bluetooth LE protocol stack via BGAPI. Figure 1.4. SoC Mode ... 1 0-255 1 ... Size 4 4 ... Max_support_tx_power min_configured_tx_power
Resource TypeApplication Notes
    Results 1-5 of 5 for connect-stack/4.0.0/connect-stack-api/group-parent-support