License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

SPDX-License-Identifier: Zlib

The licensor of this software is Silicon Laboratories Inc.

This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.

Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:

  1. The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.

  2. Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.

  3. This notice may not be removed or altered from any source distribution.

/***************************************************************************/
#ifndef __EMBER_TYPES_H__
#define __EMBER_TYPES_H__

#ifdef EMBER_TEST
#include PLATFORM_HEADER
#endif
#include "sl_common.h"

#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>

#ifndef DOXYGEN_SHOULD_SKIP_THIS
#include "stack/config/ember-configuration-defaults.h"
#endif //DOXYGEN_SHOULD_SKIP_THIS

#define EXTENDED_PAN_ID_SIZE 8

#define EUI64_SIZE 8

#define EMBER_ENCRYPTION_KEY_SIZE 16

typedef uint8_t EmberEUI64[EUI64_SIZE];

typedef uint16_t EmberNodeId;

typedef uint16_t EmberPanId;

#define EMBER_NULL_NODE_ID                0xFFFFu

#define EMBER_BROADCAST_ADDRESS           0xFFFF

#define EMBER_USE_LONG_ADDRESS            0xFFFE

#define EMBER_COORDINATOR_ADDRESS         0x0000

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberNodeType
#else
typedef uint8_t EmberNodeType;
enum
#endif
{
  EMBER_UNKNOWN_DEVICE = 0,
  EMBER_STAR_COORDINATOR = 1,
  EMBER_STAR_RANGE_EXTENDER = 2,
  EMBER_STAR_END_DEVICE = 3,
  EMBER_STAR_SLEEPY_END_DEVICE = 4,
  EMBER_DIRECT_DEVICE = 5,
  EMBER_MAC_MODE_DEVICE = 6,
  EMBER_MAC_MODE_SLEEPY_DEVICE = 7,
};

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberNetworkStatus
#else
typedef uint8_t EmberNetworkStatus;
enum
#endif
{
  EMBER_NO_NETWORK,
  EMBER_JOINING_NETWORK,
  EMBER_JOINED_NETWORK,
  EMBER_RADIO_TEST
};

typedef struct {
  uint16_t  panId;
  int16_t   radioTxPower;
  uint16_t   radioChannel;
} EmberNetworkParameters;

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberChildFlags
#else
typedef uint8_t EmberChildFlags;
enum
#endif
{
  EMBER_CHILD_FLAGS_DEVICE_IS_RANGE_EXTENDER_BIT       = 0x02,
  EMBER_CHILD_FLAGS_DEVICE_IS_SLEEPY_BIT               = 0x04,
  EMBER_CHILD_FLAGS_HAVE_PENDING_DATA_BIT              = 0x08,
  EMBER_CHILD_FLAGS_AES_SECURITY_CAPABLE_BIT           = 0x10,
  EMBER_CHILD_FLAG_DEVICE_IS_EXTENDED_BIT              = 0x20,
};

typedef uint16_t EmberMessageLength;

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberMessageOptions
#else
typedef uint8_t EmberMessageOptions;
enum
#endif
{
  EMBER_OPTIONS_NONE                     = 0x00,
  EMBER_OPTIONS_SECURITY_ENABLED         = 0x01,
  EMBER_OPTIONS_ACK_REQUESTED            = 0x02,
  EMBER_OPTIONS_HIGH_PRIORITY            = 0x04,
  EMBER_OPTIONS_INDIRECT                 = 0x08,
};

typedef struct {
  EmberMessageOptions options;
  EmberNodeId source;
  uint8_t endpoint;
  int8_t rssi;
  EmberMessageLength length;
  uint8_t *payload;
  uint32_t timestamp;
  uint8_t lqi;
} EmberIncomingMessage;

typedef struct {
  EmberMessageOptions options;
  EmberNodeId destination;
  uint8_t endpoint;
  uint8_t tag;
  EmberMessageLength length;
  uint8_t *payload;
  int8_t ackRssi;
  uint32_t timestamp;
} EmberOutgoingMessage;

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberMacAddressMode
#else
typedef uint8_t EmberMacAddressMode;
enum
#endif
{
  EMBER_MAC_ADDRESS_MODE_NONE  = 0x00,
  EMBER_MAC_ADDRESS_MODE_SHORT = 0x02,
  EMBER_MAC_ADDRESS_MODE_LONG  = 0x03,
};

typedef struct {
  union {
    uint8_t longAddress[EUI64_SIZE];
    uint16_t shortAddress;
  } addr;

  EmberMacAddressMode mode; 
} EmberMacAddress;

typedef struct {
  EmberMacAddress srcAddress;
  EmberMacAddress dstAddress;
  EmberPanId srcPanId;
  EmberPanId dstPanId;
  bool srcPanIdSpecified;
  bool dstPanIdSpecified;
} EmberMacFrame;

typedef struct {
  EmberMessageOptions options;
  EmberMacFrame macFrame;
  int8_t rssi;
  uint8_t lqi;
  uint32_t frameCounter;
  EmberMessageLength length;
  uint8_t *payload;
  uint32_t timestamp;
} EmberIncomingMacMessage;

typedef struct {
  EmberMessageOptions options;
  EmberMacFrame macFrame;
  uint8_t tag;
  uint32_t frameCounter;
  EmberMessageLength length;
  uint8_t *payload;
  int8_t ackRssi;
  uint32_t timestamp;
} EmberOutgoingMacMessage;

typedef struct {
  uint8_t contents[EMBER_ENCRYPTION_KEY_SIZE];
} EmberKeyData;

#if defined DOXYGEN_SHOULD_SKIP_THIS
uint8_t* emberKeyContents(EmberKeyData* key);
#else
#define emberKeyContents(key) ((key)->contents)
#endif

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberEventUnits
#else
typedef uint8_t EmberEventUnits;
enum
#endif
{
  EMBER_EVENT_INACTIVE = 0,
  EMBER_EVENT_MS_TIME,
  EMBER_EVENT_QS_TIME,
  EMBER_EVENT_MINUTE_TIME,
  EMBER_EVENT_ZERO_DELAY
};

typedef uint8_t EmberTaskId;

typedef struct sl_connect_radio_priority {
  uint8_t rx;
  uint8_t starting_tx;
  uint8_t tx_step;
} sl_connect_radio_priority_t;

//----------------------------------------------------------------
// Events and event queues.

// Forward declarations to make up for C's one-pass type checking.
struct Event_s;
struct EventQueue_s;

typedef const struct {
  struct EventQueue_s *queue;           // the queue this event goes on
  void (*handler)(struct Event_s *);    // called when the event fires
  void (*marker)(struct Event_s *);     // marking function, can be NULL
  const char *name;                     // event name for debugging purposes
} EventActions;

typedef struct Event_s {
  EventActions *actions;                // static data

  // For internal use only, but the 'next' field must be initialized
  // to NULL.
  struct Event_s *next;
  uint32_t timeToExecute;
} Event;

typedef struct EventQueue_s {
  Event *isrEvents;
  Event *events;
} EventQueue;

typedef struct {
  EmberEventUnits status;
  EmberTaskId taskid;
  uint32_t timeToExecute;
} EmberEventControl;

typedef const struct EmberEventData_S {
  EmberEventControl *control;
  void (*handler)(void);
} EmberEventData;

typedef struct {
  uint32_t nextEventTime;
  EmberEventData *events;
  bool busy;
} EmberTaskControl;

enum {
  EMBER_OUTGOING_MESSAGES = 0x0001,
  EMBER_INCOMING_MESSAGES = 0x0002,
  EMBER_RADIO_IS_ON = 0x0004,
  EMBER_ASSOCIATING = 0x0008,
  EMBER_SCANNING = 0x0010,
};

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberCounterType
#else
typedef uint8_t EmberCounterType;
enum
#endif
{
  EMBER_COUNTER_PHY_IN_PACKETS,

  EMBER_COUNTER_PHY_OUT_PACKETS,

  EMBER_COUNTER_MAC_IN_UNICAST,

  EMBER_COUNTER_MAC_IN_BROADCAST,

  EMBER_COUNTER_MAC_OUT_UNICAST_NO_ACK,

  EMBER_COUNTER_MAC_OUT_UNICAST_ACK_SUCCESS,

  EMBER_COUNTER_MAC_OUT_UNICAST_ACK_FAIL,

  EMBER_COUNTER_MAC_OUT_UNICAST_CCA_FAIL,

  EMBER_COUNTER_MAC_OUT_UNICAST_RETRY,

  EMBER_COUNTER_MAC_OUT_BROADCAST,

  EMBER_COUNTER_MAC_OUT_BROADCAST_CCA_FAIL,

  EMBER_COUNTER_MAC_OUT_ENCRYPT_FAIL,

  EMBER_COUNTER_MAC_DROP_IN_MEMORY,

  EMBER_COUNTER_MAC_DROP_IN_FRAME_COUNTER,

  EMBER_COUNTER_MAC_DROP_IN_DECRYPT,

  EMBER_COUNTER_NWK_OUT_FORWARDING,

  EMBER_COUNTER_NWK_IN_SUCCESS,

  EMBER_COUNTER_NWK_DROP_IN_WRONG_SOURCE,

  EMBER_COUNTER_NWK_DROP_IN_FORWARDING,

  EMBER_COUNTER_UART_IN_DATA,
  EMBER_COUNTER_UART_IN_MANAGEMENT,
  EMBER_COUNTER_UART_IN_FAIL,
  EMBER_COUNTER_UART_OUT_DATA,
  EMBER_COUNTER_UART_OUT_MANAGEMENT,
  EMBER_COUNTER_UART_OUT_FAIL,

  // Counters for non-packet events below.
  EMBER_COUNTER_ROUTE_2_HOP_LOOP,
  EMBER_COUNTER_BUFFER_ALLOCATION_FAIL,

  EMBER_ASH_V3_ACK_SENT,
  EMBER_ASH_V3_ACK_RECEIVED,
  EMBER_ASH_V3_NACK_SENT,
  EMBER_ASH_V3_NACK_RECEIVED,
  EMBER_ASH_V3_RESEND,
  EMBER_ASH_V3_BYTES_SENT,
  EMBER_ASH_V3_TOTAL_BYTES_RECEIVED,
  EMBER_ASH_V3_VALID_BYTES_RECEIVED,
  EMBER_ASH_V3_PAYLOAD_BYTES_SENT,

  EMBER_COUNTER_TYPE_COUNT,
};

typedef uint16_t EmberBuffer;

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberPhyType
#else
typedef uint8_t EmberPhyType;
enum
#endif
{
  EMBER_RADIO_CONFIGURATOR,

  EMBER_STANDARD_PHY_2_4GHZ,

  EMBER_STANDARD_PHY_915MHZ,

  EMBER_STANDARD_PHY_863MHZ
};

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberCalType
#else
typedef uint32_t EmberCalType;
enum
#endif
{
  EMBER_CAL_TEMP_VCO = 0x00000001,

  EMBER_CAL_IRCAL    = 0x00010000,

  EMBER_CAL_ALL      = 0x00010001
};

#define EMBER_CAL_INVALID_VALUE    (0xFFFFFFFF)

#ifndef DOXYGEN_SHOULD_SKIP_THIS
//doxygen should see this in error-def.h

#ifndef __EMBERSTATUS_TYPE__
#define __EMBERSTATUS_TYPE__
typedef uint8_t EmberStatus;
#endif //__EMBERSTATUS_TYPE__

#endif //DOXYGEN_SHOULD_SKIP_THIS

//------------------------------------------------------------------------------
// INTERNAL TYPES AND DEFINES
//------------------------------------------------------------------------------

#ifndef DOXYGEN_SHOULD_SKIP_THIS

typedef struct {
  EmberNodeId destination;
  uint8_t endpoint;
  uint8_t tag;
  EmberBuffer payload;
  EmberMessageOptions txOptions;
} EmOutgoingPacket;

typedef struct {
  uint32_t lastSeen;
  uint32_t frameCounter;
  EmberNodeId shortId;
  EmberEUI64 longId;
  uint8_t flags;
  uint8_t leaveCount;
} EmberChildEntry;

typedef uint8_t EmberLibraryStatus;

typedef void (*ClientResyncCallback)(EmberStatus status);

typedef struct {
  EmberBuffer* buffer_addr;
  uint16_t buffer_length;
} EmberBufferDesc;

// A library's status is an 8-bit value with information about it.
// The high bit indicates whether the library is present (1), or if it is a
// stub (0).  The lower 7-bits can be used for codes specific to the library.
// This allows a library, like the security library, to specify what additional
// features are present.
// A value of 0xFF is reserved, it indicates an error in retrieving the
// library status.
#define EMBER_LIBRARY_PRESENT_MASK          0x80
#define EMBER_LIBRARY_IS_STUB               0x00
#define EMBER_LIBRARY_ERROR                 0xFF

#define emberDebugPrintf(...)
#define emLog(type, ...)
#define emLogLine(type, ...)
#define emLogBytes(type, format, bytes, count, ...)

#endif //DOXYGEN_SHOULD_SKIP_THIS

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberTxStreamParameters
#else
typedef uint8_t EmberTxStreamParameters;
enum
#endif
{
  TX_STREAM_PN9, 
  TX_STREAM_CW   
};

#endif // __EMBER_TYPES_H__

Modules#

EmberNetworkParameters

EmberIncomingMessage

EmberOutgoingMessage

EmberMacAddress

EmberMacFrame

EmberIncomingMacMessage

EmberOutgoingMacMessage

EmberKeyData

sl_connect_radio_priority

EventActions

Event_s

EventQueue_s

EmberEventControl

EmberEventData_S

EmberTaskControl

Macros#

#define
EXTENDED_PAN_ID_SIZE 8

Size of an extended PAN identifier in bytes (8).

#define
EUI64_SIZE 8

Size of EUI64 (an IEEE address) in bytes (8).

#define
EMBER_ENCRYPTION_KEY_SIZE 16

Size of an encryption key in bytes (16).

#define
EMBER_NULL_NODE_ID 0xFFFFu

A distinguished network ID that will never be assigned to any node. Used to indicate the absence of a node ID.

#define
EMBER_BROADCAST_ADDRESS 0xFFFF

Broadcast address.

#define
EMBER_USE_LONG_ADDRESS 0xFFFE

Special short address indicating the node should use long addressing as source address.

#define
EMBER_COORDINATOR_ADDRESS 0x0000

The coordinator short address.

#define
EMBER_CAL_INVALID_VALUE (0xFFFFFFFF)

Enumerations#

enum
EMBER_UNKNOWN_DEVICE = 0
EMBER_STAR_COORDINATOR = 1
EMBER_STAR_RANGE_EXTENDER = 2
EMBER_STAR_END_DEVICE = 3
EMBER_STAR_SLEEPY_END_DEVICE = 4
EMBER_DIRECT_DEVICE = 5
EMBER_MAC_MODE_DEVICE = 6
EMBER_MAC_MODE_SLEEPY_DEVICE = 7
}

Define the possible types of nodes and the roles that a node might play in a network.

enum
EMBER_NO_NETWORK
EMBER_JOINING_NETWORK
EMBER_JOINED_NETWORK
EMBER_RADIO_TEST
}

Defines the possible join states for a node.

enum
EMBER_CHILD_FLAGS_DEVICE_IS_RANGE_EXTENDER_BIT = 0x02
EMBER_CHILD_FLAGS_DEVICE_IS_SLEEPY_BIT = 0x04
EMBER_CHILD_FLAGS_HAVE_PENDING_DATA_BIT = 0x08
EMBER_CHILD_FLAGS_AES_SECURITY_CAPABLE_BIT = 0x10
EMBER_CHILD_FLAG_DEVICE_IS_EXTENDED_BIT = 0x20
}

Child flags.

enum
EMBER_OPTIONS_NONE = 0x00
EMBER_OPTIONS_SECURITY_ENABLED = 0x01
EMBER_OPTIONS_ACK_REQUESTED = 0x02
EMBER_OPTIONS_HIGH_PRIORITY = 0x04
EMBER_OPTIONS_INDIRECT = 0x08
}

Message options.

enum
EMBER_MAC_ADDRESS_MODE_NONE = 0x00
EMBER_MAC_ADDRESS_MODE_SHORT = 0x02
EMBER_MAC_ADDRESS_MODE_LONG = 0x03
}

802.15.4 addressing mode.

enum
EMBER_EVENT_INACTIVE = 0
EMBER_EVENT_MS_TIME
EMBER_EVENT_QS_TIME
EMBER_EVENT_MINUTE_TIME
EMBER_EVENT_ZERO_DELAY
}

Either marks an event as inactive or specifies the units for the event execution time.

enum
@2 {
EMBER_OUTGOING_MESSAGES = 0x0001
EMBER_INCOMING_MESSAGES = 0x0002
EMBER_RADIO_IS_ON = 0x0004
EMBER_ASSOCIATING = 0x0008
EMBER_SCANNING = 0x0010
}

Define tasks that prevent the stack from sleeping.

enum
EMBER_COUNTER_PHY_IN_PACKETS
EMBER_COUNTER_PHY_OUT_PACKETS
EMBER_COUNTER_MAC_IN_UNICAST
EMBER_COUNTER_MAC_IN_BROADCAST
EMBER_COUNTER_MAC_OUT_UNICAST_NO_ACK
EMBER_COUNTER_MAC_OUT_UNICAST_ACK_SUCCESS
EMBER_COUNTER_MAC_OUT_UNICAST_ACK_FAIL
EMBER_COUNTER_MAC_OUT_UNICAST_CCA_FAIL
EMBER_COUNTER_MAC_OUT_UNICAST_RETRY
EMBER_COUNTER_MAC_OUT_BROADCAST
EMBER_COUNTER_MAC_OUT_BROADCAST_CCA_FAIL
EMBER_COUNTER_MAC_OUT_ENCRYPT_FAIL
EMBER_COUNTER_MAC_DROP_IN_MEMORY
EMBER_COUNTER_MAC_DROP_IN_FRAME_COUNTER
EMBER_COUNTER_MAC_DROP_IN_DECRYPT
EMBER_COUNTER_NWK_OUT_FORWARDING
EMBER_COUNTER_NWK_IN_SUCCESS
EMBER_COUNTER_NWK_DROP_IN_WRONG_SOURCE
EMBER_COUNTER_NWK_DROP_IN_FORWARDING
EMBER_COUNTER_UART_IN_DATA
EMBER_COUNTER_UART_IN_MANAGEMENT
EMBER_COUNTER_UART_IN_FAIL
EMBER_COUNTER_UART_OUT_DATA
EMBER_COUNTER_UART_OUT_MANAGEMENT
EMBER_COUNTER_UART_OUT_FAIL
EMBER_COUNTER_ROUTE_2_HOP_LOOP
EMBER_COUNTER_BUFFER_ALLOCATION_FAIL
EMBER_ASH_V3_ACK_SENT
EMBER_ASH_V3_ACK_RECEIVED
EMBER_ASH_V3_NACK_SENT
EMBER_ASH_V3_NACK_RECEIVED
EMBER_ASH_V3_RESEND
EMBER_ASH_V3_BYTES_SENT
EMBER_ASH_V3_TOTAL_BYTES_RECEIVED
EMBER_ASH_V3_VALID_BYTES_RECEIVED
EMBER_ASH_V3_PAYLOAD_BYTES_SENT
EMBER_COUNTER_TYPE_COUNT
}

Define the event counters that can be requested from the application using emberGetCounter()

enum
EMBER_RADIO_CONFIGURATOR
EMBER_STANDARD_PHY_2_4GHZ
EMBER_STANDARD_PHY_915MHZ
EMBER_STANDARD_PHY_863MHZ
}

Define the PHY configuration of connect stack.

enum
EMBER_CAL_TEMP_VCO = 0x00000001
EMBER_CAL_IRCAL = 0x00010000
EMBER_CAL_ALL = 0x00010001
}

Define the type of calibration requested.

enum
TX_STREAM_PN9
TX_STREAM_CW
}

Radio Stream mode.

Typedefs#

typedef uint8_t
EmberEUI64[EUI64_SIZE]

EUI 64-bit ID (IEEE 802.15.4 long address).

typedef uint16_t

IEEE 802.15.4 node ID. Also known as short address.

typedef uint16_t

IEEE 802.15.4 PAN ID.

typedef uint16_t

Message length in bytes.

typedef uint8_t

An identifier for a task.

Struct used to specify priorities for Connect's radio operations in multiprotocol.

typedef struct Event_s
typedef struct EventQueue_s

An event queue is currently just a list of events ordered by execution time.

typedef const struct EmberEventData_S

Complete events with a control and a handler procedure.

typedef uint16_t

Buffers used by the memory buffer system.

Functions#

uint8_t *
emberKeyContents(EmberKeyData *key)

This macro allows the programmer to gain access to the key data bytes of the EmberKeyData structure.

 

Enumeration Documentation#

EmberNodeType#

EmberNodeType

Define the possible types of nodes and the roles that a node might play in a network.

Enumerator
EMBER_UNKNOWN_DEVICE

Device is not in network.

EMBER_STAR_COORDINATOR

Extended star mode device: Will relay messages and can act as a parent to range extender and end device nodes. A node can be started as a coordinator using the emberFormNetwork() API.

EMBER_STAR_RANGE_EXTENDER

Extended star mode device: Will relay messages and can act as a parent to end device nodes. Joins to a coordinator. A node can be started as a range extender using the emberJoinNetwork() or emberJoinNetworkExtended() API.

EMBER_STAR_END_DEVICE

Extended star mode device: Communicates only with its parent and will not relay messages. A node can be started as an end device using the emberJoinNetwork() or emberJoinNetworkExtended() API.

EMBER_STAR_SLEEPY_END_DEVICE

Extended star mode device: An end device whose radio is turned off when not communicating to save power. The application must call emberPollForData() to receive messages. A node can be started as a sleepy end device using the emberJoinNetwork() or emberJoinNetworkExtended() API.

EMBER_DIRECT_DEVICE

Direct mode device: A device able to send and receive messages from other devices in range on the same PAN ID, with no star topology restrictions. Such device does not relay messages. A node can be started as a direct device by using the emberJoinCommissioned() API.

EMBER_MAC_MODE_DEVICE

MAC mode device: A device able to send and receive MAC-level messages. A node can be started as a MAC mode device by using the emberJoinCommissioned(), the emberJoinNetworkExtended() or the emberMacFormNetwork() API.

EMBER_MAC_MODE_SLEEPY_DEVICE

MAC mode device: A sleepy device able to send and receive MAC-level messages. The radio on the device is turned off when not communicating. The application must call emberPollForData() to receive messages. A node can be started as a sleepy MAC mode device by using the emberJoinCommissioned() API or the emberJoinNetworkExtended() API.


EmberNetworkStatus#

EmberNetworkStatus

Defines the possible join states for a node.

Enumerator
EMBER_NO_NETWORK

The node is not associated with a network in any way.

EMBER_JOINING_NETWORK

The node is currently attempting to join a network.

EMBER_JOINED_NETWORK

The node is joined to a network.

EMBER_RADIO_TEST

The node is currently using its radio for test


EmberChildFlags#

EmberChildFlags

Child flags.

Enumerator
EMBER_CHILD_FLAGS_DEVICE_IS_RANGE_EXTENDER_BIT

The child is a range extender.

EMBER_CHILD_FLAGS_DEVICE_IS_SLEEPY_BIT

The child is a sleepy end device.

EMBER_CHILD_FLAGS_HAVE_PENDING_DATA_BIT

The node has data pending for the child.

EMBER_CHILD_FLAGS_AES_SECURITY_CAPABLE_BIT

The child supports AES-based security.

EMBER_CHILD_FLAG_DEVICE_IS_EXTENDED_BIT

The child is connected through range extender.


EmberMessageOptions#

EmberMessageOptions

Message options.

Enumerator
EMBER_OPTIONS_NONE

No options.

EMBER_OPTIONS_SECURITY_ENABLED

The packet should be sent out encrypted.

EMBER_OPTIONS_ACK_REQUESTED

An acknowledgment should be requested for the outgoing packet.

EMBER_OPTIONS_HIGH_PRIORITY

The packet should be sent with high priority. High priority messages are added to the head of transmit queue, other messages are added to the tail.

EMBER_OPTIONS_INDIRECT

The packet should be sent via the indirect queue. This option only applies to nodes with EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE node type.


EmberMacAddressMode#

EmberMacAddressMode

802.15.4 addressing mode.

Enumerator
EMBER_MAC_ADDRESS_MODE_NONE

No address on this field.

EMBER_MAC_ADDRESS_MODE_SHORT

Short addressing mode.

EMBER_MAC_ADDRESS_MODE_LONG

Long addressing mode.


EmberEventUnits#

EmberEventUnits

Either marks an event as inactive or specifies the units for the event execution time.

Enumerator
EMBER_EVENT_INACTIVE

The event is not scheduled to run.

EMBER_EVENT_MS_TIME

The execution time is in approximate milliseconds.

EMBER_EVENT_QS_TIME

The execution time is in 'binary' quarter seconds (256 timer ticks).

EMBER_EVENT_MINUTE_TIME

The execution time is in 'binary' minutes (65536 timer ticks).

EMBER_EVENT_ZERO_DELAY

The event is scheduled to run at the earliest opportunity.


@2#

@2

Define tasks that prevent the stack from sleeping.

Enumerator
EMBER_OUTGOING_MESSAGES

Messages are waiting for transmission.

EMBER_INCOMING_MESSAGES

One or more incoming messages are processed.

EMBER_RADIO_IS_ON

The radio is currently powered on. On sleepy devices, the radio is turned off when not in use. On non-sleepy devices, i.e., EMBER_STAR_COORDINATOR, EMBER_STAR_RANGE_EXTENDER, EMBER_STAR_END_DEVICE, or EMBER_MAC_MODE_DEVICE, the radio is always on.

EMBER_ASSOCIATING

The node is currently trying to associate to a Connect network.

EMBER_SCANNING

The node is currently performing a MAC-level scanning procedure.


EmberCounterType#

EmberCounterType

Define the event counters that can be requested from the application using emberGetCounter()

Enumerator
EMBER_COUNTER_PHY_IN_PACKETS

Every packet that comes in over the radio (except MAC ACKs).

EMBER_COUNTER_PHY_OUT_PACKETS

Every packet that goes out over the radio (except MAC ACKs).

EMBER_COUNTER_MAC_IN_UNICAST

Incoming MAC layer unicasts.

EMBER_COUNTER_MAC_IN_BROADCAST

Incoming MAC layer broadcasts.

EMBER_COUNTER_MAC_OUT_UNICAST_NO_ACK

Outgoing MAC layer unicasts that do not require an ACK.

EMBER_COUNTER_MAC_OUT_UNICAST_ACK_SUCCESS

Outgoing MAC layer unicasts that required an ACK, for which an ACK was received (possibly after retrying).

EMBER_COUNTER_MAC_OUT_UNICAST_ACK_FAIL

Outgoing MAC layer unicasts that required an ACK, for which an ACK was never received (even after retrying).

EMBER_COUNTER_MAC_OUT_UNICAST_CCA_FAIL

Outgoing MAC layer packets which were never transmitted because clear channel assessment always returned busy.

EMBER_COUNTER_MAC_OUT_UNICAST_RETRY

Outgoing MAC layer unicast retries. This does not count the initial transmission. Note a single MAC transmission can result in multiple retries.

EMBER_COUNTER_MAC_OUT_BROADCAST

Outgoing MAC layer broadcasts

EMBER_COUNTER_MAC_OUT_BROADCAST_CCA_FAIL

Outgoing MAC layer broadcasts which were never transmitted because clear channel assessment always returned busy.

EMBER_COUNTER_MAC_OUT_ENCRYPT_FAIL

Outgoing MAC layer messages which were not transmitted due to security error e.g. because security key was not set.

EMBER_COUNTER_MAC_DROP_IN_MEMORY

Dropped incoming MAC layer packets (out of memory)

EMBER_COUNTER_MAC_DROP_IN_FRAME_COUNTER

Dropped incoming MAC layer packets (invalid frame counter)

EMBER_COUNTER_MAC_DROP_IN_DECRYPT

Dropped incoming MAC layer packets (can't decrypt)

EMBER_COUNTER_NWK_OUT_FORWARDING

Outgoing Network layer forwarded packets

EMBER_COUNTER_NWK_IN_SUCCESS

Incoming Network layer data frames correctly processed

EMBER_COUNTER_NWK_DROP_IN_WRONG_SOURCE

Dropped incoming Network layer packets (wrong source node)

EMBER_COUNTER_NWK_DROP_IN_FORWARDING

Dropped incoming Network layer packets (can't forward)

EMBER_COUNTER_UART_IN_DATA

NCP UART in data packet

EMBER_COUNTER_UART_IN_MANAGEMENT

NCP UART in management packet

EMBER_COUNTER_UART_IN_FAIL

NCP UART in frame errors

EMBER_COUNTER_UART_OUT_DATA

NCP UART out data packet

EMBER_COUNTER_UART_OUT_MANAGEMENT

NCP UART out management packet

EMBER_COUNTER_UART_OUT_FAIL

NCP UART out frame errors

EMBER_COUNTER_ROUTE_2_HOP_LOOP
EMBER_COUNTER_BUFFER_ALLOCATION_FAIL
EMBER_ASH_V3_ACK_SENT

ASHv3 ACK frame sent

EMBER_ASH_V3_ACK_RECEIVED

ASHv3 ACK frame received

EMBER_ASH_V3_NACK_SENT

ASHv3 NACK frame sent

EMBER_ASH_V3_NACK_RECEIVED

ASHv3 NACK frame received

EMBER_ASH_V3_RESEND

ASHv3 resends of frames that were not acked

EMBER_ASH_V3_BYTES_SENT

ASHv3 number of bytes sent

EMBER_ASH_V3_TOTAL_BYTES_RECEIVED

ASHv3 number of bytes received

EMBER_ASH_V3_VALID_BYTES_RECEIVED

ASHv3 number of valid bytes received

EMBER_ASH_V3_PAYLOAD_BYTES_SENT

ASHv3 number of payload bytes sent

EMBER_COUNTER_TYPE_COUNT

A placeholder giving the number of Ember counter types.


EmberPhyType#

EmberPhyType

Define the PHY configuration of connect stack.

Enumerator
EMBER_RADIO_CONFIGURATOR

Connect uses radio configurator PHY

EMBER_STANDARD_PHY_2_4GHZ

Connect is configured to use only 2.4GHz standard PHY

EMBER_STANDARD_PHY_915MHZ

Connect is configured to use only 915MHz standard PHY

EMBER_STANDARD_PHY_863MHZ

Connect is configured to use only 863MHz standard PHY


EmberCalType#

EmberCalType

Define the type of calibration requested.

Enumerator
EMBER_CAL_TEMP_VCO

Temperature calibration

EMBER_CAL_IRCAL

Image Rejection calibration

EMBER_CAL_ALL

Both calibrations


EmberTxStreamParameters#

EmberTxStreamParameters

Radio Stream mode.

Enumerator
TX_STREAM_PN9

Pseudo random PN9 byte sequence

TX_STREAM_CW

An unmodulated carrier wave


Typedef Documentation#

EmberEUI64#

typedef uint8_t EmberEUI64[EUI64_SIZE] [EUI64_SIZE]

EUI 64-bit ID (IEEE 802.15.4 long address).


EmberNodeId#

typedef uint16_t EmberNodeId

IEEE 802.15.4 node ID. Also known as short address.


EmberPanId#

typedef uint16_t EmberPanId

IEEE 802.15.4 PAN ID.


EmberMessageLength#

typedef uint16_t EmberMessageLength

Message length in bytes.


EmberTaskId#

typedef uint8_t EmberTaskId

An identifier for a task.


sl_connect_radio_priority_t#

typedef struct sl_connect_radio_priority sl_connect_radio_priority_t

Struct used to specify priorities for Connect's radio operations in multiprotocol.


Event#

typedef struct Event_s Event

EventQueue#

typedef struct EventQueue_s EventQueue

An event queue is currently just a list of events ordered by execution time.


EmberEventData#

typedef const struct EmberEventData_S EmberEventData

Complete events with a control and a handler procedure.

An application typically creates an array of events along with their handlers. The main loop passes the array to emberRunEvents() to call the handlers of any events whose time has arrived.


EmberBuffer#

typedef uint16_t EmberBuffer

Buffers used by the memory buffer system.


Function Documentation#

emberKeyContents#

uint8_t * emberKeyContents (EmberKeyData * key)

This macro allows the programmer to gain access to the key data bytes of the EmberKeyData structure.

Parameters
TypeDirectionArgument NameDescription
EmberKeyData *[in]key

A Pointer to an EmberKeyData structure.

Returns

  • uint8_t* Returns a pointer to the first byte of the key data.