Connect Version 4.1.1 (July 21, 2025) - Release Notes#

Simplicity SDK Version 2025.6.1

The Connect SDK is a complete software development suite for proprietary wireless applications that was previously part of the Proprietary SDK. Starting with the Connect SDK 4.0.0 release, Proprietary SDK is split into RAIL SDK and Connect SDK.

Connect SDK uses Silicon Labs Connect, an IEEE 802.15.4-based networking stack designed for customizable broad-based proprietary wireless networking solutions that require low power consumption and operate in either the sub-GHz or 2.4 GHz frequency bands. The solution is targeted towards simple network topologies.

Connect SDK is supplied with extensive documentation and sample applications. All examples are provided in source code within the Connect SDK sample applications.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 4.1.1#

None.

Added in 4.1.0#

  • Added Connect RAIL DMP component to support custom proprietary communication next to the Connect network. This component is able to handle additional stacks, for example a setup with Connect-BLE-RAIL DMP.

  • Connect Stack and SDK was updated to use new RAIL 2.19.0 APIs.

API Changes#

None.

Bug Fixes#

Fixed in 4.1.1#

  • Fixed an issue where sendCallbackCommand accepted NULL pointer

  • Fixed missing radio configuration file for FGM23 OPNs

  • Fixed an issue where CCA/CSMA error wasn't handled

Fixed in 4.1.0#

  • emberAfStackStatusCallback() was not called if application is RTOS.

  • RAIL Assert codes was missing from Connect Assert.

Chip Enablement#

Added in 4.1.1#

None.

Added in 4.1.0#

EFRxG29

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

Added in 4.1.1#

None.

Added in 4.1.0#

  • Added Connect RAIL DMP component to support custom proprietary communication next to Connect network, component is able to handle additional stack like a setup with Connect-BLE-RAIL DMP.

  • Connect Stack and SDK was updated to use new RAIL 2.19.0 APIs.

Enhancements#

Added in 4.1.1#

None.

Added in 4.1.0#

Updated sample applications to use sl_main instead of sl_system. main.c is now provided by platform with improved optimization.

Removed Features#

None.

Deprecated Features#

None.

API Changes#

New APIs#

Added in 4.1.1#

None.

Added in 4.1.0#

New API Signature

Deprecated API replaced by this (if any)

void rail_app_task_init(void)

void rail_app_task(void *p_arg)

void handle_os_pending(void)

void post_os_flag(void)

sl_rail_time_t calculate_transaction_time(sl_rail_handle_t rail_handle)

EmberStatus emberSetRadioRxFifo(uint16_t rxFifoSize)

Modified APIs#

None.

Removed APIs#

None.

Deprecated APIs#

None.

Bug Fixes#

Fixed in 4.1.1#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1478113 sendCallbackCommand accepted NULL pointer. None
  • Connect Stack
  • All
  • SoC, NCP mode
1474777 Missing radio configuration file for FGM23 OPNs. None
  • Connect Stack
  • All
  • SoC, NCP mode
1465062 CCA/CSMA TX Scheduling error wasn't handled in the Connect Stack. None
  • Connect Stack
  • All
  • SoC, NCP mode

Fixed in 4.1.0#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1456611 If RTOS is enabled, emberAfStackStatusCallback() is not called. None
  • Connect Stack
  • All
  • SoC, NCP mode
1402669 RAIL LIB assert codes are not coming out from the Connect Stack. None
  • Connect Stack
  • All
  • SoC, NCP mode

Chip Enablement#

Added in 4.1.1#

None.

Added in 4.1.0#

Chip Family OPNs / Boards / OPN Combinations Supported Software Variants (if applicable) Supported Modes Supported Host Interfaces
EFR32xG29
  • OPN: EFR32MG29B, EFR32BG29B
  • Boards: BRD1021A,BRD4412A,BRD4413A,BRD4414A,BRD4420A
  • External Hosts: hosts
All sample apps

    SoC

UART,EUSART,SPI

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

None.

Modified Examples#

Modified in 4.1.1#

None.

Modified in 4.1.0#

Example Name Changes Supported Software Variants if applicable Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces
Connect - NCP sample application
  • Updated to use sl_main instead of sl_system
  • Added app.c instead of main.c for custom code
Standard NCP
  • OPN: All
  • Boards: All supported boards
SPI, EUART, UART

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitations#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
652925 EFR32XG21 is not supported for “Flex (Connect) - SoC Light Example DMP” and “Flex (Connect) - SoC Switch Example” None. None.
  • EFR32XG21
  • BRD4176A,BRD4179B,BRD4180A,BRD4180B,BRD4181A,BRD4181B,BRD4181C,BRD4195A,BRD4195B,BRD4196A,BRD4196B,BRD4332A
  • SoC
1139850 DMP instabilities with EFR32XG27 None. None.
  • EFR32XG27
  • BRD2602A,BRD4109A,BRD4110A,BRD4110B,BRD4111A,BRD4111B,BRD4113A,BRD4194A
  • SoC
501561 In the Legacy HAL component, the PA configuration is hardcoded regardless of the user or boards settings. None. Until this is changed to properly pull from the configuration header, the file ember-phy.c in the user's project will need to be modified by hand to reflect the desired PA mode, voltage, and ramp time.
  • All
  • All
  • SoC
None. When running the RAIL Multiprotocol Library (used, for example, when running DMP Connect+BLE), IR Calibration is not performed because of a known issue in the RAIL Multiprotocol Library. As result, there is an RX sensitivity loss in the order of 3 or 4 dBm. None.
  • All
  • All
  • SoC
None. Updating the Baremetal sample applications to RTOS causes build errors. None.

Follow the Platforms guide sl_main Baremetal to RTOS Application Transition

  • Connect SDK Baremetal sample applications
  • All supported boards
  • SoC, NCP mode
  • UART,SPI interface

Impact of Release Changes#

Impact Statements | Migration Guide

Impact Statements#

None.

Migration Guide#

Click here for the migration guide for deprecated, removed, and modified items.

Using This Release#

What's in the Release? | Compatible Software | Installation and Use | Help and Feedback

What's in the Release?#

Connect SDK 4.1.0 showcasing the usage of the Connect stack 4.1.0 with the lates Simplicity SDK.

Compatible Software#

None.

Installation and Use#

To upgrade your existing software with this release, see instructions here.

To run your first demo, see our Getting Started Guides.

To kick start your development, see our Developer's Guide.

To learn more about the software in this release, dive into our online documentation.

For information about Secure Vault Integration, see here.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

Help and Feedback#

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.