Developing and Debugging Connect Applications#
These pages provide details on developing and debugging applications using the Connect stack. Content includes:
Architecture of the Silicon Labs Connect Stack v3.x: Describes the architecture of the Silicon Labs Connect stack v3.x an how it implements IEEE 802.15.4.
Customizing Applications with Silicon Labs Connect v3.x: Describes how to use components, callbacks, and events on top of the Gecko Platform application framework to configure features and application behavior.
Network Co-Processor Applications with Silicon Labs Connect v3.x: Describes how to run the Silicon Labs Connect stack in Network Co-Processor (NCP) mode, where the NCP runs on the EFR32 while the Host application and the Co-processor Communication daemon (CPCd) run on the Host device.
**Using Real Time Operating Systems with Silicon Labs Connect v3.x **: Describes the process to implement a Connect-based application on top of one of the supported Real Time Operating Systems (RTOS).
Energy Saving with Silicon Labs Connect v3.x: Describes the features available in Connect v3.x to reduce power consumption. Using those features is described in Building Low Power Networks with the Silicon Labs Connect Stack v3.x.
Building Low Power Networks with the Silicon Labs Connect Stack v3.x: Illustrates reducing power consumption in a Connect v3.x application using the sensor example.
Proprietary Radio Configurator Guide: Documents the Radio Configurator tool, which can be used to create customizations at the PHY level.
PHY Limitations and Timing Optimization: Connect specific recommendations on radio config customizations.
Development Tools#
Simplicity Studio and the Simplicity IDE: Simplicity Studio is the unified development environment for all Silicon Labs technologies, SoCs, and modules. It provides you with access to the target device-specific web and SDK resources, software and hardware configuration tools, and an integrated development environment (IDE) featuring industry-standard code editors, compilers, and debuggers. See the silabs.com Simplicity Studio page to download the tools and for more information.
Network Analyzer: Simplicity Studio® 5 (SSv5)'s Network Analyzer enables debugging of complex wireless systems. This tool captures a trace of wireless network activity that can be examined in detail live or at a later time. See the Network Analyzer section of the Simplicity Studio 5 User's Guide for more information.
Wireshark: Wireshark is the recommended network protocol analyzer for the use with Wi-SUN networks. Download instructions are provided for Windows/Mac users or Linux users. Simplicity Studio® 5 supports live interaction between the application running on a Silicon Labs device and Wireshark.
Energy Profiler: Simplicity Studio® 5 (SSv5)'s Energy Profiler enables you to visualize the energy consumption of individual devices, multiple devices on one target system, or a network of interacting wireless devices to analyze and improve the power performance of these systems. Real-time information on current consumption is correlated with the program counter providing advanced energy software monitoring capabilities. It also provides a basic level of integration with the Network Analyzer network analysis tool. See the Energy Profiler section of the Simplicity Studio 5 User's Guide for more information.
Simplicity Commander: Simplicity Commander is a single, all-purpose tool to be used in a production environment. It is invoked using a simple Command Line Interface (CLI) that is also scriptable. Simplicity Commander enables customers to complete essential tasks such as configuring and building applications and bootloaders and flashing images to their devices. Simplicity Commander is available through Simplicity Studio or can be downloaded through system-specific installers. The Simplicity Commander User's Guide provides more information.
Silicon Labs Configurator (SLC): SLC offers command-line access to application configuration and generation functions. Software Project Generation and Configuration with SLC-CLI provides instructions on downloading and using the SLC-CLI tool.