Full HAL functions common across all microcontroller-specific files. See Common Microcontroller Functions for documentation.
Some functions in this file return an ::sl_status_t value. See sl_status.h for definitions of all ::sl_status_t return values.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
/***************************************************************************/
#ifndef __MICRO_H__
#define __MICRO_H__
#include "micro-types.h"
#ifndef DOXYGEN_SHOULD_SKIP_THIS
// Make sure that a proper plat/micro combination was selected if we aren't
// building for a host processor
#if ((!defined(EZSP_HOST)) && (!defined(UNIX_HOST)) && (!defined(TOKEN_MANAGER_TEST)) && (!defined(SL_TOKEN_MANAGER_COMPATIBILITY)) && !defined(SL_ZIGBEE_TEST) && !defined(ZIGBEE_STACK_ON_HOST))
#ifndef PLAT
#error no platform defined, or unsupported
#endif
#ifndef MICRO
#error no micro defined, or unsupported
#endif
#ifndef PHY
#error no phy defined, or unsupported
#endif
#endif // ((! defined(EZSP_HOST)) && (! defined(UNIX_HOST)))
#endif // DOXYGEN_SHOULD_SKIP_THIS
uint8_t halGetResetInfo(void);
const char * halGetResetString(void);
#ifndef DOXYGEN_SHOULD_SKIP_THIS
#include "micro-common.h"
#if defined(CORTEXM3_EFM32_MICRO)
#include "efm32_micro.h"
#elif defined(SL_TOKEN_MANAGER_COMPATIBILITY) || defined(TOKEN_MANAGER_TEST) || defined(SL_ZIGBEE_TEST) || defined(ZIGBEE_STACK_ON_HOST)
// pass
#elif ((defined(EZSP_HOST) || defined(UNIX_HOST)))
#include "micro_host.h"
#else
#error no platform or micro defined
#endif
#endif // DOXYGEN_SHOULD_SKIP_THIS
#endif //__MICRO_H__
Functions#
Gets information about what caused the microcontroller to reset.
Calls halGetResetInfo() and supplies a string describing it.
Function Documentation#
halGetResetInfo#
uint8_t halGetResetInfo (void )
Gets information about what caused the microcontroller to reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
A code identifying the cause of the reset.
halGetResetString#
const char * halGetResetString (void )
Calls halGetResetInfo() and supplies a string describing it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Useful for diagnostic printing of text just after program initialization.
Returns
A pointer to a program space string.