License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

SPDX-License-Identifier: Zlib

The licensor of this software is Silicon Laboratories Inc.

This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.

Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:

  1. The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.

  2. Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.

  3. This notice may not be removed or altered from any source distribution.

/***************************************************************************/
void emberAfPluginPollSetShortPollInterval(uint8_t intervalQS);

void emberAfPluginPollSetLongPollInterval(uint16_t intervalS);

void emberAfPluginPollEnableShortPolling(bool enable);

Functions#

void

Set the short poll interval.

void

Set the long poll interval.

void

Enable/disable short polling.

Function Documentation#

emberAfPluginPollSetShortPollInterval#

void emberAfPluginPollSetShortPollInterval (uint8_t intervalQS)

Set the short poll interval.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]intervalQS

The short poll interval in quarter seconds.


Definition at line 68 of file /mnt/raid/workspaces/ws.pFXAwOgGO/overlay/gsdk/protocol/flex/poll/poll.h

emberAfPluginPollSetLongPollInterval#

void emberAfPluginPollSetLongPollInterval (uint16_t intervalS)

Set the long poll interval.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]intervalS

The long poll interval in seconds.


Definition at line 74 of file /mnt/raid/workspaces/ws.pFXAwOgGO/overlay/gsdk/protocol/flex/poll/poll.h

emberAfPluginPollEnableShortPolling#

void emberAfPluginPollEnableShortPolling (bool enable)

Enable/disable short polling.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable

If this parameter is true, short polling is enabled. Otherwise, the node switches back to long polling.


Definition at line 81 of file /mnt/raid/workspaces/ws.pFXAwOgGO/overlay/gsdk/protocol/flex/poll/poll.h