See Standalone for documentation.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef __BOOTLOADER_STANDALONE_H__
#define __BOOTLOADER_STANDALONE_H__
uint16_t halGetStandaloneBootloaderVersion(void);
#define NO_BOOTLOADER_MODE 0xFF
#define STANDALONE_BOOTLOADER_NORMAL_MODE 1
#define STANDALONE_BOOTLOADER_RECOVERY_MODE 0
EmberStatus halLaunchStandaloneBootloader(uint8_t mode);
#endif //__BOOTLOADER_STANDALONE_H__
Macros#
Define a numerical value for NO BOOTLOADER mode. In other words, the bootloader should not be run.
Define a numerical value for the normal bootloader mode.
Define a numerical value for the recovery bootloader mode.
Functions#
Detects if the standalone bootloader is installed, and if so returns the installed version.
Quits the current application and launches the standalone bootloader (if installed). The function returns an error if the standalone bootloader is not present.
Function Documentation#
halGetStandaloneBootloaderVersion#
uint16_t halGetStandaloneBootloaderVersion (void )
Detects if the standalone bootloader is installed, and if so returns the installed version.
N/A |
A returned version of 0x1234 would indicate version 1.2 build 34
Returns
BOOTLOADER_INVALID_VERSION if the standalone bootloader is not present, or the version of the installed standalone bootloader.
38
of file /Users/vihuszar/Git/EmbeddedSoftware/super/platform/base/hal/micro/bootloader-interface-standalone.h
halLaunchStandaloneBootloader#
EmberStatus halLaunchStandaloneBootloader (uint8_t mode)
Quits the current application and launches the standalone bootloader (if installed). The function returns an error if the standalone bootloader is not present.
N/A | mode | Controls the mode in which the standalone bootloader will run. See the bootloader Application Note for full details. Options are:
|
Both modes also allow an image transfer to begin via serial xmodem.
Returns
An EmberStatus error if the standalone bootloader is not present, or EMBER_SUCCESS.
71
of file /Users/vihuszar/Git/EmbeddedSoftware/super/platform/base/hal/micro/bootloader-interface-standalone.h