Release Notes for Gecko OS Edition 2
Gecko OS 2 evolved from ZentriOS WL 1.5. To update from ZentriOS WL to Gecko OS, see Updating to Gecko OS. This page also lists differences between ZentriOS WL and Gecko OS 2.
We recommend upgrading to the latest version of Gecko OS 2. See release notes for the latest version of Gecko OS 2.
Version String
Note that the version string changes format in Gecko OS 2. The ZentriOS WL 1.5 version string is similar to:
ZENTRI-AMW007-1.5.0.13, 2018-09-03T06:06:14Z, ZentriOS-WL-1.5.0.13, Board:AMW007-E03.2
The Gecko OS 2 version string is similar to:
SILABS-AMW007-2.1.5, Gecko OS-2.1.5, AMW007-W00001
The version number in Gecko OS 2 contains major version, minor version, and patch version, e.g. 2.1.5
. It does not contain a release candidate version number.
Gecko OS 2.0.4
Last Updated: April, 2019
Gecko OS 2.0 is a pre-release of Gecko OS 2.
The changes shown below are differences between Gecko OS 2.0 and ZentriOS WL 1.5.
Commands Changed
Change | Description |
---|---|
dms_activate | The dms activate command has been renamed to dms_activate. |
dms_claim | The dms claim command has been renamed to dms_claim. |
Variables Changed
Change | Description |
---|---|
broadcast.udp.remote_port | The broadcast.udp.port variable has been renamed to broadcast.udp.remote_port. |
system.cmd.format | The system.cmd.mode variable has been renamed to system.cmd.format. |
Variables Added
Change | Description |
---|---|
hboot.filename | The hboot.filename variable supports the host boot feature. |
hboot.gpio | The hboot.gpio variable supports the host boot feature. |
Variables Removed
Change | Description |
---|---|
bus.command.rx_bufsize | The bus.command.rx_bufsize variable has been removed. |
bus.command.tx_bufsize | The bus.command.tx_bufsize variable has been removed. |