Networking and Security
Gecko OS includes a full IPv4 networking stack and SSL/TLS security suite that supports a range of popular networking protocols including TCP, UDP, DNS, DHCP. Additional network application libraries are provided for native HTTP/S and secure cloud access.
The Procedure for Joining a WLAN Network is described in detail below.
For each networking client and server there are configuration variables, and commands and procedures to start and stop the client or server.
- DHCP client
- DHCP server
- DNS client
- DNS server
- HTTP client
- HTTP server with RESTful API
- HTTPS client
- HTTPS server
- NTP client
- TCP client
- TCP server
- SMTP Client
- TLS 1.0 - 1.2
- SSL/TLS client
- SSL/TLS server
- UDP client
- UDP server
- WebSocket client
- WebSocket server
When a network connection is established, Gecko OS opens a network stream to write and read data. See Network Connections and Streams.
Other network features include ...
- Network status indication using GPIOs
- Remote Terminal Access
- Broadcast status announcement
- Captive Portal
Security features include ...
- SSL/TLS client and server
- HTTPS webserver
- HTTPS file upload and download
- CA certificate store
Procedure for Joining a WLAN Network
Setting WLAN Variables
To join a WLAN network, you need to pre-set some variables. In all cases, save the variable values to NVM with the save command.
- Set the wlan.ssid and wlan.passkey variables:
- Optionally set wlan.bssid and wlan.security
- to find the WLAN SSID, you can use the network_up -s or scan commands
- After the network credentials are
set
, save them to NVM with the save command
- If you want Gecko OS to attempt to join the nework on boot, set wlan.auto_join.enabled to true. You can also specify wlan.auto_join.retry_delay and wlan.auto_join.retries
- To control the timeout on join attempts, specify wlan.join.timeout. To control the number of retries Gecko OS attempts, set wlan.join.retries
- If you want to specify static IP address, DNS and gateway values, set the wlan.static.* variables
Starting the Network Up Sequence
To start the network up sequence, do one of the following:
- Set wlan.auto_join.enabled and reboot/powerup
- Invoke the network_up command
- Invoke any command that requires the network interface
The Network Up Sequence
The following diagram shows the network up sequence. Click to enlarge.
The auto join retry count is set to zero at the beginning of the entire sequence.
Circled step numbers in the diagram above correspond to the numbered steps in the network up sequence below:
check retry count:
- IF join attempt count >= wlan.join.retries, GOTO step 6: join attempt failed.
- ELSE continue to next step.
first time?:
- IF network has previously been joined successfully: skip probe and attempt to join with existing network details. GOTO step 4: attempt to join.
- ELSE continue to next step.
probe for network details:
- IF join attempt count == 1, Gecko OS probes for network with wlan.bssid and/or wlan.security if set, else wlan.ssid. Probing uses all wlan.scan.* variables
- IF probe NOT successful, GOTO step 6: join attempt failed.
- ELSE continue to next step: attempt to join
attempt to join: Gecko OS attempts to associate using network details found in probe or in stored in previous successful join:
- IF Gecko OS has network details (i.e. bssid, channel and security), Gecko OS attempts to associate to network, with timeout after wlan.join.timeout ms.
- IF association successful, goto step 5, get IP address, DNS and gateway values
- ELSE IF association failed, Gecko OS failed to associate to network. Increment join retry count and GOTO step 1
- ELSE if network not found in probing, the join attempt failed. GOTO step 6.
- IF Gecko OS has network details (i.e. bssid, channel and security), Gecko OS attempts to associate to network, with timeout after wlan.join.timeout ms.
get IP address, DNS and gateway values:
- IF the device successfully joins the network:
- IF wlan.dhcp.enabled is TRUE, Gecko OS attempts to get an IP address from the AP, timeout after wlan.dhcp.timeout seconds
- ELSE IF wlan.dhcp.enabled is FALSE then Gecko OS uses the wlan.static.* variables, which you should preset to appropriate values
network up
sequence successful. GOTO step 7: network up sequence complete.
- ELSE the join attempt failed. GOTO step 6, join attempt failed.
- IF the device successfully joins the network:
join attempt failed: Try again if auto join enabled, WLAN interface not just forced down, and auto join retries not exceeded:
- IF the join attempt failed AND wlan.auto_join.enabled is TRUE, AND auto join retry count < wlan.auto_join.retries, Gecko OS waits wlan.auto_join.retry_delay seconds and starts the
network up
sequence again. Increment auto join retry count and join retry count, then GOTO step 1. - ELSE GOTO step 7.
- IF the join attempt failed AND wlan.auto_join.enabled is TRUE, AND auto join retry count < wlan.auto_join.retries, Gecko OS waits wlan.auto_join.retry_delay seconds and starts the
network up sequence complete
Gecko OS has either succeeded or failed in joining the network. You can check wlan.join.result to determine the final result of the network_up sequence.
DHCP Client
The Gecko OS DHCP client obtains an IP address from the WLAN DHCP server when the network is brought up with the wlan
interface.
Configure the DHCP client with the variables:
Bring the network up by issuing any command that requires the network, or use the command:
DHCP Server
The Gecko OS DHCP server supplies IP addresses to clients connecting to the soft AP when the network is brought up with the softap
interface.
Configure the DHCP server with the variables:
The soft AP starts on reboot when configured to auto-start with the softap.auto_start variable.
You can bring up the soft AP with the network_up command. Either specify the softap
interface, or set the network.default_interface variable to softap
.
The soft AP starts automatically when you use Web Setup.
DNS Client
The DNS Client works with all the network protocols, including HTTP, TCP and UDP.
The network.dns.timeout variable controls the length of time Gecko OS waits while attempting to resolve a hostname via DNS.
The wlan.network.dns variable returns a list of addresses currently in use by the WLAN interface.
DNS Server
DNS Server features are available for the Soft AP interface.
Configuration options for the soft AP DNS server are:
The setup.web.url variable defines a list of URLs that clients can use to connect to the Gecko OS Web App.
HTTP Client
The HTTP Client consists of a group of commands for HTTP methods:
For a secure TLS transaction, the url scheme specified with the command must be https
. See HTTPS Client.
The http_get
, http_post
and http_head
commands have an option to queue the request, prior to sending. While the request is queued, use the http_add_header
to add custom headers as required, as shown in the example below. Use the stream_write command to add data to the body of a POST request.
Use the http_read_status
command to read the HTTP response after a request is completed.
Connection timeout for the HTTP client commands is controlled by the tcp.client.connect_timeout variable.
Stream Type: HTTP
. See Network Connections and Streams, Stream Types.
HTTP POST Example
The following (fictitious) HTTP POST example shows how to post data to an HTTP web server using the Gecko OS HTTP API. The HTTP body data posted in this example is a small piece of JSON (sent using stream_write 0 7
). Since the -o
option is used with the http_post command, a connection stream to the HTTP server is opened, but the HTTP POST is queued locally on the module.
Queuing the HTTP POST locally provides the ability to add HTTP headers using the http_add_header command, and to post data in the HTTP body using the stream_write command. Once all headers and body data are queued, the HTTP POST is sent to the server and completed using the http_post command.
Any response data received from the server may be read using stream_read.
> http_post -o example.com/hello application/json
[2019-01-01 | 19:40:23: Opening: example.com]
Request POST /hello
Connecting (HTTP): example.com:80
[2019-01-01 | 19:40:23: Opened: 0]
0
> stream_write 0 7
... JSON data goes here ...
Success
> http_read 0
HTTP response: 200
Chunked response
200
> stream_read 0 1000
{
"response": "howdy!"
}
> stream_close 0
Closing: 0
[2019-01-01 | 19:40:40: Closed: 0]
Success
HTTP Client File Upload and Download
The HTTP Client feature includes commands to handle file upload and download, between the Gecko OS device file system and an HTTP/S host:
The http_upload
and http_download
commands use HTTP POST requests in the background.
For a secure TLS transaction, the url scheme specified with the command must be https
.
See:
HTTP Client Native API
See Native API HTTP Client group.
HTTP Server with RESTful API
The Gecko OS HTTP webserver may be configured to run as a service on either the softAP or WLAN interface.
The server supports HTTP Basic Authentication with (or without) HTTPS security.
There is no network stream associated with the HTTP server. An HTTP client issues a request and the HTTP server sends a response. The client and server do not read or write data outside the request.
Gecko OS provides a simple RESTful API on top of the HTTP server. The API allows for a remote HTTP(S) client to issue any Gecko OS command. The result of the command is returned in a simple JSON format.
The RESTful API can be used in a number of ways:
- GET and POST requests - see the HTTP Server RESTful API app note
- The Gecko OS Web App provides complete control of a module via the RESTful API
- Javascript: for more sophisticated scripting, the Gecko OS JavaScript API provides a JavaScript wrapper around the HTTP server REST API
- Python: the geckoospy module provides a Python wrapper around the HTTP server RESTful API.
The HTTP Server is configured with the following variables:
- http.server.api_enabled
- http.server.cors_origin
- http.server.denied_filename
- http.server.enabled
- http.server.interface
- http.server.max_clients
- http.server.notfound_filename
- http.server.password
- http.server.port
- http.server.root_filename
- http.server.tls_cert
- http.server.tls_enabled
- http.server.tls_key
- http.server.tls_verify_peer
- http.server.username
A client can use the RESTful API to issue Gecko OS commands and receive responses, and also for retrieval of module log messages.
The available requests are as follows:
GET /command
POST /command
GET /log
POST /stream
See the HTTP Server RESTful API application note for low-level examples.
The Gecko OS Web App provides a complete demonstration of the HTTP Server RESTful API, and can be customized as required. See Customizing the Gecko OS Web App.
Notes
- Request size is limited to 4 KBytes, not including headers.
- The HTTP server does not check headers, other than the client's origin header. See CORS (Cross Origin Resource Sharing).
Command Request/Response
The API supports either a simple GET request or a slightly more complex POST request.
GET Request
GET /command/<Gecko OS command>
POST Request
POST /command
{
"flags" : <flags>,
"command" : "<Gecko OS command>",
"data" : "<command data>"
}
where:
<flags>
0x01
- "command" field is base64 encoded0x02
- base64 encode response data0x04
- "data" field is base64 encoded
<Gecko OS command>
- any Gecko OS serial command<command data>
- optional, specific to certain Gecko OS commands that require additional data (write, file_create, etc)
With the REST API, the procedure for issuing commands is:
- Open HTTP socket to server
- POST JSON formatted command to device
- Device processes request
- Device returns a JSON formatted response
- HTTP connection closed
To issue another command, repeat steps 1-5.
HTTP Response Codes
200
- the command transaction executed successfully400
- malformed request500
- server error
Response body
{
"id" : <unique id>,
"code" : <response code>,
"flags" : <flags>,
"response" : "<command response>"
}
where:
<unique id>
- unique id given to each command.<response code>
- the Gecko OS command response code.<flags>
0x01
- the command response is base64 encoded
<command response>
- the command response data
Log Request/Response
The API also buffers log messages. This is the request to retrieve the log messages.
GET Request
GET /log
HTTP Response Codes
200
- the command transaction executed successfully400
- malformed request
Response
{
"logs" : [ "<log data>", "<log data>", ....] }
}
Note: the log buffer has limited space. Older logs are replaced by newer ones. This should be called periodically to avoid losing logs.
HTTP Response Codes
200
- the command transaction executed successfully400
- malformed request404
- no available stream handles
HTTP Server Security and Authorization
The HTTP server is secured using HTTP Basic Authentication. This requires that a client supplies a username and password. Note that the username/password are sent in the HTTP request header which is encrypted only if the HTTP request itself is encrypted.
Client Authorization
The HTTP Basic Authentication client authorization feature is enabled when both the http.server.username and http.server.password variables are set.
When the HTTP Server username/password settings are set, authorization is required to access certain files and api commands.
The client must supply a username and password that matches the http.server.username and http.server.password variables.
If authorization fails the Gecko OS HTTP Server returns:
- the
webapp/unauthorized.html
page. This can be customized by uploading a newwebapp/unauthorized.html
page to the device. - a
401
error code - the following response header:
WWW-Authenticate: Basic realm=Gecko OS
Protecting or Securing a File
When client authorization is enabled, authorization is required to download all files (except unprotected files).
To unprotect a file, the -u
(unprotected) flag must be explicitly specified when the file is created using the file_create or http_download commands.
When client authorization is disabled, all files may be downloaded from the Gecko OS web server.
Securing the REST API, Whitelisting API Calls
When the authorization feature is enabled all REST API calls require authorization. It is possible to 'whitelist' certain API calls.
This is done by creating the file: http_whitelist.csv
which contains a comma separated list of REST API calls that do not require authorization.
This file also supports a trailing wildcard character *
. Some examples of this file are as follows:
- Whitelist ALL REST API calls:
*
- Whitelist the
log
andstream
API calls:
/log,/stream
- Whitelist all
get wlan
calls:
get wl*
- Whitelist the
help variables
andhelp commands
commands:
help variables,help commands
- Whitelist
/stream
,help
, and all getters:
/stream,help *,get *
CORS (Cross Origin Resource Sharing)
The Gecko OS HTTP server supports CORS (Cross-Origin Resource Sharing).
The http.server.cors_origin variable allows you to specify origins for which the same-origin policy is relaxed.
This allows control of the module, via the HTTP server, from a remote site provided the module has originally been set up with a http.server.cors_origin domain that allows access from that site. Via the Gecko OS HTTP server Gecko OS JavaScript API, the remote site can issue all Gecko OS commands, including reboot.
Setting the http.server.cors_origin results in the Gecko OS HTTP server inserting a corresponding CORS Access-Control-Allow-Origin (ACAO) response header into resources it delivers.
It also results in the Gecko OS HTTP server responding to an OPTION
request with a set of options supporting remote control.
When a client connects to the HTTP server, the server validates the client's 'origin' header against http.server.cors_origin. If the origin does not match http.server.cors_origin then the HTTP server immediately terminates the connection.
HTTP Server Security Variables
The variables for managing HTTP Basic Authentication are:
The variable for managing CORS is:
HTTPS Client
HTTPS client commands include:
The HTTP client commands use TLS when the URL supplied has the scheme https
.
The TLS CA certificate is supplied as a command argument or by default configured with the variables:
- network.tls.ca_cert
- network.tls.ca_cert_verify_enabled
- network.tls.client_cert
- network.tls.client_key
- network.tls.handshake_timeout
- network.tls.version
HTTPS Server
The HTTP Server becomes an HTTPS Server when TLS is configured for HTTP Server with the variables:
- http.server.tls_cert
- http.server.tls_client_log
- http.server.tls_enabled
- http.server.tls_key
- http.server.tls_log_clients
- http.server.tls_verify_peer
All the features described above for the HTTP Server are supported for the HTTPS Server.
NTP Client
Network Time Management
Gecko OS devices can obtain time data from an NTP (Network Time Protocol) server.
Configure NTP with the variables:
Time related variables are:
If NTP is enabled, time.last_set returns the seconds since the time was last set by NTP.
To read the time, get time.rtc and to determine the time zone, get time.zone.
SMTP Client
The SMTP Client allows Gecko OS devices to send email messages via an external SMTP server.
Configure email via SMTP with the variables:
Send email with the command:
To use TLS with the SMTP client, set the value of network.tls.ca_cert.
See the Sending a Secure SMTP Email application note.
SMTP Native API
TCP Client
Configure the TCP client with the variables:
- tcp.client.auto_interface
- tcp.client.auto_retries
- tcp.client.auto_start
- tcp.client.connect_timeout
- tcp.client.local_port
- tcp.client.remote_host
- tcp.client.remote_port
- tcp.client.retries
- tcp.client.retry_period
- tcp.client.tls_enabled
Start the TCP client with the command:
Stream Type: TCPC
. See Network Connections and Streams, Stream Types.
TCP Client Auto Connect
To connect automatically to a remote host when the network is brought up, configure TCP client auto-connect with the variables:
- tcp.client.auto_interface
- tcp.client.auto_retries
- tcp.client.auto_start- tcp.client.remote_host
- tcp.client.remote_port
To auto start with a TLS connection, set tcp.client.tls_enabled = TRUE. See TLS Client.
TCP Client Connection Retry Sequence
The TCP client connection retry sequence is shown in the following diagram. Click to enlarge:
TCP Server
Configure the TCP server with the variables:
- tcp.server.auto_interface
- tcp.server.auto_start
- tcp.server.connected_gpio
- tcp.server.data_gpio
- tcp.server.idle_timeout
- tcp.server.max_clients
- tcp.server.port
- tcp.server.tls_cert
- tcp.server.tls_enabled
- tcp.server.tls_key
- tcp.server.tls_verify_peer
Start and stop the TCP server with the TCP server command:
Stream Type: TCPS
. See Network Connections and Streams, Stream Types.
To use the TCP server with TLS, configure the tcp.server.tls*
variables and use the tls_server command. See TLS Server.
TLS 1.0-1.2 Support
Gecko OS supports TLS 1.0 to TLS 1.2.
For a full description of TLS errors and the commands that use TLS, see TLS Errors.
Supported TLS Cipher Suites
Gecko OS supports the following Cipher Suites for TLS 1.0 - 1.2:
OpenSSL Name | Key Exchange | Encryption | Hashing Algorithm |
---|---|---|---|
MBEDTLS_TLS_ECDHE_ECDSA_WITH_AES_128_GCM_SHA256 | ECDHE | AES-128 | SHA-256 |
MBEDTLS_TLS_ECDHE_RSA_WITH_AES_128_GCM_SHA256 | ECDHE | AES-128 | SHA-256 |
MBEDTLS_TLS_ECDHE_ECDSA_WITH_AES_128_CBC_SHA256 | ECDHE | AES-128 | SHA-256 |
MBEDTLS_TLS_ECDHE_ECDSA_WITH_AES_128_CBC_SHA | ECDHE | AES-128 | SHA-1 |
MBEDTLS_TLS_ECDHE_ECDSA_WITH_AES_256_CBC_SHA | ECDHE | AES-256 | SHA-1 |
MBEDTLS_TLS_ECDHE_RSA_WITH_AES_128_CBC_SHA | DHE RSA | AES-128 | SHA-1 |
MBEDTLS_TLS_DHE_RSA_WITH_AES_256_CBC_SHA256 | DHE RSA | AES-256 | SHA-256 |
MBEDTLS_TLS_DHE_RSA_WITH_AES_256_CBC_SHA | DHE RSA | AES-256 | SHA-1 |
MBEDTLS_TLS_RSA_WITH_AES_256_CBC_SHA256 | RSA | AES-256 | SHA-256 |
MBEDTLS_TLS_RSA_WITH_AES_256_CBC_SHA | RSA | AES-256 | SHA-1 |
MBEDTLS_TLS_RSA_WITH_AES_128_CBC_SHA256 | RSA | AES-128 | SHA-256 |
MBEDTLS_TLS_RSA_WITH_AES_128_CBC_SHA | RSA | AES-128 | SHA-1 |
Acronyms Used in Above Table
- AES - Advanced Encryption Standard
- CBC - Cipher Block Chaining
- CCM - Cipher Block Chaining - Message Authentication Code
- DH - Diffie-Hellman
- DHE - Diffie-Hellman Ephemeral
- EC - Elliptic Curve
- ECDHE - Elliptic Curve Diffie-Hellman Exchange
- ECDSA - Elliptic Curve Digital Signature Algorithm
- GCM - Galois/Counter Mode
- RSA - Rivest, Shamir, Adleman
- SHA - Secure Hash Algorithm
TLS Memory Requirements
Increasing Available Memory for TLS
TLS connections require a considerable amount of RAM. Low memory may result in TLS errors such as TLS malloc failed
.
To establish a TLS connection, other memory intensive features may need to be disabled. You can return the device to the default state with a factory reset.
TLS Errors
TLS Error Format
In the event of TLS failure, the response includes an error message with a format similar to the following:
Error with TLS handshake: <error code> (state: <tls state>, code: <internal error code>)
where:
<error code>
- general error code. See the TLS Error Codes table below.<tls state>
- the current parsing state when the error occurred. See the TLS States table below.<internal error code>
- internal error code used for debugging.
TLS Error Example
> http_get https://google.com
[2019-01-01 | 02:50:33: Opening: https://google.com]
Request GET /
Connecting (https): google.com:443
Starting TLS
TLS malloc failed
Error with TLS handshake: 5035
[2019-01-01 | 02:50:33: Open failed]
Command failed
TLS Error Codes
Code | Error |
---|---|
2 | TIMEOUT |
5001 | RECEIVE_FAILED |
5002 | ALERT_NO_CERTIFICATE |
5003 | ERROR_OUT_OF_MEMORY |
5004 | ERROR_FEATURE_UNAVAILABLE |
5005 | ERROR_BAD_INPUT_DATA |
5006 | ERROR_INVALID_MAC |
5007 | ERROR_INVALID_RECORD |
5008 | ERROR_INVALID_MODULUS_SIZE |
5009 | ERROR_UNKNOWN_CIPHER |
5010 | ERROR_NO_CIPHER_CHOSEN |
5011 | ERROR_NO_SESSION_FOUND |
5012 | ERROR_NO_CLIENT_CERTIFICATE |
5013 | ERROR_CERTIFICATE_TOO_LARGE |
5014 | ERROR_CERTIFICATE_REQUIRED |
5015 | ERROR_PRIVATE_KEY_REQUIRED |
5016 | ERROR_CA_CHAIN_REQUIRED |
5017 | ERROR_UNEXPECTED_MESSAGE |
5018 | ERROR_FATAL_ALERT_MESSAGE |
5019 | ERROR_PEER_VERIFY_FAILED |
5020 | ERROR_PEER_CLOSE_NOTIFY |
5021 | ERROR_BAD_HS_CLIENT_HELLO |
5022 | ERROR_BAD_HS_SERVER_HELLO |
5023 | ERROR_BAD_HS_CERTIFICATE |
5024 | ERROR_BAD_HS_CERTIFICATE_REQUEST |
5025 | ERROR_BAD_HS_SERVER_KEY_EXCHANGE |
5026 | ERROR_BAD_HS_SERVER_HELLO_DONE |
5027 | ERROR_BAD_HS_CLIENT_KEY_EXCHANGE |
5028 | ERROR_BAD_HS_CERTIFICATE_VERIFY |
5029 | ERROR_BAD_HS_CHANGE_CIPHER_SPEC |
5030 | ERROR_BAD_HS_FINISHED |
5031 | HANDSHAKE_TIMEOUT |
5032 | HANDSHAKE_ERROR |
5033 | INIT_FAIL |
5034 | BAD_MESSAGE |
5035 | UNTRUSTED_CERTIFICATE |
5036 | EXPIRED_CERTIFICATE |
5037 | CERTIFICATE_NAME_MISMATCH |
5038 | CERTIFICATE_REVOKED |
5039 | NO_DATA |
5040 | ERROR_UNSUPPORTED_EXTENSION |
TLS States
Code | TLS State |
---|---|
0 | SSL_HELLO_REQUEST |
1 | SSL_CLIENT_HELLO |
2 | SSL_SERVER_HELLO |
3 | SSL_SERVER_CERTIFICATE |
4 | SSL_SERVER_KEY_EXCHANGE |
5 | SSL_CERTIFICATE_REQUEST |
6 | SSL_SERVER_HELLO_DONE |
7 | SSL_CLIENT_CERTIFICATE |
8 | SSL_CLIENT_KEY_EXCHANGE |
9 | SSL_CERTIFICATE_VERIFY |
10 | SSL_CLIENT_CHANGE_CIPHER_SPEC |
11 | SSL_CLIENT_FINISHED |
12 | SSL_SERVER_CHANGE_CIPHER_SPEC |
13 | SSL_SERVER_FINISHED |
14 | SSL_FLUSH_BUFFERS |
15 | SSL_HANDSHAKE_OVER |
TLS Client
TLS client commands include:
See also HTTPS Client.
TLS details must be supplied as a command argument or configured with the variables:
To manually initiate a TLS connection with the TCP client, use the tls_client command.
To auto-start the TCP client with TLS, set:
- tcp.client.auto_start = TRUE
- tcp.client.tls_enabled = TRUE
The TCP client, with TLS enabled, has the features described in the TCP Client documentation.
Stream Type: TLSC
. See Network Connections and Streams, Stream Types.
OTA always uses TLS.
Commands that use TLS respond to TLS failure with a specially formatted error message. See TLS Error Format.
Connect timeout for the TLS client command is controlled by the tcp.client.connect_timeout variable.
TLS Server
Configure TLS Server with the variables:
See commands:
The TLS server has all the features described in TCP Server.
Stream Type: TLSS
. See Network Connections and Streams, Stream Types.
UDP Client
Configure the UDP client with the variables:
- udp.client.auto_interface
- udp.client.auto_retry
- udp.client.auto_start
- udp.client.remote_host
- udp.client.remote_port
Start the UDP client with the command:
Stream Type: UDPC
. See Network Connections and Streams, Stream Types.
UDP Client Auto Connect
Configure the UDP client auto-connect with the variables:
- udp.client.auto_interface
- udp.client.auto_retry
- udp.client.auto_start
- udp.client.remote_host
- udp.client.remote_port
UDP Server
Configure the UDP server with the variables:
- udp.server.auto_interface
- udp.server.auto_start
- udp.server.data_gpio
- udp.server.lock_client
- udp.server.port
- udp.server.remote_host
- udp.server.remote_port
Start and stop the UDP server with the command:
The udp_server has subcommands to read
and write
. These are equivalent to the stream read and write commands, with the added option of determining the client address and port.
The UDP server uses a single stream for multiple clients. Using the stream read and write commands applies to all clients. Using the UDP server subcommands allows writing to and reading from a specific client.
Stream Type: UDPS
. See Network Connections and Streams, Stream Types.
UDP Server Auto Connect
Configure the UDP server auto-connect with the variables:
WebSocket Client
Configuration options for the websocket client include:
- The ioconn.protocol option
web
allows a GPIO-controlled websocket connection. - The system.oob.gpio event
websocket.client.data_gpio
can provide data ready information for multiple websocket clients.
The command to invoke the websocket client is:
See the websocket_client documentation for details on the websocket message format.
The websocket client supports TLS via the websocket URL scheme and the websocket_client cert filename
argument.
The websocket_client -g
option configures a data ready GPIO for a single websocket.
Read from the Websocket with stream_read.
Write to the Websocket with stream_write.
To send a WebSocket ping frame as a keepalive, use the stream_write with the -p
option.
To send data chunks as continuation frames, use the stream_write with the -f
option.
Stream Type: WEBC
. See Network Connections and Streams, Stream Types.
WebSocket Server
The WebSocket protocol provides full-duplex communication channels over a single TCP connection. Gecko OS WebSocket server support requires the HTTP Server. The HTTP REST API includes WebSocket API calls.
Websocket server CORS policy is discussed in HTTP Server, CORS (Cross Origin Resource Sharing).
Configuration variables are:
Stream Type: WEBS
. See Network Connections and Streams, Stream Types.
WebSocket Stream
To open a WebSocket, issue the API call POST /stream
to the Gecko OS HTTP server. Gecko OS opens a WebSocket and creates a network stream. An MCU can read/write data using the Gecko OS stream_read and stream_write commands. See Network Connections and Streams.
POST /stream
<raw data .... >
See HTTP Server Simple WebSocket Demonstration.
WebSocket URI
When connecting to a Command API WebSocket server, the WebSocket URI is /stream
.
When connecting to an App WebSocket server, the WebSocket URI is /zapstreams
.
When connecting to a WebSocket command stream, the WebSocket URI is /cmdstream
. See WebSocket Command Stream below.
WebSocket Command Stream
The WebSocket command stream lets you issue commands to your Gecko OS device via a WebSocket from a remote host.
The WebSocket command stream is complementary to the REST API. It uses the WebSocket protocol and the /cmdstream
route.
When issuing a command via the WebSocket command stream, the sequence is:
- Open WebSocket stream with HTTP server via
ws://<host>/cmdstream
- Issue msgpack formatted message to Gecko OS device. For details of msgpack format, see http://msgpack.org/.
- Gecko OS device processes command message
- Gecko OS device returns msgpack formatted response
To issue another command repeat steps 2-4.
You need to import a msgpack library into your webpage or application to use the WebSocket command stream.
The command message is in the following form:
{
"command" : "<Gecko OS command>",
"data" : "<command data>",
"id" : <command id>
}
where:
<command>
- any Gecko OS string command<command data>
- addition data as required for certain commands such as write and file_create.<id>
- optional Unique command ID
The response from Gecko OS is of the following form:
{
"id" : <command id>,
"code" : <response code>,
"response" : "<command response>"
}
where:
<command id>
- ID received from command (if and ID was provided)<response code>
- the Gecko OS command response code.<command response>
- the command response data
Network Connections and Streams
Streams are associated with:
- network connections, including HTTP, HTTPS, TCP, TLS, WebSocket and UDP client and server connections
- open files
- SPI serial connections
- I2C serial connections
- the command buffering feature used in some serial apps. See system.cmd.buffered.
When Gecko OS opens a network connection, file, or serial connection, it returns a stream handle. The stream commands act on a stream handle to perform actions such as read, write, poll and close. You can list open streams. Each stream has a specific type. See Stream Types.
Stream Handles
When a stream is open, it is assigned a handle number. This handle is used to read/write/poll/close the stream.
Stream Commands
Refer to the following stream commands to use the stream handle:
- stream_list - list open streams by stream handle, with stream type and related information
- stream_read - read stream specified by stream handle
- stream_write - write to stream specified by stream handle
- stream_close - close stream specified by stream handle
- stream_poll - determine status of stream specified by stream handle, or all streams
Use the stream_list command to view open streams. For example:
> stream_list
! # Type Info
# 0 TCPS 10.5.6.146:3000 10.5.6.131:63835
# 1 UDPC 107.170.222.80:50007 (15672)
# 2 TCPC 107.170.222.80:50007 (13171)
# 3 FILE webapp/unauthorized.html-1.0.1.3 (9530, 0)
# 4 FILE favicon.ico.gz-1.0.1.3 (733, 0)
# 5 FILE webapp/gecko-os.css.gz-1.0.1.3 (22670, 0)
>
Ready
>
Serial STREAM Mode
In serial STREAM mode, a single network connection (TCP/TLS/UDP/WebSocket client/server) streams to the serial bus. No stream read or write commands are required, as data flows automatically between the serial bus and the open stream. See Serial Interface, Stream Mode.
STREAM mode does not support the following stream types:
FILE
SPI
I2C
Note: When in STREAM mode, a TCP/TLS/WebSocket server is limited to one client connection.
STREAM mode is assigned to the auto-start network stream that opens first.
The STREAM mode enabled stream appears in the stream list. Reading and writing data to the stream is not permitted.
Note: If you create a STREAM mode application with multiple network streams set to auto start, then it may not be possible to predict which will open first and which network connection is streaming. We recommend using only one auto-start network connection when booting to STREAM mode.
Stream Limitations
Gecko OS supports up to 8 simultaneous network streams. Any TCP, Websocket or HTTP stream can be a secure stream. See Stream Types below.
Each stream type in the Stream Types table below uses a single stream, with the following exceptions and qualifications:
- External UDP clients connecting to a Gecko OS UDP server do not use an additional stream. That is, a single UDP server takes only one stream and allows an unlimited number of UDP clients to be connected.
- The TCP server, with no client connected, uses no streams. Each external TCP or TLS client connecting to a Gecko OS TCP or TLS server uses an additional stream.
- When in STREAM mode, the TCP/TLS/WebSocket servers are limited to one client connection.
Stream Types
List the currently open streams with the stream_list command. Streams are listed with stream handle, type, and information about the stream source.
Note that some stream types support a limited set of operations. The following is a list of stream types, and for each type the command to create it, and the stream operations it supports.
Network Status Indication Using GPIOs
You can configure GPIOs to act as indicators of networking states, such as the state of the WLAN connection, the Soft AP connection, or DHCP progress. You can configure a selection of blink rates to indicate states.
See variables:
See Peripherals, System Indicator Functions.
Remote Terminal Access
You can control a Gecko OS device with a TCP/IP telnet connection via a remote terminal, connected to the device via the Soft AP interface or the WLAN interface.
Configure the remote terminal with the variables:
- remote_terminal.enabled
- remote_terminal.interface
- remote_terminal.password
- remote_terminal.port
- remote_terminal.timeout
See the Wi-Fi Remote Terminal application note.
Network Discovery
Network Discovery for Gecko OS is under development.
Discovery Overview
In simple terms, network discovery is used to give the module a name on the local network.
So, for instance, if the module has a domain name mymodule.local
, a remote client on the same network can connect to the module using the domain mymodule.local
even though the domain mymodule.local
is not registered with a DNS server.
This is useful because the remote client doesn't need to know the IP address of the module.
Gecko OS supports three network discovery protocols: mDNS (multicast Domain Name System), LLMNR (Link-Local Multicast Name Resolution) and NetBIOS. The latter two protocols are used by Windows systems only.
Configure mDNS with the variables:
Discovery OS Support
The remote client must support one or more network discovery protocols for device discovery to work.
Apple
Mac OS X & iOS support mDNS by default, with Bonjour.
Windows
Windows has support for mDNS, but by default it uses the LLMNR and NetBIOS protocols. These protocols are very similar to mDNS so their basic domain resolution features are supported by the module as well. When a domain is entered into the web browser, Windows follows this sequence to resolve the domain:
- Check local cache
- Issue LLMNR query
- Issue NetBIOS query
- Issue DNS query
The LLMNR and NetBIOS queries are broadcast to the local network only. The DNS query is typically sent to the internet.
If network discovery is enabled on the module, the module will receive the LLMNR and NetBIOS queries, compare the query domain to its mdns.name, and if they match respond with the module's IP address. In this way the module can easily be found on the local network from a Windows machine.
A NetBIOS domain can have up to 15 characters (including the '.local'). If mdns.name is longer than 15 characters then the NetBIOS protocol is not used.
Finally, some ISPs hijack the .local
domain for their own purposes, including advertising. This may cause a Windows PC to fail to resolve the domain.
The solution (for Windows only) is to drop .local
from the URL and simply use http://mymodule/
directly.
Linux
Linux needs an additional package installed for mDNS support. The most common package is Avahi.
Android
Android does not support mDNS (or other ZeroConf protocols) at the platform level, so third party Android apps like Chrome may not support mDNS. An Android SDK with mDNS support is available, so you can create an Android app with mDNS support. The Zentri Android Discovery
app, available from the Google Play Store, demonstrates using the Android mDNS SDK to provide mDNS discovery on Android devices.
Discovery in a Nutshell
Network discovery provides a way for remote clients to resolve the IP address of the module on a local network using a standard protocol. mDNS has other features which allow the module to advertise various services including HTTP, TCP & UDP servers. Gecko OS supports configuration of these additional features with the mdns.service variable.
mDNS Native API
Broadcast Status Announcement
A Gecko OS device broadcasts its properties in JSON format. The properties can be sent either as UDP packets to a UDP host or by a post request to an HTTP host.
Properties include by default the IP address and the MAC address.
Configure broadcast with the variables:
- broadcast.data
- broadcast.http.host
- broadcast.interface
- broadcast.interval
- broadcast.udp.ip
- broadcast.udp.local_port
- broadcast.udp.remote_port
See also the Broadcast UDP Packet Application Note.
Captive Portal
Captive portal is supported during websetup and optionally for the soft AP. When the HTTP Server receives certain requests, it redirects to the root HTTP server web page. See softap.captive_portal_enabled.
Passkeys
The following network passkeys follow the same rules for allowable characters and setting syntax:
- set wlan.passkey
- set softap.passkey
- set setup.web.passkey
Passkey values can be provided as printable ASCII, or as encoded ASCII characters.
Printable ASCII
ASCII passwords must be 8-63 characters long. Any printable ASCII (in the character code range 32
to 127
) may be used.
Example:
set wlan.passkey password
set wlan.passkey ~!@#$#@#@#^&(()
Encoded ASCII
Encoded ASCII characters may be used.
An encoding is delimited with a backslash. The following encoding values are supported:
Encoded Value | Decoded Value | ASCII Hex Value |
---|---|---|
\0 | Null character | 0x00 |
\s | Space | 0x20 |
\\ | Backslash | 0x5C |
\t | Tab | 0x09 |
\n | New line | 0x0A |
\r | Carriage Return | 0x0D |
\" | Double-quote | 0x22 |
\x?? | Hex value | 0x?? |
Example:
set wlan.passkey p\"ss\tw\nor\xFF
Note: The length of the encoded string can be longer than 63 character, however, the length of the decoded string must be 8-63 characters.
The variable getter prints all non-printable characters in their hex encoded representation (e.g. \r
-> \x0D
)
Pre-generated PSK
A 64 char hex string PSK may be supplied.
Example:
set wlan.passkey e2e04dcb82891a286e5d524b63f4963ac1f8dc49852bd6b97441d9545054d270
See https://www.wireshark.org/tools/wpa-psk.html for an example of generating a PSK.
Other Notes
Passwords can also be wrapped in double-quotes to insert spaces.
Example:
set wlan.passkey "this is a password"