0 - the request failed, the contains the error message ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... Gecko OS Plugin plugin_core_commands Example
Commands Core Functions for issuing Gecko OS commands. More. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API . ... fmt Formatted Gecko OS serial command Returns
ProductWirelessResource TypeSoftware API documentation
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... 0 = no, 1 = yes <- Print a list of faults (8 faults should print) <- Reset faults ...
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren )
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/4.0/group-api-core