DMS Settings
dms.auto_start_enabled
Abbreviation
dm a
Access
get/set
Description
The dms.auto_start_enabled
variable automatically starts the DMS websocket when the configured DMS interface is brought up.
This is useful for SDK applications that need to use the DMS APIs but do not require other DMS plugins such as Command or Telemetry.
Note: This variable is not required if another DMS plugin is enabled such as dms.cmd.enabled or dms.telemetry.interval.
Arguments
1/0
Default
0
Get example
> get dm a
0
Set example
> set dms.auto_start_enabled 1
Set OK
dms.bundle_id
Abbreviation
dm b
Access
get
Description
Displays the DMS bundle ID of the firmware bundle currently loaded onto the device.
Arguments
None
Default
None
Gecko OS Kernel Plugin
Get example
> get dm b
bc19d591-e96b-4017-9ac3-0459cb480706
dms.cmd.enabled
Abbreviation
dm c e
Access
get/set
Description
Enable support for issuing commands to the device from the DMS. When enabled, the device opens a secure websocket. With the websocket, asynchronous Gecko OS external commands can be sent to the device.
Note: The device must be claimed/activated for this feature to work.
To use this feature, set up the device with credentials for a WLAN connected to the Internet, set dms.cmd.enabled
to 1
, and reboot.
On rebooting the device opens a Websocket connection to the DMS. Log into the DMS as the user who has claimed the device, select the device, and in the Device Details page select the Console tab. The tab should display device connected
. You can now issue commands to the device via the DMS device console.
> set dms.cmd.enabled 1
Set OK
> save
Saved
Success
> reboot
Rebooting
[2019-01-01 | 06:17:20: Disassociated]
[Ready]
SILABS-WGM160P-4.0.0, Gecko_OS-STANDARD-4.0.12-1198, WGM160P
> [Associating to SLA]
> Obtaining IPv4 address via DHCP
IPv4 address: 10.5.6.74
[Associated]
> Resolving host: dfu.zentri.com
Connecting (WS): 52.65.215.174:80
DMS stream opened
Arguments
0/1
Default
0
- not enabled
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get dm c e
0
Set example
> set dm c e 1
Set OK
dms.connection.host
Abbreviation
dm c h
Access
get
Description
Return the DMS host name the device users to connect to the DMS. This value can be updated only with an appropriately configured DFU package.
Arguments
?
Default
None
Gecko OS Kernel Plugin
Get example
> get dm c h
dms.zentri.com
dms.connection.port
Abbreviation
dm c p
Access
get/set
Description
Get or set the DMS socket port.
Arguments
<1-65534>
Default
443
Gecko OS Kernel Plugin
Get example
> get dm c p
443
Set example
> set dm c p 8004
Set OK
dms.connection.timeout
Abbreviation
dm c t
Access
get/set
Description
Specifies the amount of time in seconds the device waits for DMS data before timing out.
This is useful for devices that have a poor connection to the DMS
Notes
This persists through factory resets.
Arguments
<seconds>
Range: <7 -120>
Default
20
Gecko OS Kernel Plugin
Get example
> get dm c h
dms.zentri.com
dms.interface
Abbreviation
dm i
Access
get/set
Description
Get or set the network interface to use when connecting to the DMS.
Arguments
-
Default
wlan
where options are:
wlan
ethernet
- if available for device
Gecko OS Kernel Plugin
Get example
> get dm i
wlan
Set example
> set dm i wlan
Set OK
dms.product_id
Abbreviation
dm p
Access
get
Description
Get the ID for the product to which the device is currently activated.
Arguments
-
Default
-
Get example
> get dm p
1
dms.telemetry.adc_mask
Abbreviation
dm t a
Access
get/set
Description
Bitmask of ADCs to include in posted telemetry message to DMS.
Arguments
<bitmask>
where <bitmask>
is a 32bit hex string. Each bit maps to an ADC number. e.g. 0x15
maps to ADCs 0, 2, 4.
Default
0x00
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get dms.telemetry.adc_mask
0x0
Set example
> set dm t a 0x1
Set OK
dms.telemetry.data_mask
Abbreviation
dm t d
Access
get/set
Description
Bitmask of data to include in posted telemetry message to DMS.
Arguments
<bitmask>
where <bitmask>
is a 32bit hex string with the following flags:
Flag Bit | Description |
---|---|
0x0001 | WLAN SSID |
0x0002 | WLAN BSSID |
0x0004 | WLAN channel |
0x0008 | WLAN RSSI |
0x0010 | WLAN IP address |
0x0020 | remote terminal port |
0x0040 | firmware version |
0x0080 | uptime |
0x0100 | current time |
0x0200 | system faults |
Default
0x3FF
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get dms.telemetry.data_mask
0x3FF
Set example
> set dm t a 0x211
Set OK
dms.telemetry.gpio_mask
Abbreviation
dm t g
Access
get/set
Description
Bitmask of GPIOs to include in posted telemetry message to DMS.
Arguments
<bitmask>
where <bitmask>
is a 32bit hex string. Each bit maps to a GPIO number. e.g. 0x15
maps to GPIOs 0, 2, 4.
Default
0x00
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get dms.telemetry.gpio_mask
0x0
Set example
> set dm t g 0x31
Set OK
dms.telemetry.interval
Abbreviation
dm t i
Access
get/set
Description
The period in seconds to post telemetry messages to the DMS.
When the device joins the WLAN network, Gecko OS posts a telemetry message immediately. Gecko OS posts a subsequent message every dms.telemetry.interval
seconds.
Arguments
<seconds>
Default
0
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get dm g i
0
Set example
> set dms.telemetry.interval 10
Set OK