HTTP Server
http.server.api_enabled
Abbreviation
ht s a
Access
get/set
Description
Enable the HTTP Server RESTful API.
See Networking and Security, HTTP Server.
The API is enabled by default, so enabling the HTTP server with http.server.enabled also allows access to the API. To disable HTTP RESTful API calls when the HTTP server is running, set http.server.api_enabled
to 0
.
Arguments
<1|true|on/0|false|off>
Default
1
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.api_enabled
1
Set example
> set ht s a 0
Set OK
http.server.auth_title
Abbreviation
ht s h
Access
get/set
Description
Configure the authentication header displayed when a user fails to enter a valid username or password. This sets the title of a web browser's authentication dialog.
Gecko OS sets the variable value in the WWW-Authenticate HTTP header:
WWW-Authenticate: Basic realm=<http.server.auth_title>
This variable should be used with http.server.username and http.server.password.
See Networking and Security, HTTP Server.
Arguments
title
Default
""
(empty)
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Set example
> set http.server.auth_title MyServer
Set OK
Get example
> get http.server.auth_title
MyServer
http.server.cors_origin
Abbreviation
ht s c
Access
get/set
Description
Specifies origins for which the web browser same-origin policy is relaxed.
If <origin>
is set to an empty string, then CORS is completely disabled.
For requests without credentials, a value of *
acts as a wildcard, allowing any origin to access the resource.
If the value of http.server.cors_origin
contains a #
character, then the #
character is replaced with the last 3 characters of the device's MAC address. This works in conjunction with using the #
character in mdns.name.
See HTTP Server RESTful API, CORS.
Arguments
<origin>
Default
""
(empty string). To set the http.server.cors_origin
variable to the empty string, supply an argument with two double quotes: ""
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.cors_origin
Set example
> set ht s c *
Set OK
http.server.denied_filename
Abbreviation
ht s d
Access
get/set
Description
Specify the file name of the page to be displayed in the event that the HTTP server denies authentication.
See Networking and Security, HTTP Server.
Arguments
<filename>
Default
webapp/unauthorized.html
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.denied_filename
webapp/unauthorized.html
Set example
> set ht s d access_denied.html
Set OK
http.server.enabled
Abbreviation
ht s e
Access
get/set
Description
Enable the HTTP server.
See Networking and Security, HTTP Server.
Arguments
<1|true|on/0|false|off>
Default
0
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get ht s e
0
Set example
> set ht s e 1
Set OK
http.server.interface
Abbreviation
ht s i
Access
get/set
Description
Specifies the network interface used by the HTTP server.
See Networking and Security, HTTP Server.
Arguments
<default/softap/wlan>
Default
default
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.interface
default
Set example
> set ht s i wlan
Set OK
http.server.keep_alive_enabled
Abbreviation
ht s b
Access
get/set
Description
To avoid the overhead of opening and closing a new HTTP connection for each request, you can keep the HTTP connection open for a series of requests, or for a specified time.
If http.server.keep_alive_enabled
is set to 1
and the HTTP request contains the header:
Connection: Keep-Alive
OR the Connection
header is NOT in the request, then Gecko OS keeps the HTTP connection opened until it is manually closed by the client or device, or until no requests have been received for a period set by the http.server.keep_alive_timeout variable.
While the HTTP connection is open, the client can send additional REST API requests.
Note: If this feature is enabled AND the following header is added to the HTTP request, then the HTTP connection is closed after the HTTP response is returned.
Connection: Close
See also:
Arguments
<1|true|on/0|false|off>
Default
0
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.keep_alive_enabled
0
Set example
> set ht s b 1
Set OK
http.server.keep_alive_timeout
Abbreviation
ht s j
Access
get/set
Description
The maximum time, in seconds, for which a previously opened HTTP keep-alive connection remains open without any activity. If a keep-alive connection is opened and the client does not send another HTTP request within this timeout, then the server automatically closes the connection.
See also:
Arguments
<seconds>
Range: 0-65535
Default
5*60
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.max_clients
3
Set example
> set ht s m 1
Set OK
http.server.max_clients
Abbreviation
ht s m
Access
get/set
Description
Specifies the maximum number of clients the HTTP server allows to connect.
Restricting connected clients may be necessary to limit memory usage. See Memory.
See Networking and Security, HTTP Server.
Arguments
<clients>
Default
6
Range
1 - 9
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.max_clients
3
Set example
> set ht s m 1
Set OK
http.server.notfound_filename
Abbreviation
ht s n
Access
get/set
Description
Specifies the filename of the web page to be displayed in the event that the HTTP server reports a 404 - not found error.
<filename>
See Networking and Security, HTTP Server.
Default
''
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.notfound_filename
Set example
> set ht s n notfound.html
Set OK
http.server.password
Abbreviation
ht s w
Access
get/set
Description
Set the password of the http server. The username MUST be set as well for the http server to start.
See HTTP Server Security and Authorization.
Arguments
<password>
Default
none
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Set example
> set ht s w secretpassword
Set OK
Get example
> get ht s w
secretpassword
http.server.port
Abbreviation
ht s p
Access
get/set
Description
Set the port on which the HTTP server listens.
See Networking and Security, HTTP Server.
Arguments
<listening port>
Default
80
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get ht s p
80
Set example
> set http.server.port 8080
Set OK
http.server.root_filename
Abbreviation
ht s r
Access
get/set
Description
This sets or gets the root file of the HTTP server. If a plain request to
See Networking and Security, HTTP Server.
Arguments
<filename>
Default
/webapp/index.html
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get ht s r
webapp/index.html
Set example
> set http.server.root_filename /setup/home.html
Set OK
http.server.tls_cert
Abbreviation
ht s l
Access
get/set
Description
The server TLS CA certificate filename.
See Networking and Security, HTTPS Server.
Arguments
<filename>
Default
null
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get ht s c
mycert.pem
Set example
> set ht s c mycert.pem
Set OK
http.server.tls_enabled
Abbreviation
ht s t
Access
get/set
Description
Enable server Transport Level Security (TLS).
See Networking and Security, HTTPS Server.
Arguments
<1|true|on/0|false|off>
Default
0
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get ht s t
0
Set example
> set ht s t 1
Set OK
http.server.tls_key
Abbreviation
ht s k
Access
get/set
Description
The server TLS certificate key filename.
See Networking and Security, HTTPS Server.
Arguments
<filename>
Default
null
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get ht s k
mycert.key
Set example
> set ht s k mycert.key
Set OK
http.server.tls_log_clients
Abbreviation
ht s o
Access
get/set
Description
Enable/disable TLS client logging. http.server.tls_verify_peer must be enabled for this feature.
See http.server.tls_client_log.
See Networking and Security, HTTPS Server.
Arguments
<1|true|on/0|false|off>
where
0
orfalse
oroff
: TLS client logging disabled1
ortrue
oron
: TLS client logging enabled
Default
false
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.tls_log_clients
0
Get example
> set http.server.tls_log_clients 1
Set OK
http.server.tls_verify_peer
Abbreviation
ht s v
Access
get/set
Description
When this variable is set, a connecting client must provide a valid TLS certificate that the server validates. The client is disconnected if the provided certifcate is invalid. Note: The http.server.tls_cert variable must be set if using this feature.
See Networking and Security, HTTPS Server.
Arguments
<1|true|on/0|false|off>
where
0
orfalse
oroff
: do not verify1
ortrue
oron
: verify with client TLS certificate
Default
0
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get ht s v
0
Set example
> set ht s v 1
Set OK
http.server.username
Abbreviation
ht s u
Access
get/set
Description
Set the username of the http server. The password MUST be set as well for the http server to start.
See HTTP Server Security and Authorization.
Arguments
<username>
Default
null
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.username
cyrano
Set example
> set ht s u cyrano
Set OK
http.server.ws_connected_gpio
Abbreviation
ht s x
Access
get/set
Description
The GPIO used to indicate whether a websocket stream is connected. It is asserted when one or more websocket streams are open.
Note: Set to -1
to disable feature and free assigned GPIO.
See also system.oob.gpio.
See Networking and Security, Websocket Server.
Arguments
<gpio #>
Default
-1
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.ws_connected_gpio
-1
Set example
> set http.server.ws_connected_gpio 9
Set OK
> get gp u
! # Description
...
# 9 http.server.ws_connected_gpio
...
http.server.ws_data_gpio
Abbreviation
ht s y
Access
get/set
Description
The GPIO used to indicate whether a websocket stream has data available to read. It is asserted when one or more websocket streams have data to be read.
See also system.oob.gpio.
Note: Set to -1
to disable feature and free assigned GPIO.
See Networking and Security, Websocket Server.
Arguments
<gpio #>
Default
-1
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get http.server.ws_data_gpio
-1
Set example
> set http.server.ws_data_gpio 9
Set OK
> get gp u
! # Description
...
# 9 http.server.ws_data_gpio
...