WLAN Interface
wlan.antenna.select
Abbreviation
wl a s
Access
get/set
Description
The default antenna used by the Wi-Fi radio.
Note: Availability of antennas is hardware dependent. On hardware with only one antenna this setting has no effect.
1
: antenna 1 (or the internal antenna) is selected2
: antenna 2 (or the external antenna) is selectedauto
: the best antenna is automatically selected on a per-packet basis
Note: An external antenna must be connected if 2
or auto
mode are selected.
Arguments
<1/2/auto>
Default
1
Properties
- takes effect immediately
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl a s
R000003
1
Set example
> set wl a s auto
R000008
Set OK
wlan.auto_join.enabled
Abbreviation
wl o e
Access
get/set
Description
Enable/disable network auto-join using the wlan interface on bootup.
See Procedure for Joining a WLAN Network.
Arguments
<1|true|on/0|false|off>
where
0
orfalse
oroff
: disabled1
ortrue
oron
: enabled
Default
0
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get wl o e
R000003
0
Set example
> set wl o e true
R000008
Set OK
wlan.auto_join.retries
Abbreviation
wl o r
Access
get/set
Description
Maximum number of attempts to auto-join a network. 0 = retry indefinitely.
See Procedure for Joining a WLAN Network.
Arguments
<0-255>
Default
3
Properties
Gecko OS Kernel Plugin
Get example
> get wl o r
R000003
3
Set example
> set wl o r 5
R000008
Set OK
wlan.auto_join.retry_delay
Abbreviation
wl o d
Access
get/set
Description
The period between auto-join attempts in seconds.
See Procedure for Joining a WLAN Network.
Arguments
<0-255>
Default
10
Properties
Gecko OS Kernel Plugin
Get example
> get wl o d
R000004
10
Set example
> set wl o d 5
R000008
Set OK
wlan.bssid
Abbreviation
wl b
Access
get/set
Description
Specify the BSSID for the WLAN.
When wlan.bssid
is set, Gecko OS attempts to associate with the network via the access point with the specified BSSID, regardless of the wlan.ssid setting. This allows connecting to hidden networks.
The wlan.passkey must be provided.
The wlan.ssid cannot be empty. Setting wlan.ssid clears wlan.bssid
, so set wlan.ssid first, then set wlan.bssid
. For example:
Gecko OS Commands | Description |
---|---|
|
|
Note: On joining a WLAN, if the WLAN SSID is advertised, it replaces the value of wlan.ssid.
To disable wlan.bssid
, set the value to 00:00:00:00:00:00
or set wlan.ssid to clear it.
See Procedure for Joining a WLAN Network.
Arguments
<bssid>
Default
00:00:00:00:00:00
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get wl b
R000019
00:00:00:00:00:00
Set example
> set wl b 7C:69:F6:35:8F:F8
R000008
Set OK
wlan.dhcp.enabled
Abbreviation
wl d e
Access
get/set
Description
Select whether DHCP is used to automatically obtain an IPv4 IP address on the wlan interface.
Note: Renamed from network.dhcp
after Gecko OS v1.2. Renamed from network.dhcp.enabled
in Gecko OS 3.0.
See Networking and Security, DHCP Client.
Arguments
<1|true|on/0|false|off>
where
0
orfalse
oroff
: disabled1
ortrue
oron
: enabled
Default
1
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl d e
R000003
1
Set example
> set wl d e off
R000008
Set OK
wlan.dhcp.cache_enabled
Abbreviation
wl d c
Access
get/set
Description
When DHCP caching is enabled, the received DHCP IP address and corresponding lease time is cached to RAM. When the device is rebooted via the reboot command, the RAM cache and corresponding timestamp is saved to NVM.
Upon rebooting the saved DHCP IP is restored and the lease time is updated with the amount of time that has elapsed since it was last stored. DHCP IP caching can save a considerable amount of time when re-connecting to the network as the full DHCP sequence is skipped (assuming there is enough time left on the DHCP lease).
See Networking and Security, DHCP Client.
Arguments
<1|true|on/0|false|off>
where
0
orfalse
oroff
: disabled1
ortrue
oron
: enabled
Default
1
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get wl d c
R000003
1
Set example
> set wl d c 0
R000008
Set OK
wlan.dhcp.hostname
Abbreviation
wl d h
Access
get/set
Description
Configures the DHCP client's hostname (DHCP option 12) sent to the DHCP server.
See Networking and Security, DHCP Client.
Arguments
<hostname>
Default
Gecko_OS-#
where #
is replaced by the last three digits of the WLAN MAC address
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get wl d h
R000009
Gecko_OS-#
Set example
> set wl d h my_dhcp_client
R000008
Set OK
wlan.dhcp.timeout
Abbreviation
wl d t
Access
get/set
Description
Amount of time in seconds the module waits as a client for an IP from a DHCP server. See wlan.dhcp.enabled.
See Networking and Security, DHCP Client.
Arguments
<timeout_seconds>
Range: 1-255 seconds
Default
15
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl d t
R000004
15
Set example
> set wl d t 25
R000008
Set OK
wlan.hide_passkey
Abbreviation
wl h
Access
get/set
Description
Hide the variable wlan.passkey. Once hidden, a factory reset must be issued to reset this variable and reveal the (reset value) of the passkey.
Note: Don't forget to save before reboot!
See Procedure for Joining a WLAN Network.
Arguments
<1|true|on/0|false|off>
where
0
orfalse
oroff
: hide passkey disabled1
ortrue
oron
: hide passkey enabled
Default
0
Properties
- takes effect immediately
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl h
R000003
0
Set example
> set wl h true
R000008
Set OK
> save
R000009
Success
> get wlan.passkey
R000008
******
wlan.info
Abbreviation
wl i
Access
get
Description
WLAN connection status parameters: state, SSID, BSSID, channel and datarate
Arguments
-
Default
<varies>
Gecko OS Kernel Plugin
Get example
> get wlan.info
state: up
SSID: My_Network
BSSID: 30:85:A9:E7:9C:B0
channel: 6
datarate: 450.0
wlan.join.result
Abbreviation
wl j s
Access
get
Description
Result of most recent join attempt. Returns a code:
Code | Description |
---|---|
0 | Haven't tried to join |
1 | Success - Joined network |
2 | Joining network |
3 | SSID not set |
4 | No password set and AP requires security |
5 | Specified security not supported by AP |
6 | Network not found |
7 | Failed to join network. All attempts to join have failed |
8 | Join aborted. network_down called while trying to join |
See Procedure for Joining a WLAN Network.
Arguments
-
Default
<varies>
Gecko OS Kernel Plugin
Get example
> get wl j s
1
wlan.join.retries
Abbreviation
wl j r
Access
get/set
Description
Specifies the maximum number of attempts to join a WLAN network after issuing the network_up command (or any other command requiring network access when the network is down).
See Procedure for Joining a WLAN Network.
If the network_down command is issued while attempting to join a network, the subsequent attempts are canceled.
Note that wlan.join.retries is separate from the wlan.auto_join.retries variable. If wlan.auto_join.retries > 0, then the total number of retries is calculated by the multiplication of wlan.join.retries with wlan.auto_join.retries.
Note: If wlan.join.retries
is set to 1
, the device attempts to connect only once. If the device has cached network details, and these details are no longer true due to network changes, the device fails to connect and does not attempt to connect again. Set wlan.join.retries
to 2
or more to avoid this problem. See The Network Up Sequence.
Arguments
<retries>
where '
Default
3
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl j r
R000003
5
Set example
> set wl j r 5
R000008
Set OK
wlan.join.timeout
Abbreviation
wl j t
Access
get/set
Description
The maximum amount of time to wait while the module attempts to join a network.
See Procedure for Joining a WLAN Network.
Arguments
<timeout in ms>
Default
7000 ms
Properties
- save and reboot to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wlan.join.timeout
R000006
7000
Set example
> set wl j t 5000
R000008
Set OK
wlan.link_local.enabled
Abbreviation
wl i e
Access
get/set
Description
Enables and disables the link local feature.
The device obtains an IP address using the following sequence:
- IF wlan.dhcp.enabled == true THEN Attempt DHCP
- IF wlan.static.ip != 0.0.0.0 THEN Use static IP
- IF wlan.link_local.enabled == true THEN Attempt Link Local IP (e.g. Auto IP)
If all three steps fail to obtain an IP address then the network_up
sequence fails.
Arguments
<1|true|on/0|false|off>
Default
0
Properties
- save and reboot to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wlan.link_local.enabled
0
Set example
> set wl i e 1
R000008
Set OK
wlan.link_local.timeout
Abbreviation
wl i t
Access
get/set
Description
Configures the maximum time in seconds to obtain an IP via link local protocol.
Arguments
<timeout in seconds>
where:
<timeout in seconds>
is in the range3
to30
Default
20
Properties
- save and reboot to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wlan.link_local.timeout
20
Set example
> set wl i t 30
R000008
Set OK
wlan.mac
Abbreviation
wl m
Access
get
Description
Returns the wlan MAC address.
Arguments
-
Default
varies
Properties
- available in Safe Mode
Gecko OS Kernel Plugin
Get example
> get wl m
R000019
4C:55:CC:01:23:45
wlan.multicast.address
Abbreviation
wl m a
Access
get
Description
Configure UDP multicast address range.
When the WLAN interface is brought up, it joins the configured multicast group address. When the interface is brought down it leaves the multicast group address.
Notes
The valid multicast group address range is 224.0.0.0 to 239.255.255.255
0.0.0.0 disables the multicast feature
Multicast is supported only by the UDP client and server. The TCP protocol does not support multicast.
Arguments
<IP address range>
where:
- valid range is
224.0.0.0
to239.255.255.255
0.0.0.0
disables multicast
Default
0.0.0.0
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get wl m a
0.0.0.0
Set example
> set wl m a 239.0.0.255
Set OK
wlan.network.dns
Abbreviation
wl n d
Access
get
Description
Return a comma separated list of the DNS server addresses that the wlan interface is using.
Note: To set a static DNS address list, use the wlan.static.dns variable.
See Networking and Security, DNS Client
Arguments
-
Default
0.0.0.0
(i.e. No DNS addresses in use)
Properties
- available in Safe Mode
Gecko OS Kernel Plugin
Get example
> get wl n d
10.5.6.1
wlan.network.gateway
Abbreviation
wl n g
Access
get
Description
Returns the wlan interface IPv4 gateway IP address resolved by DHCP.
Note: To set a static gateway, use the wlan.static.gateway variable.
Arguments
-
Default
0.0.0.0
Properties
- available in Safe Mode
Gecko OS Kernel Plugin
Get example
> get wl n g
R000013
192.168.0.1
wlan.network.ip
Abbreviation
wl n i
Access
get
Description
Returns the wlan interface IPv4 IP address resolved by DHCP.
Note: To set a static IP address, use the wlan.static.ip variable.
Arguments
-
Default
0.0.0.0
Properties
- available in Safe Mode
Gecko OS Kernel Plugin
Get example
> get wl n i
R000014
192.168.0.79
wlan.network.netmask
Abbreviation
wl n n
Access
get
Description
Returns the wlan interface IPv4 netmask resolved by DHCP.
Note: To set a static netmask, use the wlan.static.netmask variable.
Arguments
-
Default
0.0.0.0
Properties
- available in Safe Mode
Gecko OS Kernel Plugin
Get example
> get wl n n
R000015
255.255.255.0
wlan.network.status
Abbreviation
wl n s
Access
get
Description
Returns the wlan network status. 0 = down, 1 = WLAN connected, 2 = IP network connected (with a valid IP address)
Arguments
-
Default
0
Properties
- available in Safe Mode
Gecko OS Kernel Plugin
Get example
> get wl n s
R000003
2
wlan.network.status_gpio
Abbreviation
wl n o
Access
get/set
Description
The GPIO used to indicate network connectivity status. GPIO low = not connected, GPIO high = the default network interface is connected and has an IP address.
See also system.oob.gpio.
Arguments
<GPIO#>
Default
-1
Properties
Gecko OS Kernel Plugin
Get example
> get wl n o
R000004
-1
Set example
> set wl n o 4
R000008
Set OK
wlan.passkey
Abbreviation
wl p
Access
get/set
Description
The WPA passphrase, WPA PSK or WEP key used when connecting to a Wi-Fi Access Point.
Notes for WEP
- The WEP key is replicated across each of the four possible keys.
- Silicon Labs STRONGLY discourages the use of WEP - it is NOT secure!
Arguments
<passphrase> / <WEP key> | Description |
---|---|
WPA Passphrase | length: 8 - 63 characters |
WPA PSK | length: 64 characters |
WEP Key | A 40-bit WEP key is specified as a 5-byte hex string, for example: 1122334455 A 104-bit WEP key is specified as 13-byte hex string, for example: 112233445566778899aabbccdd |
"" | Sets a NULL passphrase |
For allowable values and set syntax see: Networking and Security, Passkeys.
Default
""
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl p
R000000
Set example
> set wl p "Use the force!"
R000008
Set OK
wlan.powersave.listen_interval
Abbreviation
wl p l
Access
get/set
Description
The Wi-Fi sub-system remains in low power mode for a period specified in units of DTIM intervals (typically multiples of 100ms).
Arguments
<sleep time>
<sleep time>
is in the range 1-10. If<sleep time>
= 0, the WLAN subsystem wakes to listen to every DTIM.
Default
0
Properties
Gecko OS Kernel Plugin
Get example
> get wl p l
R000003
0
Set example
> set wl p l 90
R000008
Set OK
wlan.powersave.mode
Abbreviation
wl p m
Access
get/set
Description
Wi-Fi powersave mode. For lowest poweruse mode = 1
.
Arguments
<mode>
Description | |
---|---|
0 | Disabled: no powersave |
1 | Beacon skipping mode |
2 | DTIM skipping mode |
Default
0
Properties
Gecko OS Kernel Plugin
Get example
> get wl p m
R000003
0
Set example
> set wl p m 2
R000008
Set OK
wlan.rate.protocol
Abbreviation
wl r p
Access
get/set
Description
WLAN client data rate protocol selection.
Arguments
<11b/11g/11n/auto>
Value | Description |
---|---|
11b | Restrict 802.11 PHY data rates to 802.11b |
11g | Restrict 802.11 PHY data rates to 802.11g |
11n | Restrict 802.11 PHY data rates to 802.11n |
auto | Automatically select the best rate from all 802.11b/g/n rates |
Default
auto
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl r p
auto
Set example
> set wlan.rate.protocol 11b
Set OK
wlan.rate.transmit
Abbreviation
wl r x
Access
get/set
Description
Force the WLAN interface to transmit at a fixed data rate. The transmit rate is taken from valid rates specified by wlan.rate.protocol.
Arguments
<rate>
where value choices depend on protocol setting:
wlan.rate.protocol setting | protocol | wlan.rate.transmit <rate> value choices |
---|---|---|
11b | 802.11b | auto , 1 , 2 , 5.5 , 11 |
11g | 802.11g | auto , 6 , 9 , 12 , 18 , 24 , 36 , 48 , 54 |
11n | 802.11n | auto , mcs0 , mcs1 , mcs2 , ... , mcs7 |
auto | Any | All the above value choices are available |
Default
auto
- automatically select the best rate from the available choices
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl r x
5.5
Set example
> set wlan.rate.transmit mcs3
Set OK
wlan.roam.threshold
Abbreviation
wl r t
Access
get/set
Description
The wlan interface searches for a new AP to connect to once the signal from the AP it is currently associated with drops below the roam trigger level. The trigger level is specified in dBm in the range -1 to -99.
Arguments
<dBm>
Default
-99
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl r t
R000005
-99
Set example
> set wl r t -70
R000008
Set OK
wlan.rssi_average
Abbreviation
wl r
Access
get/set
Description
The number of consecutive wlan RSSI readings to average. Averaging smooths variations in the measured signal strength of the AP. Set to 0
to disable averaging.
Arguments
<# readings>
Default
0
Properties
Gecko OS Kernel Plugin
Get example
> get wl r
R000003
5
Set example
> set wl r 12
R000008
Set OK
wlan.scan.active_dwell
Abbreviation
wl s a
Access
get/set
Description
Time spent listening on a channel when actively scanning for APs.
Arguments
<milliseconds>
Default
75
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl s a
R000004
75
Set example
> set wl s a 90
R000008
Set OK
wlan.scan.channel_mask
Abbreviation
wl s m
Access
get/set
Description
Channels to scan. Specified by a hex bitmask.
Arguments
<channel_bitmask>
where bits correspond to channels, as shown in the following examples:
Channels : | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | channel_bitmask | |||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Channel 1 only | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0x001 | |||
Channels 11/6/1 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 1 | 0x421 | |||
All US region channels | 0 | 0 | 0 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0x7FF | |||
All except for channel 14 | 0 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0x1FFF | |||
All EU, Japan, Rest of World channels | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0x3FFF |
Note: Availability of channels 12, 13 and 14 depends on the wlan.region.
Default
0x07FF
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl s m
R000007
0x7FF
Set example
Set channels 11 & 1 only
> set wl s m 0x401
R000008
Set OK
wlan.scan.home_dwell
Abbreviation
wl s h
Access
get/set
Description
Time spent listening on the softap home channel when scanning in softap mode.
Arguments
<milliseconds>
Default
50
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl s h
R000004
50
Set example
> set wl s h 70
R000008
Set OK
wlan.scan.num_probes
Abbreviation
wl s n
Access
get/set
Description
Number of 802.11 probes to send when actively scanning.
Arguments
<# probes>
Default
3
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl s n
R000003
3
Set example
> set wl s n 5
R000008
Set OK
wlan.scan.passive_dwell
Abbreviation
wl s p
Access
get/set
Description
Time spent listening on a channel when passive scanning.
Arguments
<milliseconds>
Default
110
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl s p
R000005
110
Set example
> set wl s p 130
R000008
Set OK
wlan.scan.retries
Abbreviation
wl s r
Access
get/set
Description
Number of times to repeat a full scan when the scan command is issued.
Arguments
<# retries>
Default
3
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl s r
R000003
3
Set example
> set wl s r 5
R000008
Set OK
wlan.scan.type
Abbreviation
wl s t
Access
get/set
Description
Type of scan. Passive is listen-only, active transmits 802.11 probe management frames.
Arguments
<passive/active>
Default
active
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl s t
R000008
active
Set example
> set wl s t passive
R000008
Set OK
wlan.security
Abbreviation
wl c
Access
get/set
Description
The wlan security type. If set to Auto
, the security type is automatically populated when joining a network (except WEP). Alternatively, the security type may be forced to one of the options listed in Arguments below.
Notes for WEP
- wlan.security must be manually set to
WEP
BEFORE setting wlan.passkey if WEP security is used. - Silicon Labs STRONGLY discourages the use of WEP - it is NOT secure!
See Procedure for Joining a WLAN Network.
Arguments
<security type>
Options:
Auto
Open
WEP
WPA-AES
WPA-TKIP
WPA2-AES
WPA2-Mixed
WPA2-TKIP
Default
Auto
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl c
R000006
Auto
Set example
> set wl c WPA2-AES
R000008
Set OK
wlan.ssid
Abbreviation
wl s
Access
get/set
Description
The name of the AP the wlan client interface will attempt to join.
See Procedure for Joining a WLAN Network.
Arguments
<ssid>
A string containing spaces must be enclosed in double quotes:
> set wl s "My SSID"
Set OK
> get wl s
My SSID
A double quote in the string must be escaped with a backslash:
> set wl s "My \"SSID\""
Set OK
> get wl s
My "SSID"
ASCII characters can be input represented by their ASCII code in hex, in the form: \x<code>
. For example a backslash is represented by \x5C
. Unprintable ASCII characters, and the backslash, are displayed as their hex ASCII code in the get wl s
output:
> set wl s abc\x5Cdef
Set OK
> get wl s
abc\x5Cdef
A backslash can also be entered escaped by a backslash:
> set wl s abc\\def
Set OK
> get wl s
abc\x5Cdef
Default
""
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl s
R000012
My Home AP
Set example
> set wl s "Obi-wan Kenobi"
R000008
Set OK
wlan.static.dns
Abbreviation
wl t d
Access
get/set
Description
DNS server address if static network settings are used for the wlan interface.
See Networking and Security, DNS Server.
Arguments
<[IP address]/[host name]>
Default
8.8.8.8
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl t d
R000009
8.8.8.8
Set example
> set wl t d 8.8.4.4
R000008
Set OK
wlan.static.gateway
Abbreviation
wl t g
Access
get/set
Description
Gateway address if static network settings are used for the wlan interface.
Arguments
<IP address>
Default
0.0.0.0
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl t g
R000009
0.0.0.0
Set example
> set wl t g 192.168.0.1
R000008
Set OK
wlan.static.ip
Abbreviation
wl t i
Access
get/set
Description
Local IP address if static network settings are used for the wlan interface.
Arguments
<IP address>
Default
0.0.0.0
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl t i
R000009
0.0.0.0
Set example
> set wl t i 192.168.0.2
R000008
Set OK
wlan.static.netmask
Abbreviation
wl t n
Access
get/set
Description
Netmask if static network settings are used for the wlan interface.
Arguments
<network mask>
Default
0.0.0.0
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Kernel Plugin
Get example
> get wl t n
R000009
0.0.0.0
Set example
> set wl t n 255.255.255.0
R000008
Set OK
wlan.tx_power
Abbreviation
wl t
Access
get/set
Description
The Wi-Fi RF transmit power in units of dBm. Range is 0-20
.
The maximum transmit power is module dependent.
The value auto
sets wlan.tx_power
to the maximum value permitted by the region which is auto-detected.
Arguments
0-20/auto/default
Default
auto
Properties
- takes effect immediately
- available in Safe Mode
- preserved by NVM Backup
Gecko OS Plugin
Get example
> get wl t
R000006
auto
Set example
> set wl t 15
R000008
Set OK