http_upload Ping ping Setup ... 0 - the request failed, the contains the error message ... Gecko OS writes the file to extended flash or bulk flash, depending on the location option: -l ...
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... 0 = no, 1 = yes <- Print a list of faults (8 faults should print) <- Reset faults ...
ProductWirelessResource TypeSoftware API documentation
Login ... // Bluetooth LE//Version 4.0 //General ... You are viewing documentation for version: 4.0 Central and Peripheral Roles# ... Bluetooth Low Energy is a powerful and complex technology.
Results 1-5 of 5 for gecko-os/4/standard/4.0/sdk/api/gos_network_ping