0 - the request failed, the contains the error message ... c rc: CRC32 checksum of the file data, in hex format 2 . ... WGM160P Gecko OS Plugin file_system Example > fop myfile.txt
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
... system print level ( sy p ) = all, and system command header enabled ( sy c h ) = ... Example Example usage. Alphabetical List of Commands ... os pins can only use the strong drive strength.
ProductWirelessResource TypeSoftware API documentation
You are viewing documentation for version: 4.0 Central and Peripheral Roles# ... is to create a custom profile(s) for your application because it provides ultimate flexibility and doesn't cost ...
Results 1-5 of 5 for gecko-os/4/standard/4.0/sdk/system-application-nvm-nvm-defaults-c-example