system/custom_commands/nvm_defaults_validate.c
/*
* EVALUATION AND USE OF THIS SOFTWARE IS SUBJECT TO THE TERMS AND
* CONDITIONS OF THE CONTROLLING LICENSE AGREEMENT FOUND AT LICENSE.md
* IN THIS SDK. IF YOU DO NOT AGREE TO THE LICENSE TERMS AND CONDITIONS,
* PLEASE RETURN ALL SOURCE FILES TO SILICON LABORATORIES.
* (c) Copyright 2018, Silicon Laboratories Inc. All rights reserved.
*/
// This file is optional.
// It simply ensures all the entries in the NVM defines are within the valid range.
// If you see a compilation error here then an entry is out of range.
#define GOS_NVM_VALIDATE_ENTRIES
#include "nvm_settings.h"