system/settings_file/main.c
/*
* EVALUATION AND USE OF THIS SOFTWARE IS SUBJECT TO THE TERMS AND
* CONDITIONS OF THE CONTROLLING LICENSE AGREEMENT FOUND AT LICENSE.md
* IN THIS SDK. IF YOU DO NOT AGREE TO THE LICENSE TERMS AND CONDITIONS,
* PLEASE RETURN ALL SOURCE FILES TO SILICON LABORATORIES.
* (c) Copyright 2018, Silicon Laboratories Inc. All rights reserved.
*/
/*
* Documentation for this app is available online.
* See https://docs.silabs.com/gecko-os/4/standard/latest/sdk/examples/system/settings-file
*/
/*
* This demonstrates how to save and load configuration files
* to/from the extended flash file system.
*/
#include "gos.h"
#include "nvm_settings.h"
#define CONFIG_FILE "example_settings.csv"
#define APPLICATION_START_LINE "\r\nSettings File example starting ..."
static myapp_settings_t *myapp_settings;
/*************************************************************************************************/
void gos_app_init(void)
{
gos_result_t result;
GOS_LOG(APPLICATION_START_LINE);
GOS_LOG("NOTE: 'default_config.csv' will automatically be loaded after programming or DFU");
{
GOS_LOG("Failed to retrieve reference to MYAPP.SETTINGS settings from NVM, err:%d", result);
return;
}
// If myapp.version is zero then load the settings from the config file
if (myapp_settings->version == 0)
{
GOS_LOG("Verbosely loading configuration file: %s", CONFIG_FILE);
// NOTE: This will reboot the system if the file is successfully loaded
{
GOS_LOG("Error loading file, err:%d", result);
}
}
else
{
GOS_LOG("Example settings up-to-date");
}
GOS_LOG("Issue the command:");
GOS_LOG("- get myapp : View the current app settings");
GOS_LOG("- save my_settings.csv -u : Save all current settings to a file");
GOS_LOG("- load my_settings.csv -v : Load the saved settings file");
GOS_LOG("- load example_settings.csv -v' : Reload the example app settings file");
}
/*************************************************************************************************/
{
GOS_CMD_PARSE_INT_ARG_WITH_VAR(uint32_t, myapp_settings->version, argv[1], 0, UINT32_MAX);
}
/*************************************************************************************************/
{
return GOS_CMD_SUCCESS;
}
/*************************************************************************************************/
{
return GOS_CMD_SUCCESS;
}
/*************************************************************************************************/
{
GOS_CMD_PARSE_INT_ARG_WITH_VAR(uint32_t, myapp_settings->timeout, argv[1], 0, UINT32_MAX);
return GOS_CMD_SET_OK;
}
/*************************************************************************************************/
{
return GOS_CMD_SUCCESS;
}
/*************************************************************************************************/
{
}