0 - the request failed, the contains the error message ... File permissions bit m ask, specified as hex string 2 . ... Gecko OS lists all the variables in that group with their values.
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
These settings are provided to make it easy for a host microcontroller to parse ... Example Example usage. Alphabetical List of Commands ... os pins can only use the strong drive strength.
ProductWirelessResource TypeSoftware API documentation
Login ... // Bluetooth LE//Version 4.0 //General ... You are viewing documentation for version: 4.0 Central and Peripheral Roles# ... Bluetooth Low Energy is a powerful and complex technology.
Results 1-5 of 5 for gecko-os/4/standard/4.0/sdk/system-settings-file-nvm-defaults-c-example