Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... 0 = no, 1 = yes <- Print a list of faults (8 faults should print) <- Reset faults ...
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
More. gos_result_t gos_cmd_issue_return_uint32 (uint32_t *uint32_ptr, const char *fmt,.) ... Issue Gecko OS command, store string result in buffer. ... fmt Formatted Gecko OS command Returns
ProductWirelessResource TypeSoftware API documentation
Support ... Value 0 indicates no advertising duration limit and advertising continues until it is disabled. ... 3: Advertise on CH37 and CH38 4: Advertise on CH39 5: Advertise on CH37 and CH39
For 125 Kbps coded PHY, the device doesn’t pass the 8 dBm/ 3 KHz PSD limit with ... There isn’t any limitation on channel 39 because the upper channel is only used for advertisements, so ...
Results 1-5 of 5 for gecko-os/4/standard/4.0/structgos-http-upload-t