Silicon Labs
gecko-os/4/standard/4.1/group-api-log-file
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
      Results 1-5 of 5 for gecko-os/4/standard/4.1/group-api-log-file in 0.17 seconds
      TX Power Limitations for Regulatory Compliance (ETSI, FCC) | System & Performance | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../tx-power-limitations-for-regulatory-compliance-etsi-...
      // Bluetooth LE//Version 5.0 //General ... For 2 Mbps PHY, it is a few tenths dB more. ... , the output power can go up to 30 dBm and the power spectral density must be below 8 dBm / 3 KHz.
      Advertising and Scanning with LE Coded PHY | Advertising & Scanning | Bluetooth LE | v2.13 | Silicon Labs
      https://docs.silabs.com/.../adv-and-scanning-with-le-coded-...
      // Bluetooth LE//Version 2.13 // ... You are viewing documentation for version: 2.13 ... how advertising on the coded PHY works, as well how to establish a connection using the coded PHY.
      Bluetooth Advertising Data Basics | Advertising and Scanning | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/....
      // Bluetooth LE//Version 5.0 //General ... List of adopted services Bluetooth API reference manual Bluetooth Core Specification - This is the golden reference, but not that easy to ...
      Using Bluetooth Security Features in Silicon Labs Bluetooth SDK | General Security | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../using-bluetooth-security-features-in-silicon-labs-bluetooth-...
      // Bluetooth LE//Version 5.0 //General ... Bluetooth uses Secure Simple Pairing (SSP) pairing model. ... 2: new bonding will overwrite the existing bonding, which has not been in use the ...
      Using Energy Modes with Bluetooth Stack | System & Performance | Bluetooth LE | v2.13 | Silicon Labs
      https://docs.silabs.com/.../using-energy-modes-with-bluetooth-st...
      // Bluetooth LE//Version 2.13 //Getting Started ... returns only when a stack event (e.g., connection established event) is raised. ... The Bluetooth stack does not work in EM3 Stop mode.
        Results 1-5 of 5 for gecko-os/4/standard/4.1/group-api-log-file