1 - an update is available, the contains the new bundle version string ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... ipd 1 Input, high-impedance
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... system.safemode.sleep_timeout - Set the duration for which the device sleeps before ...
ProductWirelessResource TypeSoftware API documentation
BGX13-1.x Command Reference This page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... > gge 5 1 gges
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Modules Types Command data types. Functions ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API . ... Note
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/4.1/group-api-system-time-types