Silicon Labs
gecko-os/4/standard/4.1/group-api-util-bitstring
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
    Results 1-5 of 5 for gecko-os/4/standard/4.1/group-api-util-bitstring in 0.07 seconds
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    Nav Tips for Humans ... smtp_send TCP tcp_client tcp_server tls_client tls_server UART uart_update UDP ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ...
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all ... tcp.client.connect_timeout tcp.client.local_port tcp.client.retries tcp.client.retry_period uart.baud
    ProductWireless Resource TypeSoftware API documentation
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    uartu --- restart UART with new baud rate and flow control settings ... os pins can only use the strong drive strength. ... Use the dfu parameter to reboot in the UART-DFU bootloader mode.
    ProductWireless Resource TypeSoftware API documentation
      Results 1-5 of 5 for gecko-os/4/standard/4.1/group-api-util-bitstring