GPIO

gpio.alias

Abbreviation

gp a

Access

get/set

Description

A GPIO alias name between 1-15 characters. GPIO name aliasing avoids the need to remember which GPIO is connected where. You can give the GPIO a recognisable name instead! Retrieve aliases with get gp a all. Remove an alias by setting to an empty double quoted string ("").

Arguments

<all>/<GPIO#> <alias name>

Default

None

Platforms

Properties

Gecko OS Plugin

Get example

> get gp a 6
R000008
MyGPIO

Set example

> set gp a 6 FrontDoor
R000008
Set OK

gpio.init

Abbreviation

gp i

Access

get/set

Description

The initial direction and value of a GPIO after bootup/reset. Use the all option to retrieve a list of GPIOs and their current initialization settings.

GPIOs are initialized as follows:

Arguments

<all> / <GPIO#> <direction> <initial value>

Default

none

The default applies for unassigned GPIOs.

Platforms

Properties

Gecko OS Plugin

Get example

> get gp i 0
R000021
output_open_drain 1

Set example

> set gp i 0 out 1
R000008
Set OK

gpio.sleep

Abbreviation

gp s

Access

get/set

Description

Set the state of the specified GPIO when sleeping.

GPIOs are initialized as follows:

Arguments

<all> / <GPIO#> <state>

where state is one of the following:

StateDescription
defaultfactory default state
input_highzinput high impedance
input_pull_downinput pull down
input_pull_upinput pull up
output_highoutput high
output_lowoutput low

Default

default

Platforms

Properties

Gecko OS Plugin

Get example

> get gp s 0
input_pull_up

Set example

> set gp s 0 output_low
Set OK

gpio.usage

Abbreviation

gp u

Access

get

Description

Returns information about which GPIOs have been registered for functions, and which have standard I/O options set. GPIOs may be de-registered by setting the GPIO to -1 using the appropriate variable. e.g. set ioconn.status_gpio -1. See Peripherals.

Arguments

None

Default

<platform dependent>

Platforms

Gecko OS Plugin

Get example

> get  gp u
!  # Description
#  0 GPIO in
#  1 system.indicator.wlan
#  2 system.indicator.network
#  5 system.indicator.softap
# 11 setup.control_gpio
# 13 UART1 RX
# 14 UART1 TX
# 17 SPI0 CLK
# 18 SPI0 MOSI
# 19 SPI0 MISO
# 21 GPIO out
# 22 GPIO out