NTP

ntp.enabled

Abbreviation

nt e

Access

get/set

Description

Enable/disable synchronization of local time with network time.

See Networking and Security, NTP Client.

Arguments

1|true|on/0|false|off

where

Default

1

Platforms

Properties

Gecko OS Plugin

Get example

> get nt e
R000003
1

Set example

> set nt e off
R000008
Set OK

ntp.interface

Abbreviation

nt f

Access

get/set

Description

Specify the network interface used by NTP feature.

See Networking and Security, NTP Client.

Arguments

default/wlan/ethernet

where:

Default

default

Platforms

Properties

Gecko OS Plugin

Get example

> get nt f
wlan

Set example

> set nt f ethernet
R000008
Set OK

ntp.interval

Abbreviation

nt i

Access

get/set

Description

The synchronization interval used when updating local time with network time.

See Networking and Security, NTP Client.

Arguments

<seconds>

Default

3600

Platforms

Properties

Gecko OS Plugin

Get example

> get nt i
R000006
3600

Set example

> set nt i 14400
R000008
Set OK

ntp.server

Abbreviation

nt s

Access

get/set

Description

The IP address or host name of the NTP server used to obtain network time.

See Networking and Security, NTP Client.

Arguments

<IP address / host name>

Default

pool.ntp.org

Platforms

Properties

Gecko OS Plugin

Get example

> get nt s
R000014
pool.ntp.org

Set example

> set nt s 203.26.72.7
R000008
Set OK