Custom Commands
This contains all functionality needed to add/override commands to the Gecko OS Command API. More...
Modules | |
Types | |
Command types. | |
Macros | |
Command specific macros. | |
Functions | |
gos_result_t | gos_cmd_start_response (gos_cmd_result_t cmd_result, size_t size) |
Begin printing a command response. More... | |
gos_result_t | gos_cmd_write_continued_response (const void *data, size_t data_size) |
Write the command response body. More... | |
gos_result_t | gos_cmd_write_response (gos_cmd_result_t cmd_result, const void *data, size_t data_size) |
Write a complete command response. More... | |
gos_result_t | gos_cmd_format_response (gos_cmd_result_t cmd_result, const char *fmt,...) |
Write formatted command response. More... | |
gos_result_t | gos_cmd_format_vresponse (gos_cmd_result_t cmd_result, const char *fmt, va_list args) |
Write formatted command response. More... | |
gos_result_t | gos_cmd_read_data (void *data, uint32_t size, uint32_t *bytes_read_ptr, uint32_t timeout_ms) |
Read data from the command data bus. More... | |
gos_result_t | gos_cmd_write_data (const void *data, uint32_t size, uint32_t *bytes_written_ptr, uint32_t timeout_ms) |
Write data to command data bus. More... | |
gos_result_t | gos_cmd_update_system_monitor (void) |
Update the command thread's system monitor. More... | |
void | gos_cmd_set_console_enabled (bool enabled) |
Enable/disable the command serial console. More... | |
gos_result_t | gos_cmd_convert_cmd_result (gos_cmd_result_t cmd_result) |
gos_cmd_result_t | gos_cmd_set_bool (int argc, char **argv, bool *bool_val) |
gos_cmd_result_t | gos_cmd_set_flag (int argc, char **argv, uint32_t flag_mask, void *flag_ptr, uint8_t flag_width) |
Utility to parse flag argument and store to given pointer. More... | |
gos_cmd_result_t | gos_cmd_set_int (int argc, char **argv, intmax_t *int_val, intmax_t min, intmax_t max) |
Utility to parse integer argument and store to given pointer. More... | |
gos_cmd_result_t | gos_cmd_set_hex (int argc, char **argv, intmax_t *int_val, intmax_t min, intmax_t max) |
Utility to parse hex string and store to given pointer. More... | |
gos_cmd_result_t | gos_cmd_set_encoded_str (int argc, char **argv, void *buffer, size_t max_len, size_t *saved_len) |
Utility to parse encoded string and save to given buffer. More... | |
gos_cmd_result_t | gos_cmd_set_str (int argc, char **argv, char *buffer, size_t max_len) |
Utility to parse string and save to given buffer. More... | |
gos_cmd_result_t | gos_cmd_set_ip_address (int argc, char **argv, gos_ip_address_t *ip_addr) |
Utility to parse string into IP address. More... | |
gos_result_t | gos_cmd_read_write_data (size_t size, uint32_t read_timeout_ms, void *user, gos_cmd_writer_t writer, gos_cmd_write_poller_t poller) |
Utility to read command bus and write data to writer argument. If system.cmd.echo = 1 then characters are echoed to the command bus. More... | |
gos_cmd_result_t | gos_cmd_print_gpio_response (gos_gpio_t gpio) |
Print gos_gpio_t command response. More... | |
gos_cmd_result_t | gos_cmd_print_int32_response (int32_t value) |
Print 32bit signed integer command response. More... | |
gos_cmd_result_t | gos_cmd_print_uint32_response (uint32_t value) |
Print 32bit unsigned integer command response. More... | |
gos_cmd_result_t | gos_cmd_print_str_response (const char *str) |
Print string string command response. More... | |
gos_cmd_result_t | gos_cmd_print_hex_uint32_response (uint32_t value, uint8_t padding) |
Print 32bit unsigned integer as hex string command response. More... | |
gos_cmd_result_t | gos_cmd_print_ipv4_address_response (uint32_t ip) |
Print IPv4 address string as command response. More... | |
gos_cmd_result_t | gos_cmd_print_ip_address_response (const gos_ip_address_t *ip) |
Print IP address as string command response. More... | |
Detailed Description
This contains all functionality needed to add/override commands to the Gecko OS Command API.
Function Documentation
◆ gos_cmd_convert_cmd_result()
gos_result_t gos_cmd_convert_cmd_result | ( | gos_cmd_result_t | cmd_result | ) |
Converts a gos_cmd_result_t to gos_result_t
- Parameters
-
cmd_result
The result of a command, see gos_cmd_result_t
- Returns
- The corresponding gos_result_t of the gos_cmd_result_t
◆ gos_cmd_format_response()
gos_result_t gos_cmd_format_response | ( | gos_cmd_result_t | cmd_result, |
const char * | fmt, |
||
... |
|||
) |
Write formatted command response.
This will print the command header and supplied format string
- Parameters
-
[in] cmd_result
The result of the command [in] fmt
Response formatting string
- Returns
- gos_result_t result of api call
- Examples:
- cloud/coap_demo/commands.c, cloud/dps_demo/dps_demo_cli_commands.c, cloud/dps_demo/dps_demo_cli_variables.c, cloud/mqtt_demo/mqtt_cli_variables.c, hurricane/gps/main.c, hurricane/security_camera/settings.c, system/custom_commands/main.c, system/settings_file/main.c, and test/throughput/main.c.
◆ gos_cmd_format_vresponse()
gos_result_t gos_cmd_format_vresponse | ( | gos_cmd_result_t | cmd_result, |
const char * | fmt, |
||
va_list | args |
||
) |
Write formatted command response.
This will print the command header and supplied format string
- Parameters
-
[in] cmd_result
The result of the command [in] fmt
Response formatting string [in] args
Formatting string arguments
- Returns
- gos_result_t result of api call
◆ gos_cmd_print_gpio_response()
gos_cmd_result_t gos_cmd_print_gpio_response | ( | gos_gpio_t | gpio | ) |
Print gos_gpio_t command response.
- Parameters
-
gpio
gos_gpio_t value to print
- Returns
- GOS_CMD_SUCCESS if successfully printed, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_print_hex_uint32_response()
gos_cmd_result_t gos_cmd_print_hex_uint32_response | ( | uint32_t | value, |
uint8_t | padding |
||
) |
Print 32bit unsigned integer as hex string command response.
- Parameters
-
value
32bit unsigned integer value padding
Padding of printed hex value
- Returns
- GOS_CMD_SUCCESS if successfully printed, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_print_int32_response()
gos_cmd_result_t gos_cmd_print_int32_response | ( | int32_t | value | ) |
Print 32bit signed integer command response.
- Parameters
-
value
32bit signed integer
- Returns
- GOS_CMD_SUCCESS if successfully printed, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_print_ip_address_response()
gos_cmd_result_t gos_cmd_print_ip_address_response | ( | const gos_ip_address_t * | ip | ) |
Print IP address as string command response.
- Parameters
-
ip
Ip address, see gos_ip_address_t
- Returns
- GOS_CMD_SUCCESS if successfully printed, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_print_ipv4_address_response()
gos_cmd_result_t gos_cmd_print_ipv4_address_response | ( | uint32_t | ip | ) |
Print IPv4 address string as command response.
- Parameters
-
ip
IPv4 as integer
- Returns
- GOS_CMD_SUCCESS if successfully printed, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_print_str_response()
gos_cmd_result_t gos_cmd_print_str_response | ( | const char * | str | ) |
Print string string command response.
- Parameters
-
str
String value
- Returns
- GOS_CMD_SUCCESS if successfully printed, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_print_uint32_response()
gos_cmd_result_t gos_cmd_print_uint32_response | ( | uint32_t | value | ) |
Print 32bit unsigned integer command response.
- Parameters
-
value
32bit unsigned integer
- Returns
- GOS_CMD_SUCCESS if successfully printed, else corresponding error code, see gos_cmd_result_t
- Examples:
- demo/uart_blaster/commands.c, and network/uart_tcp_client/variables.c.
◆ gos_cmd_read_data()
gos_result_t gos_cmd_read_data | ( | void * | data, |
uint32_t | size, |
||
uint32_t * | bytes_read_ptr, |
||
uint32_t | timeout_ms |
||
) |
Read data from the command data bus.
This reads data from the data bus while a command is active.
- Note
- This should only be called during a custom command callback.
- Parameters
-
data
Buffer to hold read data size
Number of bytes to read bytes_read_ptr
Pointer to hold amount of data actually read timeout_ms
Time in milliseconds to wait for size
bytes of data
- Returns
- gos_result_t result of api call
- Examples:
- demo/secure_element/commands.c.
◆ gos_cmd_read_write_data()
gos_result_t gos_cmd_read_write_data | ( | size_t | size, |
uint32_t | read_timeout_ms, |
||
void * | user, |
||
gos_cmd_writer_t | writer, |
||
gos_cmd_write_poller_t | poller |
||
) |
Utility to read command bus and write data to writer argument. If system.cmd.echo = 1 then characters are echoed to the command bus.
There is also an optional argument to poll the available write TX buffer before writing the data.
- Parameters
-
size
Number of bytes to read read_timeout_ms
Time in milliseconds to wait for more data to be read user
User argument to pass to writer
andpoller
callbackswriter
Data writer callback, see gos_cmd_writer_t poller
Data polling callback, see gos_cmd_write_poller_t
- Returns
- result of API, see gos_result_t
◆ gos_cmd_set_bool()
gos_cmd_result_t gos_cmd_set_bool | ( | int | argc, |
char ** | argv, |
||
bool * | bool_val |
||
) |
Utility to parse a boolean argument and store to given pointer
- Note
- The second argument in
argv
is parsed. e.g.argv[1]
is parsed.
- Parameters
-
[in] argc
Number of arguments supplied to custom command callback [in] argv
Command arguments supplied to custom command callback [out] bool_val
Pointer to hold parsed argument
- Returns
- GOS_CMD_SET_OK if successful, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_set_console_enabled()
void gos_cmd_set_console_enabled | ( | bool | enabled | ) |
Enable/disable the command serial console.
When the command serial console is disabled, Gecko OS will not listen on the command bus for commands.
- Parameters
-
[in] enabled
Enable/disable serial command processing
◆ gos_cmd_set_encoded_str()
gos_cmd_result_t gos_cmd_set_encoded_str | ( | int | argc, |
char ** | argv, |
||
void * | buffer, |
||
size_t | max_len, |
||
size_t * | saved_len |
||
) |
Utility to parse encoded string and save to given buffer.
- Note
- The second argument in
argv
is parsed. e.g.argv[1]
is parsed.
- Parameters
-
[in] argc
Number of arguments supplied to custom command callback [in] argv
Command arguments supplied to custom command callback [out] buffer
Buffer to hold decoded string argument [in] max_len
Maximum length of the decoded string [out] saved_len
Pointer to hold actual length of decoded string
- Returns
- GOS_CMD_SET_OK if successful, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_set_flag()
gos_cmd_result_t gos_cmd_set_flag | ( | int | argc, |
char ** | argv, |
||
uint32_t | flag_mask, |
||
void * | flag_ptr, |
||
uint8_t | flag_width |
||
) |
Utility to parse flag argument and store to given pointer.
- Note
- The second argument in
argv
is parsed. e.g.argv[1]
is parsed.
- Parameters
-
[in] argc
Number of arguments supplied to custom command callback [in] argv
Command arguments supplied to custom command callback [in] flag_mask
The mask of the flag to set or clear based on the boolean value of argv[1] [in,out] flag_ptr
Pointer to existing flag value [in] flag_width
The size in bytes of the flag buffer
- Returns
- GOS_CMD_SET_OK if successful, else corresponding error code, see gos_cmd_result_t
- Examples:
- demo/uart_blaster/commands.c.
◆ gos_cmd_set_hex()
gos_cmd_result_t gos_cmd_set_hex | ( | int | argc, |
char ** | argv, |
||
intmax_t * | int_val, |
||
intmax_t | min, |
||
intmax_t | max |
||
) |
Utility to parse hex string and store to given pointer.
- Note
- The second argument in
argv
is parsed. e.g.argv[1]
is parsed.
- Parameters
-
[in] argc
Number of arguments supplied to custom command callback [in] argv
Command arguments supplied to custom command callback [out] int_val
Pointer to hold parsed argument [in] min
Minimum value the parsed argument can be [in] max
Maximum value the parsed argument can be
- Returns
- GOS_CMD_SET_OK if successful, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_set_int()
gos_cmd_result_t gos_cmd_set_int | ( | int | argc, |
char ** | argv, |
||
intmax_t * | int_val, |
||
intmax_t | min, |
||
intmax_t | max |
||
) |
Utility to parse integer argument and store to given pointer.
- Note
- The second argument in
argv
is parsed. e.g.argv[1]
is parsed. -
If the argument starts with
0x
then it is parsed as a hex number.
- Parameters
-
[in] argc
Number of arguments supplied to custom command callback [in] argv
Command arguments supplied to custom command callback [out] int_val
Pointer to hold parsed argument [in] min
Minimum value of the argument [in] max
Maximum value of the argument
- Returns
- GOS_CMD_SET_OK if successful, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_set_ip_address()
gos_cmd_result_t gos_cmd_set_ip_address | ( | int | argc, |
char ** | argv, |
||
gos_ip_address_t * | ip_addr |
||
) |
Utility to parse string into IP address.
- Note
- The second argument in
argv
is parsed. e.g.argv[1]
is parsed.
- Parameters
-
[in] argc
Number of arguments supplied to custom command callback [in] argv
Command arguments supplied to custom command callback [out] ip_addr
Pointer to gos_ip_address_t to hold parsed IP address
- Returns
- GOS_CMD_SET_OK if successful, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_set_str()
gos_cmd_result_t gos_cmd_set_str | ( | int | argc, |
char ** | argv, |
||
char * | buffer, |
||
size_t | max_len |
||
) |
Utility to parse string and save to given buffer.
- Note
- The second argument in
argv
is parsed. e.g.argv[1]
is parsed.
- Parameters
-
[in] argc
Number of arguments supplied to custom command callback [in] argv
Command arguments supplied to custom command callback [out] buffer
Buffer to hold string argument [in] max_len
Maximum length of the string
- Returns
- GOS_CMD_SET_OK if successful, else corresponding error code, see gos_cmd_result_t
◆ gos_cmd_start_response()
gos_result_t gos_cmd_start_response | ( | gos_cmd_result_t | cmd_result, |
size_t | size |
||
) |
Begin printing a command response.
This will print a serial command response header.
- Parameters
-
[in] cmd_result
The result of the command [in] size
The total size in bytes of the command response
- Returns
- gos_result_t result of api call
◆ gos_cmd_update_system_monitor()
gos_result_t gos_cmd_update_system_monitor | ( | void |
| ) |
Update the command thread's system monitor.
For long running commands, this should be periodically invoked so the system thread's system monitor does not trigger.
- Note
- The command thread's system monitor has a timeout of 30s so this should be invoke ~every 15s.
- Returns
- gos_result_t result of api call
◆ gos_cmd_write_continued_response()
gos_result_t gos_cmd_write_continued_response | ( | const void * | data, |
size_t | data_size |
||
) |
Write the command response body.
This will print the supplied response data. This should be called until the specified number of bytes from gos_cmd_start_response() have been written. e.g.:
- Parameters
-
[in] data
Response data [in] data_size
The size of command data to be written
- Returns
- gos_result_t result of api call
◆ gos_cmd_write_data()
gos_result_t gos_cmd_write_data | ( | const void * | data, |
uint32_t | size, |
||
uint32_t * | bytes_written_ptr, |
||
uint32_t | timeout_ms |
||
) |
Write data to command data bus.
This writes data to the data bus while a command is active.
- Note
- This should only be called during a custom command callback.
- Parameters
-
data
Pointer to data to write size
Number of bytes to write bytes_written_ptr
Pointer to hold amount of data actually written timeout_ms
Time in milliseconds to wait for size
bytes to be written
- Returns
- gos_result_t result of api call
◆ gos_cmd_write_response()
gos_result_t gos_cmd_write_response | ( | gos_cmd_result_t | cmd_result, |
const void * | data, |
||
size_t | data_size |
||
) |
Write a complete command response.
This will print the command header and supplied response data
- Parameters
-
[in] cmd_result
The result of the command [in] data
Response data [in] data_size
The size in bytes of the command response
- Returns
- gos_result_t result of api call