1 - an update is available, the contains the new bundle version string ... Default: extended . -c <checksum> c rc: CRC32 checksum of the file data, in hex format 2 . ... none -1 Platforms
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
4.1 Applying a PHY from RAIL rx 0 // Configs can be loaded only in radio Idle state ... 4.7.2 Dynamic FEC SUN FSK protocol defines the dynamic FEC feature which is supported on certain EFR32 ...
Resource TypeApplication Notes
Results 1-5 of 5 for gecko-os/4/standard/4.1/sdk/demo-secure-element-main-c-example