// Bluetooth LE//Version 5.0 //API Reference //BGAPI Headers You are viewing documentation for version: 5.0 BGAPI# BGAPI message header format# ... BGAPI protocol stores data in little endian.
// Bluetooth LE//Version 5.0 //API Reference //Commands & Events ... //sl_bt_evt_scanner_scan_report You are viewing documentation for version: 5.0 sl_bt_evt_scanner_scan_reportScanner#
// Bluetooth LE//Version 7.1.1 //Bluetooth Stack API Reference //Security Manager ... 0: If database is full, new bonding attempts will fail ... address The Bluetooth device address uint32_t *
// Bluetooth LE//Version 6.1.0 //Bluetooth API Reference Guide //System You are viewing documentation for version: 6.1.0 Modules# ... Bluetooth identity address in little endian format
0 dBm is enough to cover about 10 to 15 m range, based on tests made with iBeacon example and Android ... Bluetooth 5 introduced 2M PHY for faster throughput and higher energy efficiency.
Results 1-5 of 5 for gecko-os/4/standard/4.1/sdk/file-log-file-encrypted-main-c-example