hurricane/security_camera/resources/cloud_server/public/src/router/index.js
import Vue from 'vue'
import VueRouter from 'vue-router'
import routes from './routes'
Vue.use(VueRouter)
/*
* If not building with SSR mode, you can
* directly export the Router instantiation
*/
export default function (/* { store, ssrContext } */) {
const Router = new VueRouter({
scrollBehavior: () => ({ x: 0, y: 0 }),
routes,
// Leave these as is and change from quasar.conf.js instead!
// quasar.conf.js -> build -> vueRouterMode
// quasar.conf.js -> build -> publicPath
mode: process.env.VUE_ROUTER_MODE,
base: process.env.VUE_ROUTER_BASE
})
return Router
}