network/http_methods/http_methods.mk
# The name of the project component
NAME := app_network_http_methods
$(NAME)_RESOURCE_MANIFEST_PATH := manifest.cfg
# Paths to app settings .ini files (paths are relative to project directory)
$(NAME)_SETTINGS_INCLUDES := resources/settings.ini
# Enable/disable automatic generation of static function prototypes in project source code
$(NAME)_AUTO_PROTOTYPE := 1
$(NAME)_REQUIRED_COMPONENTS := resources.gecko_os.webapp
# List of files to include in the project build. Paths relative to the project's directory
$(NAME)_SOURCES := main.c \
http_get.c \
http_post.c \
http_put.c \
http_delete.c \
http_head.c