network/tcp_echo_server/resources/settings.ini
network.buffer.size 50000
network.buffer.control_size 12000
wlan.rssi_average 0
wlan.auto_join.enabled 1
tcp.keepalive.enabled 1
tcp.keepalive.initial_timeout 5
tcp.keepalive.retry_count 3
tcp.keepalive.retry_timeout 1
tcp.server.idle_timeout 15
tcp.server.port 3000
# Remote terminal is NOT used, but the python TCP client script
# uses this variable to determine the TCP server port
remote_terminal.port 3000
stream.auto_close 0
broadcast.data ip,remote_terminal_port,mac,uuid
broadcast.interval 5
broadcast.udp.remote_port 55555