system/application_settings/application_settings.mk

# The name of the project component
NAME := app_system_application_settings
# Enable/disable automatic generation of static function prototypes in project source code
$(NAME)_AUTO_PROTOTYPE := 1
# List of files to include in the project build. Paths relative to the project's directory
$(NAME)_SOURCES := main.c
# Paths to app settings .ini files (paths are relative to project directory)
$(NAME)_SETTINGS_INCLUDES := resources/one_time_settings.ini \
resources/runtime_settings.ini
# Include the webapp resource files
$(NAME)_REQUIRED_COMPONENTS := resources.gecko_os.webapp