The Gecko OS Command API is friendly for humans too. ... 2 : hex format: upper or lower case, with leading 0x , e.g. 0xFE , 0xe1c8 ... WGM160P Gecko OS Plugin plugin_core_commands Example
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Modules Types Command data types. Functions ... Issue Gecko OS command, store string result in buffer. ... Command configuration, see gos_cmd_operation_config_t for more details.
ProductWirelessResource TypeSoftware API documentation
OS timer frequency configuration parameters that can be set to modify the timer ... API references and other information about this and earlier releases is available on https://docs.silabs.com ...
... modules using the Xpress framework, which provides a simple API for BGX interaction. ... , exercising both the streaming interface and the Xpress command API through remote command execution.
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/4.2/group-api-core-command-types