// Gecko Platform//Version 4.4.1 //Services ... The hardware timer peripheral must be properly clocked from the application. ... All API functions can be called from within interrupt handlers.
Gecko Platform 3.0.0.2 GA Gecko SDK Suite 3.0 July 29, 2020 ... Gecko Bootloader Added rollback prevention feature ... Documentation can be found at service/api/group-device-init.
// Platform//Version 5.0.1 //Security ... Hardware block inside the SE used for generating random numbers. ... sl_se_otp_init_t otp_settings_init = SL_SE_OTP_INIT_DEFAULT;
You should avoid using it in production. ... Functions sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables sl_iostream_t * sl_iostream_rtt_handle ... ) RTT Stream init. Returns
ProductMicrocontrollersResource TypeSoftware API documentation
Results 1-6 of 6 for gecko-os/4/standard/4.2/group-api-proto-http-server-stream-types