2 - no update available (i.e. the device's current firmware is up-to-date) <message> - bundle version or ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ...
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Modules Types Command data types. Functions ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API . ... Note
ProductWirelessResource TypeSoftware API documentation
OS timer frequency configuration parameters that can be set to modify the timer frequency (and the ... API references and other information about this and earlier releases is available on ...
... with BGX modules using the Xpress framework, which provides a simple API for BGX interaction. ... both the streaming interface and the Xpress command API through remote command execution.
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/4.2/group-api-proto-http-server-types