Gecko OS writes the file to extended flash or bulk flash, depending on the location option: -l extended/bulk . ... 2 : hex format: upper or lower case, with leading 0x , e.g. 0xFE , 0xe1c8
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API .
ProductWirelessResource TypeSoftware API documentation
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... Safe mode operation is guaranteed in the unlikely event the device is configured in a ...
ProductWirelessResource TypeSoftware API documentation
OS timer frequency configuration parameters that can be set to modify the timer ... API references and other information about this and earlier releases is available on https://docs.silabs.com ...
Resource TypeRelease Notes
Results 1-5 of 5 for gecko-os/4/standard/4.2/group-api-util-safe-objects