Interface
Functions for starting/stop WLAN & SoftAP interfaces. More...
Modules | |
Types | |
Network Interface Types. | |
Macros | |
Network interface specific macros. | |
Functions | |
gos_result_t | gos_network_set_credentials (gos_interface_t interface, const char *ssid, const char *password, bool save_to_nvm) |
Set the interface's network credentials. More... | |
gos_result_t | gos_network_get_credentials (gos_interface_t interface, gos_ssid_t *ssid, gos_buffer_t *password) |
Get the interface's network credentials. More... | |
gos_result_t | gos_network_get_security (gos_interface_t interface, gos_security_t *security_ptr) |
Get the current security of the interface. More... | |
gos_result_t | gos_network_up (gos_interface_t interface, bool block) |
Bring network interface up. More... | |
gos_result_t | gos_network_down (gos_interface_t interface) |
Bring network interface down. More... | |
gos_result_t | gos_network_restart (gos_interface_t interface) |
Restart network interface. More... | |
bool | gos_network_is_up (gos_interface_t interface) |
Return status of network interface. More... | |
bool | gos_network_is_permanent_down (void) |
Return if the network interface is permanently down, this occurs when the module is being rebooted. More... | |
gos_interface_t | gos_network_get_default_interface (void) |
Return the currently active default network interface. More... | |
gos_result_t | gos_network_set_default_interface (gos_interface_t interface) |
Set the default network interface. More... | |
gos_wlan_result_t | gos_network_get_wlan_join_result (void) |
Return the result of the most recent WLAN join attempt. More... | |
const char * | gos_network_get_wlan_join_result_str (void) |
Return the result string of the most recent WLAN join attempt. More... | |
gos_network_status_t | gos_network_get_status (gos_interface_t interface) |
Return the current interface status. More... | |
gos_result_t | gos_network_close_all_streams (gos_interface_t interface) |
Close all data streams on specified network interface. More... | |
gos_result_t | gos_network_softap_client_list (gos_softap_client_t *client_list, uint32_t *client_count) |
Return list of SoftAP clients. More... | |
gos_result_t | gos_network_softap_deauth_client (gos_mac_t *mac, gos_deauth_reason_t reason) |
Deauthenticate SoftAP client. More... | |
gos_result_t | gos_network_register_event_handler (gos_interface_t interface, gos_network_handler_t handler) |
Register network event handler. More... | |
gos_result_t | gos_network_register_softap_event_handler (gos_softap_event_handler_t handler) |
Register SoftAP client event handler. More... | |
void | gos_network_set_softap_domain_list (const char *domain_list) |
Set list of domain names DNS server will resolve. More... | |
Detailed Description
Functions for starting/stop WLAN & SoftAP interfaces.
Function Documentation
◆ gos_network_close_all_streams()
gos_result_t gos_network_close_all_streams | ( | gos_interface_t | interface | ) |
Close all data streams on specified network interface.
- Parameters
-
[in] interface
gos_interface_t the interface to close all streams on
- Returns
- gos_result_t result of api call
◆ gos_network_down()
gos_result_t gos_network_down | ( | gos_interface_t | interface | ) |
Bring network interface down.
See Gecko OS Command API documentation: network_down.
- Parameters
-
[in] interface
gos_interface_t the interface to bring down
- Returns
- gos_result_t result of api call
- Examples:
- utility/profiler/main.c.
◆ gos_network_get_credentials()
gos_result_t gos_network_get_credentials | ( | gos_interface_t | interface, |
gos_ssid_t * | ssid, |
||
gos_buffer_t * | password |
||
) |
Get the interface's network credentials.
This returns the current credentials for the given network interface.
- Note
- The supplied
password
buffer should be at least 64 bytes.
- Parameters
-
[in] interface
Interface to retrieve network credentials. See gos_interface_t [out] ssid
gos_ssid_t To be populated with interface's current SSID. [out] password
To be populated with interface's current password, the supplied buffer should be at least 64 chars
- Returns
- gos_result_t result of api call
◆ gos_network_get_default_interface()
gos_interface_t gos_network_get_default_interface | ( | void |
| ) |
Return the currently active default network interface.
- Returns
- gos_interface_t the currently configured default network interface
◆ gos_network_get_security()
gos_result_t gos_network_get_security | ( | gos_interface_t | interface, |
gos_security_t * | security_ptr |
||
) |
Get the current security of the interface.
- Parameters
-
interface
Interface to retrieve network security security_ptr
Pointer to gos_security_t to be populated with network's security
- Returns
- gos_result_t result of api call
◆ gos_network_get_status()
gos_network_status_t gos_network_get_status | ( | gos_interface_t | interface | ) |
Return the current interface status.
See gos_network_status_t for more info.
- Parameters
-
interface
Network interface, see gos_interface_t
- Returns
- Current interface status, see gos_network_status_t
◆ gos_network_get_wlan_join_result()
gos_wlan_result_t gos_network_get_wlan_join_result | ( | void |
| ) |
Return the result of the most recent WLAN join attempt.
See gos_wlan_result_t for more info.
- Returns
- Result of last join attempt, see gos_wlan_result_t
- Examples:
- hurricane/security_camera/main.c, and wifi/web_setup/main.c.
◆ gos_network_get_wlan_join_result_str()
const char* gos_network_get_wlan_join_result_str | ( | void |
| ) |
Return the result string of the most recent WLAN join attempt.
See gos_wlan_result_t for more info.
- Returns
- Result of last join attempt as string, see gos_wlan_result_t
◆ gos_network_is_permanent_down()
bool gos_network_is_permanent_down | ( | void |
| ) |
Return if the network interface is permanently down, this occurs when the module is being rebooted.
- Returns
- true if the network interface is permanently down, false else
◆ gos_network_is_up()
bool gos_network_is_up | ( | gos_interface_t | interface | ) |
Return status of network interface.
- Parameters
-
[in] interface
gos_interface_t the interface to check status of
- Returns
- true is network interface is up, false else
◆ gos_network_register_event_handler()
gos_result_t gos_network_register_event_handler | ( | gos_interface_t | interface, |
gos_network_handler_t | handler |
||
) |
Register network event handler.
- Note
- The event handler executes in the app thread context
- Parameters
-
[in] interface
gos_interface_t the interface to register handler with [in] handler
gos_network_handler_t to be called on network interface event
- Returns
- gos_result_t result of api call
◆ gos_network_register_softap_event_handler()
gos_result_t gos_network_register_softap_event_handler | ( | gos_softap_event_handler_t | handler | ) |
Register SoftAP client event handler.
- Note
- The event handler executes in the app thread context
- Parameters
-
[in] handler
gos_softap_event_handler_t to be called on softap client event
- Returns
- gos_result_t result of api call
- Examples:
- network/softap_tcp_server/main.c.
◆ gos_network_restart()
gos_result_t gos_network_restart | ( | gos_interface_t | interface | ) |
Restart network interface.
See Gecko OS Command API documentation: network_restart.
- Parameters
-
[in] interface
gos_interface_t the interface to restart
- Returns
- gos_result_t result of api call
- Examples:
- cloud/coap_demo/main.c.
◆ gos_network_set_credentials()
gos_result_t gos_network_set_credentials | ( | gos_interface_t | interface, |
const char * | ssid, |
||
const char * | password, |
||
bool | save_to_nvm |
||
) |
Set the interface's network credentials.
This sets the network credentials for the given interface.
- Note
- If
save_to_nvm
is false, the credentials are cached in RAM only. Ifsave_to_nvm
is true, the credentials are ALSO saved to NVM. Any other currently cached settings are also saved to NVM.
- Parameters
-
[in] interface
The network interface, see gos_interface_t [in] ssid
The network name, leave NULL to clear the interface's SSID [in] password
The network password, optional, leave NULL to clear the interface's password [in] save_to_nvm
Save credentials to NVM to they persist through reboots/powercycles
- Returns
- gos_result_t result of api call
◆ gos_network_set_default_interface()
gos_result_t gos_network_set_default_interface | ( | gos_interface_t | interface | ) |
Set the default network interface.
- Note
- The default interface will NOT update until the previous default interface is brought down.
- Returns
- gos_result_t result of api call
◆ gos_network_set_softap_domain_list()
void gos_network_set_softap_domain_list | ( | const char * | domain_list | ) |
Set list of domain names DNS server will resolve.
This set a list of domain names the SoftAP's DNS server will resolve. The specified list overrides the Gecko OS setting: softap.dns_server.url
- Parameters
-
[in] domain_list
Comma seperated list of domain names
◆ gos_network_softap_client_list()
gos_result_t gos_network_softap_client_list | ( | gos_softap_client_t * | client_list, |
uint32_t * | client_count |
||
) |
Return list of SoftAP clients.
The supplied client_list argument should be a buffer large enough to hold all associated clients. e.g.
- Parameters
-
[out] client_list
Buffer containing list of associated client's information [out] client_count
Pointer to hold number of client's associated, leave NULL if unused
- Returns
- gos_result_t result of api call
◆ gos_network_softap_deauth_client()
gos_result_t gos_network_softap_deauth_client | ( | gos_mac_t * | mac, |
gos_deauth_reason_t | reason |
||
) |
Deauthenticate SoftAP client.
This boots a softap client of the softap network.
- Parameters
-
[in] mac
MAC address of SoftAP client [in] reason
Reason for deauthenticating client, see gos_deauth_reason_t
- Returns
- gos_result_t result of api call
◆ gos_network_up()
gos_result_t gos_network_up | ( | gos_interface_t | interface, |
bool | block |
||
) |
Bring network interface up.
See Gecko OS Command API documentation: network_up.
- Parameters
-
[in] interface
gos_interface_t the interface to bring up [in] block
true if API call should block until interface is brought up, false if it should return immediately
- Returns
- gos_result_t result of api call
- Examples:
- demo/3d_demo/main.c, demo/accelerometer_stream/main.c, hurricane/security_camera/main.c, network/softap_tcp_server/main.c, network/tcp_client/main.c, network/uart_tcp_client/main.c, network/udp_client/main.c, network/websocket_client/main.c, utility/profiler/main.c, and wifi/device_setup/main.c.