WebSocket Client/Server
WebSocket client/server functions. More...
Modules | |
Types | |
WebSocket data types. | |
Functions | |
gos_result_t | gos_websocket_connect (gos_interface_t interface, const char *host, gos_handle_t *handle_ptr) |
Connect to a remote websocket server. More... | |
gos_result_t | gos_websocket_connect_with_config (const gos_websocket_config_t *config, gos_handle_t *handle_ptr) |
Connect to a remote websocket server with configuration. More... | |
gos_result_t | gos_websocket_read (gos_handle_t handle, void *data, uint32_t max_size, uint32_t *bytes_read_ptr) |
Read websocket stream data. More... | |
gos_result_t | gos_websocket_read_with_buffer (gos_handle_t handle, gos_buffer_t *buffer) |
Read websocket stream data into buffer. More... | |
gos_result_t | gos_websocket_write (gos_handle_t handle, const void *data, uint32_t size, bool continue_frame) |
Write websocket stream data. More... | |
gos_result_t | gos_websocket_disconnect (gos_handle_t handle) |
Close websocket stream. More... | |
gos_result_t | gos_websocket_poll (gos_handle_t handle, uint32_t *rx_bytes_available, uint32_t *tx_bytes_available) |
Poll websocket stream for RX data. More... | |
gos_result_t | gos_websocket_send_ping (gos_handle_t handle, const void *data, uint32_t size) |
Send a 'Ping' to Websocket client or server. More... | |
gos_result_t | gos_websocket_client_read_frame (gos_handle_t handle, gos_websocket_frame_t *frame, uint32_t timeout_ms) |
Read complete websocket frame. More... | |
void | gos_websocket_register_server_event_handlers (gos_stream_event_handler_t connect, gos_stream_event_handler_t disconnect, gos_stream_event_handler_t receive) |
Register websocket server event handlers. More... | |
void | gos_websocket_register_client_event_handlers (gos_handle_t handle, gos_stream_event_handler_t disconnect, gos_stream_event_handler_t receive) |
Register websocket client event handlers. More... | |
gos_result_t | gos_websocket_get_client_info (gos_handle_t handle, char *host_buffer, uint32_t host_buffer_len, uint16_t *local_port_ptr, uint16_t *remote_port_ptr) |
Get Websocket client info. More... | |
Detailed Description
WebSocket client/server functions.
Function Documentation
◆ gos_websocket_client_read_frame()
gos_result_t gos_websocket_client_read_frame | ( | gos_handle_t | handle, |
gos_websocket_frame_t * | frame, |
||
uint32_t | timeout_ms |
||
) |
Read complete websocket frame.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
◆ gos_websocket_connect()
gos_result_t gos_websocket_connect | ( | gos_interface_t | interface, |
const char * | host, |
||
gos_handle_t * | handle_ptr |
||
) |
Connect to a remote websocket server.
This opens a websocket client stream.
See Gecko OS Command API documentation: websocket_client.
- Parameters
-
interface
The network interface to open connect host
The remote websocket server's URL handle_ptr
The stream handle of the opened websocket client stream
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_client/main.c.
◆ gos_websocket_connect_with_config()
gos_result_t gos_websocket_connect_with_config | ( | const gos_websocket_config_t * | config, |
gos_handle_t * | handle_ptr |
||
) |
Connect to a remote websocket server with configuration.
See Gecko OS Command API documentation: websocket_client.
This does the same thing as gos_websocket_connect() but allows for additional configuration. See gos_websocket_config_t for optional configuration settings.
- Parameters
-
config
Websocket client configuration handle_ptr
The stream handle of the opened websocket client stream
- Returns
- gos_result_t result of api call
◆ gos_websocket_disconnect()
gos_result_t gos_websocket_disconnect | ( | gos_handle_t | handle | ) |
Close websocket stream.
See Gecko OS Command API documentation: stream_close.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handle
Handle of stream to close
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_client/main.c.
◆ gos_websocket_get_client_info()
gos_result_t gos_websocket_get_client_info | ( | gos_handle_t | handle, |
char * | host_buffer, |
||
uint32_t | host_buffer_len, |
||
uint16_t * | local_port_ptr, |
||
uint16_t * | remote_port_ptr |
||
) |
Get Websocket client info.
See Gecko OS Command API documentation: stream_list.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handle
Client stream handle [in] host_buffer
Buffer to hold client host domain or IP address string [in] host_buffer_len
Length of host_buffer
[in] local_port_ptr
Pointer to hold client's local port, leave NULL to ignore [in] remote_port_ptr
Pointer to hold client's remote port, leave NULL to ignore
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_server/main.c.
◆ gos_websocket_poll()
gos_result_t gos_websocket_poll | ( | gos_handle_t | handle, |
uint32_t * | rx_bytes_available, |
||
uint32_t * | tx_bytes_available |
||
) |
Poll websocket stream for RX data.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handle
Handle of stream to poll [out] rx_bytes_available
Pointer to hold number of bytes available to read [out] tx_bytes_available
Pointer to hold available TX buffer space
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_client/main.c.
◆ gos_websocket_read()
gos_result_t gos_websocket_read | ( | gos_handle_t | handle, |
void * | data, |
||
uint32_t | max_size, |
||
uint32_t * | bytes_read_ptr |
||
) |
Read websocket stream data.
See Gecko OS Command API documentation: stream_read.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handle
Stream handle returned by API call [out] data
Buffer to hold read data [in] max_size
Maximum amount of data to read [out] bytes_read_ptr
Pointer to hold actual amount of data read (set NULL if not used)
- Returns
- gos_result_t result of api call
◆ gos_websocket_read_with_buffer()
gos_result_t gos_websocket_read_with_buffer | ( | gos_handle_t | handle, |
gos_buffer_t * | buffer |
||
) |
Read websocket stream data into buffer.
See gos_read_with_buffer() for more information.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
handle
Stream handle buffer
Buffer to specify how much data to read, then return how much data was read with pointer to data
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_client/main.c, and network/websocket_server/main.c.
◆ gos_websocket_register_client_event_handlers()
void gos_websocket_register_client_event_handlers | ( | gos_handle_t | handle, |
gos_stream_event_handler_t | disconnect, |
||
gos_stream_event_handler_t | receive |
||
) |
Register websocket client event handlers.
The corresponding event handlers will be called on the given websocket clients event. See gos_websocket_connect() to open a websocket client.
- Note
- The event handlers execute in the app thread context
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
handle
Stream handle of websocket client stream (returned by gos_websocket_connect() ) disconnect
Websocket client disconnect event handler receive
Websocket client data received event handler
- Examples:
- network/websocket_client/main.c.
◆ gos_websocket_register_server_event_handlers()
void gos_websocket_register_server_event_handlers | ( | gos_stream_event_handler_t | connect, |
gos_stream_event_handler_t | disconnect, |
||
gos_stream_event_handler_t | receive |
||
) |
Register websocket server event handlers.
The following event handler will be called on the corresponding websocket server events. Set to NULL to disable the event handler.
- Note
- The event handlers execute in the app thread context
- Parameters
-
connect
Websocket client connect event handler disconnect
Websocket client disconnect event handler receive
Websocket client data received event handler
- Examples:
- network/websocket_server/main.c.
◆ gos_websocket_send_ping()
gos_result_t gos_websocket_send_ping | ( | gos_handle_t | handle, |
const void * | data, |
||
uint32_t | size |
||
) |
Send a 'Ping' to Websocket client or server.
This sends a 'Ping' with an optional data payload to the websocket client/server. If no data payload is required then leave the 'size' paramater zero.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
handle
Handle of websocket client/server stream data
Optional ping data payload, leave NULL if unused size
Size of optional data payload, leave zero if unused
- Returns
- gos_result_t result of api call
◆ gos_websocket_write()
gos_result_t gos_websocket_write | ( | gos_handle_t | handle, |
const void * | data, |
||
uint32_t | size, |
||
bool | continue_frame |
||
) |
Write websocket stream data.
See Gecko OS Command API documentation: stream_write.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handle
Stream handle returned by API call [in] data
Data to write to stream [in] size
Size of data in bytes to write [in] continue_frame
If true then sends 'continued' websocket frame, false send 'final' websocket frame
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_client/main.c, and network/websocket_server/main.c.