network/softap_tcp_server/main.c
/*******************************************************************************
* # License
* Copyright 2019 Silicon Laboratories Inc. www.silabs.com
*******************************************************************************
*
* The licensor of this software is Silicon Laboratories Inc. Your use of this
* software is governed by the terms of Silicon Labs Master Software License
* Agreement (MSLA) available at
* www.silabs.com/about-us/legal/master-software-license-agreement. This
* software is distributed to you in Source Code format and is governed by the
* sections of the MSLA applicable to Source Code.
*
******************************************************************************/
/* Documentation for this app is available online.
* See https://docs.silabs.com/gecko-os/4/standard/latest/sdk/examples/network/softap-tcp-server
*/
#include "gos.h"
#define TCP_SERVER_PORT 2000
#define WELCOME_MSG "Welcome to the TCP Echo Server\r\n"
#define APPLICATION_START_LINE "\r\nSoftAP TCP Server Example starting ..."
/*************************************************************************************************/
{
gos_result_t result;
char buffer[32];
GOS_LOG(APPLICATION_START_LINE);
{
GOS_LOG("Failed to load settings, err:%d", result);
return;
}
gos_tcp_register_server_event_handlers(tcp_client_connect_handler, tcp_client_disconnect_handler, tcp_client_receive_handler);
gos_network_register_softap_event_handler(softap_event_handler);
GOS_LOG("Starting SoftAP...");
{
GOS_LOG("Failed to start SoftAP, err:%d", result);
return;
}
GOS_LOG("Starting TCP Echo Server...");
{
GOS_LOG("Failed to start TCP Server: %d", result);
return;
}
GOS_LOG("TCP Echo Server listening on: %s:%u", GOS_GET_SETTING_STR("softap.dns_server.url", buffer), TCP_SERVER_PORT);
}
/*************************************************************************************************/
{
char mac_str[32];
char ip_str[32];
}
/*************************************************************************************************/
{
char host_buffer[64];
uint16_t local_port, remote_port;
if (gos_tcp_get_client_info(handle, host_buffer, sizeof(host_buffer), &local_port, &remote_port) == GOS_SUCCESS)
{
GOS_LOG("TCP Client: %s:%u connected", host_buffer, remote_port);
}
}
/*************************************************************************************************/
{
GOS_LOG("TCP Client: %d disconnected", handle);
}
/*************************************************************************************************/
{
#define STREAM_READ_TIMEOUT 100
gos_result_t result;
// NOTE: We do NOT want to spend too much time in this loop reading the RX stream data
// as it will starve the rest of the system.
// Thus we break out of the loop after STREAM_READ_TIMEOUT milliseconds.
// Another RX event will be triggered if more data is available.
while ((gos_rtos_get_time() - start_time) < STREAM_READ_TIMEOUT)
{
{
break;
}
{
GOS_LOG("Failed to read from stream %d, err:%d", handle, result);
break;
}
GOS_LOG("Rx data:");
{
GOS_LOG("Failed to write to stream %d, err:%d", handle, result);
break;
}
}
}