system/settings_file/settings_file.mk
# The name of the project component
NAME := app_system_settings_file
# Enable/disable automatic generation of static function prototypes in project source code
$(NAME)_AUTO_PROTOTYPE := 1
# List of files to include in the project build. Paths relative to the project's directory
$(NAME)_SOURCES := main.c \
nvm_defaults.c \
nvm_defaults_validate.c
# Include the webapp resource files
$(NAME)_REQUIRED_COMPONENTS := resources.gecko_os.webapp
$(NAME)_RESOURCE_MANIFEST_PATH := resources/manifest.cfg