// Bluetooth LE//Version 5.0 //API Reference ... You are viewing documentation for version: 5.0 sl_bt_evt_system_external_signalSystem# Indicates that the external signals have been received.
// Bluetooth LE//Version 6.1.0 //Bluetooth API Reference Guide //System You are viewing documentation for version: 6.1.0 Modules# ... Bluetooth identity address in little endian format
// Bluetooth LE//Version 5.0 //API Reference ... To use these new events, the application needs to include the bluetooth_feature_legacy_scanner or bluetooth_feature_extended_scanner component.
Training ... // Bluetooth LE//Version 5.0 //API Reference //Commands & Events //Scanner ... You are viewing documentation for version: 5.0 sl_bt_evt_scanner_legacy_advertisement_reportScanner#
For legacy devices (BLExxx) <=1.5.0 4.0 ... Bluetooth 4.2 specifies the PHY bitrate to be exactly 1 Mbps. Bluetooth 5 (introduced in Bluetooth SDK v2.3) specifies PHY bitrates as follows:
... Allow connections only from bonded devices Bit 5: 0: Prefer just works pairing when both options are possible based on the settings. ... 0: If database is full, new bonding attempts will fail
Results 1-6 of 6 for gecko-os/4/standard/4.2/sdk/using-emlib