Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... system.cmd.buffered system.cmd.echo system.cmd.header_enabled system.cmd.prompt_enabled
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
gos_result_t gos_cmd_issue (const char *fmt,.) Issue Gecko OS Command. More. ... Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer.
ProductWirelessResource TypeSoftware API documentation
Gecko OS Web App The Gecko OS Web App provides complete monitoring and control of your Gecko OS device ... As well as standard Gecko OS terminal behavior, the Console tab provides additional ...
os pins can only use the strong drive strength. ... Output, push-pull 4 Output, open-drain with no pull-up (see gdi od prdi ) ... Output, open-source with pull-up (see gdi os pren )
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/cmd/apps/web-app-customization