Update and Recovery Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... ls ... The factory reset GPIO is GPIO 0 on all Gecko OS devices.
ProductWirelessResource TypeSoftware API documentation
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Gecko OS evaluation boards are by default configured to enter Setup Web mode when you hold down Button 2 ... As well as standard Gecko OS terminal behavior, the Console tab provides additional ...
where: <GPIO#> - The GPIO number <direction> - Pin direction. ... os pins can only use the strong drive strength. ... GPIO function pins typically only operate in one direction (in or out).
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/apps/oob-gpio