Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... reboot ... tcp.client.local_port tcp.client.retries tcp.client.retry_period uart.baud
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command ... Commands Variables Examples
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
Return variables to factory default settings by deleting user configuration (if ... os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren )
ProductWirelessResource TypeSoftware API documentation
Gecko OS evaluation boards are by default configured to enter Setup Web mode when you hold down Button 2 ... As well as standard Gecko OS terminal behavior, the Console tab provides additional ...
Results 1-5 of 5 for gecko-os/4/standard/latest/apps/serial-http-server