Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... reboot ... The following variables can be locked to prevent change on factory reset.
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command ... Commands Variables Examples
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
Gecko OS Web App The Gecko OS Web App provides complete monitoring and control of your Gecko OS device ... As well as standard Gecko OS terminal behavior, the Console tab provides additional ...
Return variables to factory default settings by deleting user configuration (if ... os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren )
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/apps/udp-client