Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... system.cmd.buffered system.cmd.echo system.cmd.header_enabled system.cmd.prompt_enabled
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
gos_result_t gos_cmd_issue (const char *fmt,.) Issue Gecko OS Command. More. ... Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer.
ProductWirelessResource TypeSoftware API documentation
Gecko OS evaluation boards are by default configured to enter Setup Web mode when you hold down Button 2 ... As well as standard Gecko OS terminal behavior, the Console tab provides additional ...
... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren )
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-cmd