Commands Core Functions for issuing Gecko OS commands. ... Issue Gecko OS command, store string result in buffer. ... Command configuration, see gos_cmd_operation_config_t for more details.
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... to update the firmware, or switch back to Gecko OS using the faults_reset command.
ProductWirelessResource TypeSoftware API documentation
... of Bluetooth Xpress API commands with a full description of how to use each command. Command Editing The Bluetooth Xpress command mode is ... os pins can only use the strong drive strength.
ProductWirelessResource TypeSoftware API documentation
... application (e.g., putting them below FreeRTOS OS atomic for access to OS functions in RAIL callbacks). ... This API indicates that the DCDC peripheral bus clock has changed allowing RAIL to ...
Resource TypeSoftware API Documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-core-command