Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... and Setup, Resetting Variable Values for details of reset types and the reset process.
ProductWirelessResource TypeSoftware API documentation
Modules Types Command data types. Functions ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API . ... Note
ProductWirelessResource TypeSoftware API documentation
... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. May be one of the following types: drvst : Strong drive ...
ProductWirelessResource TypeSoftware API documentation
... the standard PHYs defined by the 802.15.4 PHY layer specification, it is possible to ... 4.1 Applying a PHY from RAIL rx 0 // Configs can be loaded only in radio Idle state config2p4GHz802154 ...
Resource TypeApplication Notes
Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-disco-broadcast-types